This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:tools-software:linux-drivers:iio-transceiver:adrv9002-customization [11 Dec 2020 14:13] – [AGC Settings] Nuno Sá | resources:tools-software:linux-drivers:iio-transceiver:adrv9002-customization [07 Jan 2021 20:24] (current) – Add examples of split and mimo devtrees Travis Collins | ||
---|---|---|---|
Line 8: | Line 8: | ||
If unsure please see the manual or don't change! | If unsure please see the manual or don't change! | ||
</ | </ | ||
+ | |||
+ | ====== RX and TX Channels ====== | ||
+ | |||
+ | ADRV9002 can operate different RX and TX channels at different rates due to the flexibility of the hardware. Making it possible to run four channels (TX1, | ||
+ | |||
+ | The two main categories are combined DMA mode, which we refer to as MIMO mode, and a split DMA mode. In the first case, a single DMA driver is instantiated with up to four channels (two complex) per data direction. This allows for synchronous capture between RX1 and RX2 or transmission with TX1 and TX2. Alternatively, | ||
+ | |||
+ | For examples of these arrangements, | ||
+ | * [[linux.github> | ||
+ | * [[linux.github> | ||
====== RX ====== | ====== RX ====== |