Wiki

This version is outdated by a newer approved version.DiffThis version (02 Jul 2021 10:22) was approved by Michael Hennerich.The Previously approved version (04 Feb 2021 20:14) is available.Diff

This is an old revision of the document!


Table of Contents

AD9371, AD9375 highly integrated, wideband RF transceiver Linux device driver

AD9371 The AD9371 AD9375 is a highly integrated, wideband RF transceiver offering dual channel transmitters and receivers, integrated synthesizers, and digital signal processing functions. The IC delivers a versatile combination of high performance and low power consumption required by 3G/4G micro and macro base station equipment in both FDD and TDD applications. The AD9371 operates from 300 MHz to 6000 MHz, covering most of the licensed and unlicensed cellular bands. The IC supports receiver bandwidths up to 100 MHz. It also supports observation receiver and transmit synthesis bandwidths up to 250 MHz to accommodate digital correction algorithms. The transceiver consists of wideband direct conversion signal paths with state-of-the-art noise figure and linearity. Each complete receiver and transmitter subsystem includes dc offset correction, quadrature error correction, and programmable digital filters, eliminating the need for these functions in the digital baseband. Several auxiliary functions such as an auxiliary analog-to-digital converter (ADC), auxiliary digital-to-analog converters (DACs), and general-purpose input/outputs (GPIOs) are integrated to provide additional monitoring and control capability. An observation receiver channel with two inputs is included to monitor each transmitter output and implement interference mitigation and calibration applications. This channel also connects to three sniffer receiver inputs that can monitor radio activity in different bands.

The AD9375 device variant provides digital signal processing capabilities in the embedded ARM processor using closed-loop feedback signals from the observation receiver channels. These functions improve transmitter performance, measure system output, and reduce system power consumption. The list of functions includes the following: digital predistortion (DPD), closed-loop gain control (CLGC), and voltage standing wave ratio (VSWR) measurement.

Supported Devices

Evaluation Boards

Description

This is a Linux industrial I/O (IIO) subsystem driver, targeting RF Transceivers. The industrial I/O subsystem provides a unified framework for drivers for many different types of converters and sensors using a number of different physical interfaces (i2c, spi, etc). See IIO for more information.

Source Code

Status

Source Mainlined?
git No

Files

Interrelated Device Drivers

Receive AXI-ADC driver

Transmit AXI-DAC / DDS driver

AXI JESD204B HDL driver

AXI JESD204B GT (Gigabit Tranceiver) HDL driver (XILINX/ALTERA-INTEL)

Function File
driver drivers/iio/jesd204/axi_adxcvr.c

Device Driver Customization

Please follow the link here for detailed options and examples:

Example Linux Device-Tree Initialization

The AD9371 driver is a spi-bus driver and can currently only be instantiated via device tree.

Required devicetree properties:

  • compatible: Should always be either “ad9371” or “ad9375”
  • reg: SPI slave select number
Function File
ADRV9371 Device Tree adi-adrv9371.dtsi
ADRV9371 Device Tree zynq-zc706-adv7511-adrv9371.dts
ADRV9371 Device Tree socfpga_arria10_socdk_adrv9009.dts
ADRV9375 Device Tree zynq-zc706-adv7511-adrv9375.dts

Enabling Linux driver support

Configure kernel with “make menuconfig” (alternatively use “make xconfig” or “make qconfig”)

The AD9371 driver depends on CONFIG_SPI

Adding Linux driver support

Configure kernel with “make menuconfig” (alternatively use “make xconfig” or “make qconfig”)

Linux Kernel Configuration
	Device Drivers  --->
	<*>     Industrial I/O support --->
	    --- Industrial I/O support
	    -*-   Enable ring buffer support within IIO
	    -*-     Industrial I/O lock free software ring
	    -*-   Enable triggered sampling support

	          *** Analog to digital converters ***
	    [--snip--]

		-*- Analog Devices High-Speed AXI ADC driver core
		< > Analog Devices AD9361, AD9364 RF Agile Transceiver driver
		<*> Analog Devices AD9371 RF Transceiver driver
		< > Analog Devices AD6676 Wideband IF Receiver driver
		< > Analog Devices AD9467, AD9680, etc. high speed ADCs
		< > Analog Devices Motor Control (AD-FMCMOTCON) drivers
		< > Generic FFT driver
		<*> Generic AXI JESD204B configuration driver

	    [--snip--]

	Frequency Synthesizers DDS/PLL  --->
    		Direct Digital Synthesis  --->
	 		<*> Analog Devices CoreFPGA AXI DDS driver

Hardware configuration

Driver testing / API

Each and every IIO device, typically a hardware chip, has a device folder under /sys/bus/iio/devices/iio:deviceX. Where X is the IIO index of the device. Under every of these directory folders reside a set of files, depending on the characteristics and features of the hardware device in question. These files are consistently generalized and documented in the IIO ABI documentation. In order to determine which IIO deviceX corresponds to which hardware device, the user can read the name file /sys/bus/iio/devices/iio:deviceX/name. In case the sequence in which the iio device drivers are loaded/registered is constant, the numbering is constant and may be known in advance.

02 Mar 2011 15:16

TIP: An example program which uses the interface can be found here:


General attribute naming convention:

IIO sysfs attribute naming prefix Target
Transceiver
in_voltage0_[…] RX1
in_voltage1_[…] RX2
in_voltage2_[…] Observation RX
out_voltage0_[…] TX1
out_voltage1_[…] TX2
out_altvoltage0_[…] RX LO
out_altvoltage1_[…] TX LO
out_altvoltage1_[…] SNIFFER LO
Auxilary Converters
in_voltage3_[…] AUX ADC0
in_voltage4_[…] AUX ADC1
in_voltage5_[…] AUX ADC2
in_voltage6_[…] AUX ADC3
out_voltage2_[…] AUX DAC0
out_voltage3_[…] AUX DAC1
out_voltage4_[…] AUX DAC2
out_voltage5_[…] AUX DAC3
out_voltage6_[…] AUX DAC4
out_voltage7_[…] AUX DAC5
out_voltage8_[…] AUX DAC6
out_voltage9_[…] AUX DAC7
out_voltage10_[…] AUX DAC8
out_voltage11_[…] AUX DAC9

This specifies any shell prompt running on the target

root:/> cd /sys/bus/iio/devices/
root:/sys/bus/iio/devices> ls
iio:device0  iio:device3  iio:device2  iio:device3  iio:device4  iio:device5  iio:device6

root:/sys/bus/iio/devices> cd iio:device3

root@analog:/sys/bus/iio/devices/iio:device3# ls -l
total 0
-rw-rw-rw- 1 root root  4096 May 31 14:49 calibrate
-rw-rw-rw- 1 root root  4096 May 31 14:49 calibrate_rx_qec_en
-rw-rw-rw- 1 root root  4096 May 31 14:49 calibrate_tx_lol_en
-rw-rw-rw- 1 root root  4096 May 31 14:49 calibrate_tx_lol_ext_en
-rw-rw-rw- 1 root root  4096 May 31 14:49 calibrate_tx_qec_en
-rw-rw-rw- 1 root root  4096 May 19 07:59 dev
-rw-rw-rw- 1 root root  4096 May 19 08:28 ensm_mode
-rw-rw-rw- 1 root root  4096 May 19 08:28 ensm_mode_available
-rw-rw-rw- 1 root root 32768 May 19 07:59 gain_table_config
-rw-rw-rw- 1 root root  4096 May 19 08:28 in_voltage0_gain_control_mode
-rw-rw-rw- 1 root root  4096 May 19 08:28 in_voltage0_hardwaregain
-rw-rw-rw- 1 root root  4096 May 19 08:28 in_voltage0_quadrature_tracking_en
-rw-rw-rw- 1 root root  4096 May 19 07:59 in_voltage0_rf_bandwidth
-rw-rw-rw- 1 root root  4096 May 19 07:59 in_voltage0_rssi
-rw-rw-rw- 1 root root  4096 May 19 07:59 in_voltage0_sampling_frequency
-rw-rw-rw- 1 root root  4096 May 19 08:28 in_voltage0_temp_comp_gain
-rw-rw-rw- 1 root root  4096 May 19 08:28 in_voltage1_gain_control_mode
-rw-rw-rw- 1 root root  4096 May 19 08:28 in_voltage1_hardwaregain
-rw-rw-rw- 1 root root  4096 May 19 08:28 in_voltage1_quadrature_tracking_en
-rw-rw-rw- 1 root root  4096 May 19 07:59 in_voltage1_rf_bandwidth
-rw-rw-rw- 1 root root  4096 May 19 07:59 in_voltage1_rssi
-rw-rw-rw- 1 root root  4096 May 19 07:59 in_voltage1_sampling_frequency
-rw-rw-rw- 1 root root  4096 May 19 08:28 in_voltage1_temp_comp_gain
-rw-rw-rw- 1 root root  4096 May 19 08:28 in_voltage2_gain_control_mode
-rw-rw-rw- 1 root root  4096 May 19 08:28 in_voltage2_hardwaregain
-rw-rw-rw- 1 root root  4096 May 19 07:59 in_voltage2_rf_bandwidth
-rw-rw-rw- 1 root root  4096 May 19 08:28 in_voltage2_rf_port_select
-rw-rw-rw- 1 root root  4096 May 19 07:59 in_voltage2_rssi
-rw-rw-rw- 1 root root  4096 May 19 07:59 in_voltage2_sampling_frequency
-rw-rw-rw- 1 root root  4096 May 19 08:28 in_voltage2_temp_comp_gain
-rw-rw-rw- 1 root root  4096 May 19 07:59 in_voltage3_offset
-rw-rw-rw- 1 root root  4096 May 19 07:59 in_voltage3_raw
-rw-rw-rw- 1 root root  4096 May 19 07:59 in_voltage3_scale
-rw-rw-rw- 1 root root  4096 May 19 07:59 in_voltage4_offset
-rw-rw-rw- 1 root root  4096 May 19 07:59 in_voltage4_raw
-rw-rw-rw- 1 root root  4096 May 19 07:59 in_voltage4_scale
-rw-rw-rw- 1 root root  4096 May 19 07:59 in_voltage5_offset
-rw-rw-rw- 1 root root  4096 May 19 07:59 in_voltage5_raw
-rw-rw-rw- 1 root root  4096 May 19 07:59 in_voltage5_scale
-rw-rw-rw- 1 root root  4096 May 19 07:59 in_voltage6_offset
-rw-rw-rw- 1 root root  4096 May 19 07:59 in_voltage6_raw
-rw-rw-rw- 1 root root  4096 May 19 07:59 in_voltage6_scale
-rw-rw-rw- 1 root root  4096 May 19 08:28 in_voltage_gain_control_mode_available
-rw-rw-rw- 1 root root  4096 May 19 08:28 in_voltage_rf_port_select_available
-rw-rw-rw- 1 root root  4096 May 19 07:59 name
-rw-rw-rw- 1 root root  4096 May 19 08:28 out_altvoltage0_RX_LO_frequency
-rw-rw-rw- 1 root root  4096 May 19 08:28 out_altvoltage1_TX_LO_frequency
-rw-rw-rw- 1 root root  4096 May 19 08:28 out_altvoltage2_RX_SN_LO_frequency
-rw-rw-rw- 1 root root  4096 May 19 08:28 out_voltage0_hardwaregain
-rw-rw-rw- 1 root root  4096 May 19 08:28 out_voltage0_lo_leakage_tracking_en
-rw-rw-rw- 1 root root  4096 May 19 08:28 out_voltage0_quadrature_tracking_en
-rw-rw-rw- 1 root root  4096 May 19 07:59 out_voltage0_rf_bandwidth
-rw-rw-rw- 1 root root  4096 May 19 07:59 out_voltage10_offset
-rw-rw-rw- 1 root root  4096 May 19 07:59 out_voltage10_raw
-rw-rw-rw- 1 root root  4096 May 19 07:59 out_voltage10_scale
-rw-rw-rw- 1 root root  4096 May 19 07:59 out_voltage11_offset
-rw-rw-rw- 1 root root  4096 May 19 07:59 out_voltage11_raw
-rw-rw-rw- 1 root root  4096 May 19 07:59 out_voltage11_scale
-rw-rw-rw- 1 root root  4096 May 19 08:28 out_voltage1_hardwaregain
-rw-rw-rw- 1 root root  4096 May 19 08:28 out_voltage1_lo_leakage_tracking_en
-rw-rw-rw- 1 root root  4096 May 19 08:28 out_voltage1_quadrature_tracking_en
-rw-rw-rw- 1 root root  4096 May 19 07:59 out_voltage1_rf_bandwidth
-rw-rw-rw- 1 root root  4096 May 19 07:59 out_voltage2_offset
-rw-rw-rw- 1 root root  4096 May 19 07:59 out_voltage2_raw
-rw-rw-rw- 1 root root  4096 May 19 07:59 out_voltage2_scale
-rw-rw-rw- 1 root root  4096 May 19 07:59 out_voltage3_offset
-rw-rw-rw- 1 root root  4096 May 19 07:59 out_voltage3_raw
-rw-rw-rw- 1 root root  4096 May 19 07:59 out_voltage3_scale
-rw-rw-rw- 1 root root  4096 May 19 07:59 out_voltage4_offset
-rw-rw-rw- 1 root root  4096 May 19 07:59 out_voltage4_raw
-rw-rw-rw- 1 root root  4096 May 19 07:59 out_voltage4_scale
-rw-rw-rw- 1 root root  4096 May 19 07:59 out_voltage5_offset
-rw-rw-rw- 1 root root  4096 May 19 07:59 out_voltage5_raw
-rw-rw-rw- 1 root root  4096 May 19 07:59 out_voltage5_scale
-rw-rw-rw- 1 root root  4096 May 19 07:59 out_voltage6_offset
-rw-rw-rw- 1 root root  4096 May 19 07:59 out_voltage6_raw
-rw-rw-rw- 1 root root  4096 May 19 07:59 out_voltage6_scale
-rw-rw-rw- 1 root root  4096 May 19 07:59 out_voltage7_offset
-rw-rw-rw- 1 root root  4096 May 19 07:59 out_voltage7_raw
-rw-rw-rw- 1 root root  4096 May 19 07:59 out_voltage7_scale
-rw-rw-rw- 1 root root  4096 May 19 07:59 out_voltage8_offset
-rw-rw-rw- 1 root root  4096 May 19 07:59 out_voltage8_raw
-rw-rw-rw- 1 root root  4096 May 19 07:59 out_voltage8_scale
-rw-rw-rw- 1 root root  4096 May 19 07:59 out_voltage9_offset
-rw-rw-rw- 1 root root  4096 May 19 07:59 out_voltage9_raw
-rw-rw-rw- 1 root root  4096 May 19 07:59 out_voltage9_scale
-rw-rw-rw- 1 root root  4096 May 19 07:59 out_voltage_sampling_frequency
drwxrwxrwx 2 root root     0 May 19 07:59 power
-rw-rw-rw- 1 root root  8192 May 19 07:59 profile_config
lrwxrwxrwx 1 root root     0 May 19 09:05 subsystem -> ../../../../../../../../bus/iio
-rw-rw-rw- 1 root root  4096 May 19 07:59 uevent

Additional AD9375 specific attributes

-rw-rw-rw- 1 root root  4096 May 31 14:49 calibrate_clgc_en
-rw-rw-rw- 1 root root  4096 May 31 14:49 calibrate_dpd_en
-rw-rw-rw- 1 root root  4096 May 31 14:49 calibrate_vswr_en

-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage0_clgc_current_gain
-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage0_clgc_desired_gain
-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage0_clgc_orx_rms
-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage0_clgc_status
-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage0_clgc_track_count
-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage0_clgc_tracking_en
-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage0_clgc_tx_gain
-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage0_clgc_tx_rms

-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage0_dpd_actuator_en
-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage0_dpd_external_path_delay
-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage0_dpd_model_error
-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage0_dpd_reset_en
-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage0_dpd_status
-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage0_dpd_track_count
-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage0_dpd_tracking_en

-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage0_vswr_forward_gain
-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage0_vswr_forward_gain_imag
-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage0_vswr_forward_gain_real
-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage0_vswr_forward_orx
-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage0_vswr_forward_tx
-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage0_vswr_reflected_gain
-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage0_vswr_reflected_gain_imag
-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage0_vswr_reflected_gain_real
-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage0_vswr_reflected_orx
-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage0_vswr_reflected_tx
-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage0_vswr_status
-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage0_vswr_track_count
-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage0_vswr_tracking_en

-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage1_clgc_current_gain
-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage1_clgc_desired_gain
-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage1_clgc_orx_rms
-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage1_clgc_status
-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage1_clgc_track_count
-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage1_clgc_tracking_en
-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage1_clgc_tx_gain
-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage1_clgc_tx_rms

-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage1_dpd_actuator_en
-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage1_dpd_external_path_delay
-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage1_dpd_model_error
-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage1_dpd_reset_en
-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage1_dpd_status
-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage1_dpd_track_count
-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage1_dpd_tracking_en

-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage1_vswr_forward_gain
-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage1_vswr_forward_gain_imag
-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage1_vswr_forward_gain_real
-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage1_vswr_forward_orx
-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage1_vswr_forward_tx
-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage1_vswr_reflected_gain
-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage1_vswr_reflected_gain_imag
-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage1_vswr_reflected_gain_real
-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage1_vswr_reflected_orx
-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage1_vswr_reflected_tx
-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage1_vswr_status
-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage1_vswr_track_count
-rw-rw-rw- 1 root root  4096 May 31 14:49 out_voltage1_vswr_tracking_en

Show device name

This specifies any shell prompt running on the target

root:/sys/bus/iio/devices/iio:device3> cat name
ad9371-phy

Enable State Machine Controls

The AD9371 transceiver includes an Enable State Machine (ENSM), allowing real time control over the current state of the device. The ENSM has two possible control methods – SPI control (writing ensm_mode), and pin control.

This specifies any shell prompt running on the target

root@analog:/sys/bus/iio/devices/iio:device3# cat ensm_mode_available 
radio_on radio_off

This specifies any shell prompt running on the target

root:/sys/bus/iio/devices/iio:device3> cat ensm_mode
radio_on

root:/sys/bus/iio/devices/iio:device3> echo radio_off > ensm_mode
root:/sys/bus/iio/devices/iio:device3> cat ensm_mode
radio_off

Local Oscillator Control (LO)

The AD9371 contains three fractional-N PLLs to generate the RF LOs used by the transmitter, receiver, and observation receiver. The tuning range supported by this driver covers 300MHz to 6GHz.

  • out_altvoltage0_RX_LO_frequency
  • out_altvoltage1_TX_LO_frequency
  • out_altvoltage2_RX_SN_LO_frequency

This specifies any shell prompt running on the target

 cat out_altvoltage0_RX_LO_frequency
2400000000
root:/sys/bus/iio/devices/iio:device3> echo 2450000000 >  out_altvoltage0_RX_LO_frequency
root:/sys/bus/iio/devices/iio:device3> cat out_altvoltage0_RX_LO_frequency
2450000000

This specifies any shell prompt running on the target

root:/sys/bus/iio/devices/iio:device3> cat out_altvoltage1_TX_LO_frequency
2450000000

Filter and Signal Path Configuration

Profiles

AD9371 uses profiles to designate different device configuration settings for the Tx/Rx/ORx/SnRx channels. When selecting a profile, note that Rx1 and Rx2 use the same profile; Tx1 and Tx2 use the same profile; ORx1 and ORx2 use the same profile; and SnRxA, SnRxB, and SnRxC use the same profile. The profile dictates how the digital filters, analog filters, clock rates, and clock dividers are configured in the device. Some specific parameters set by profiles include the IQ data rate, ADC clock rate, analog filter corners, FIR filter coefficients, and interpolation/decimation factors in the half band filters. Several profiles can be examined in the AD9371 Transceiver Evaluation Software for given device clock frequencies. If the desired profile exists in the software, it is recommended to setup the desired profile in and use the data structure values generated by the “Create Config.c File” button for the Tx/Rx/ORx/SnRx profile data structures. Custom profiles can be generated using other ADI software tools not described here MATLAB Profile/Filter Generator for AD9371.

Loading a Profile

This specifies any shell prompt running on the target

root@analog:/sys/bus/iio/devices/iio:device3# cat /usr/local/mykonos/profiles/lte20.txt > profile_config 
root@analog:/sys/bus/iio/devices/iio:device3# 

RX Signal Path

The AD9371 contains dual receiver channels. Each Rx channel is a direct conversion system that contains a programmable attenuator stage, followed by matched I and Q mixers that down convert received signals to baseband for digitization. To achieve gain control, a programmed gain index map is implemented. This gain map distributes attenuation among the various Rx blocks for optimal performance at each power level. In addition, support is available for both automatic and manual gain control modes. The receiver includes S-? ADCs and adjustable sample rates that produce data streams from the received signals. The signals can be conditioned further by a series of decimation filters and a fully programmable 72-tap FIR filter with additional decimation settings. The sample rate of each digital filter block is adjustable by changing the decimation factors to produce the desired output data rate.

Querying the RX Sample Rate and Primary Signal Bandwidth

This specifies any shell prompt running on the target

root:/sys/bus/iio/devices/iio:device3> cat in_voltage0_sampling_frequency
122880000
root@analog:/sys/bus/iio/devices/iio:device3# cat in_voltage0_rf_bandwidth 
100000000

Observation RX Signal Path

The ORx operates in a similar manner to the main receivers. Each input is differential and uses a dedicated mixer. The ORx inputs share a baseband ADC and baseband section; therefore, only one can be active at any time. The mixed signal and digital section is identical in design and operation to the main receiver channels. This channel can monitor the Tx channels and implement error correction functions. It can also be used as a general-purpose receiver.

Querying the ORx Sample Rate

This specifies any shell prompt running on the target

root@analog:/sys/bus/iio/devices/iio:device3# cat in_voltage2_sampling_frequency 
245760000
root@analog:/sys/bus/iio/devices/iio:device3# cat in_voltage2_rf_bandwidth
200000000

Setting the Observation Path Source

When the ARM radio control is in ARM command mode, this attribute allows the user to selectively power-up or power-down the desired ObsRx data path.

  • OFF - SnRx path is disabled
  • ORX1_TX_LO – SnRx operates in observation mode on ORx1 with Tx LO synthesizer
  • ORX2_TX_LO – SnRx operates in observation mode on ORx2 with Tx LO synthesizer
  • INTERNALCALS – enables scheduled Tx calibrations while using SnRx path. The enableTrackingCals function needs to be called in RADIO_OFF state. It sets the calibration mask, which the scheduler will later use to schedule the desired calibrations. This command is issued in RADIO_OFF. Once the AD9371 moves to RADIO_ON state, the internal scheduler will use the enabled calibration mask to schedule calibrations whenever possible, based on the state of the transceiver. The Tx calibrations will not be scheduled until INTERNALCALS is selected and the Tx calibrations are enabled in the cal mask.
  • OBS_SNIFFER – SnRx operates in sniffer mode with latest selected Sniffer Input – for hardware pin control operation. In pin mode, the GPIO pins designated for ORX_MODE would select SNIFFER mode. Then MYKONOS_setSnifferChannel function would choose the channel.
  • ORX1_SN_LO – SnRx operates in observation mode on ORx1 with SNIFFER LO synthesizer
  • ORX2_SN_LO – SnRx operates in observation mode on ORx2 with SNIFFER LO synthesizer
  • SN_A – SnRx operates in sniffer mode on SnRxA with SNIFFER LO synthesizer
  • SN_B – SnRx operates in sniffer mode on SnRxB with SNIFFER LO synthesizer
  • SN_C – SnRx operates in sniffer mode on SnRxC with SNIFFER LO synthesizer

This specifies any shell prompt running on the target

root@analog:/sys/bus/iio/devices/iio:device3# cat in_voltage_rf_port_select_available 
OFF INTERNALCALS OBS_SNIFFER SN_A SN_B SN_C ORX1_TX_LO ORX2_TX_LO ORX1_SN_LO ORX2_SN_LO 

root@analog:/sys/bus/iio/devices/iio:device3# echo ORX1_TX_LO > in_voltage2_rf_port_select

root@analog:/sys/bus/iio/devices/iio:device3# cat in_voltage2_rf_port_select
ORX1_TX_LO

TX Signal Path

The AD9371 employs a direct conversion transmitter architecture consisting of two identical and independently controlled channels that provide all the digital processing, mixed signal, and RF blocks necessary to implement a direct conversion system. Both channels share a common frequency synthesizer. The digital data from the JESD204B lanes pass through a fully programmable 96-tap FIR filter with optional interpolation. The FIR output is sent to a series of conversion filters that provide additional filtering and data rate interpolation prior to reaching the DAC. Each DAC has an adjustable sample rate and is linear up to full scale. Once converted to baseband analog signals, the in-phase (I) and quadrature (Q) signals are filtered to remove sampling artifacts, and then the signals are fed to the upconversion mixers. At the mixer stage, the I and Q signals are recombined and modulated onto the carrier frequency for transmission to the output stage. Each transmit chain provides a wide attenuation adjustment range with fine granularity to help designers optimize SNR.

Querying the TX Sample Rate and Primary Signal Bandwidth

This specifies any shell prompt running on the target

root:/sys/bus/iio/devices/iio:device3> cat out_voltage_sampling_frequency
245760000
root@analog:/sys/bus/iio/devices/iio:device3# cat out_voltage0_rf_bandwidth 
75000000

RX Gain Control

The AD9371 main receivers (Rx1, Rx2) and sniffer receivers (SnRxA, SnRxB, SnRxC) feature automatic and manual gain control modes that provide flexible gain control in a wide array of applications. Observation receivers (ORx1, ORx2) feature Manual Gain Control (MGC) only. Automatic Gain Control (AGC) allows the receivers to autonomously adjust receiver gain depending on variations of the input signal, such as the onset of a strong interferer overloading the receiver data path. All the receivers are also capable of operating in MGC mode where changes in gain are initiated by the Baseband Processor (BBP) over SPI or GPIO.

The default gain tables can be found in the mykonos_user.c file, and are loaded by default. Custom gain tables can be loaded automatically during driver probe or anytime later via the gain_table_config sysfs attribute. Tables must be stored in the /lib/firmware folder, or compiled into the kernel using the CONFIG_FIRMWARE_IN_KERNEL, CONFIG_EXTRA_FIRMWARE config options. The table loaded during driver probe can be specified using following device tree property:

adi,gaintable-name = “ad9371_std_gaintable”;

In case no table is specified or loaded, the driver will continue to use the provided standard gain tables.

Gain tables are stored in a human readable file, with the format specified below.

Example: ad9371_std_gaintable

<list>
 <gaintable AD9371 type=FULL dest=[1|2|3|4|5] start=FREQUENCY1_Hz end=FREQUENCY2_Hz>
  gain_in_mdB, IntAttnWord, ExtAttnWord, DigGainAttenWord, DigAttenEn /* index 255 */
  gain_in_mdB, IntAttnWord, ExtAttnWord, DigGainAttenWord, DigAttenEn /* index 254 */
  gain_in_mdB, IntAttnWord, ExtAttnWord, DigGainAttenWord, DigAttenEn /* index 253 */
  gain_in_mdB, IntAttnWord, ExtAttnWord, DigGainAttenWord, DigAttenEn /* index 252 */
 
 …
 </gaintable>

...

</list>

Assumptions:

  • Gain tables must be monotonic
  • The format of the columns in the Rx and ORx gain table rows are: {gain_in_mdB, Internal Attenuator Word, External Attenuator Word, Digital Gain/Atten Word, Digital Attenuation Enable}
  • gain_in_mdB: is the absolute Gain in mdB (signed int format)
  • end must be greater than start frequency (in Hz)
  • There must be sufficient tables provided to support the entire used tuning range
  • dest specifies the targeted RX. (1 = RX1, 2=RX2, 3=RX1 and RX2, 4=ORX, 5=SNRX )

Loading a gain table

This specifies any shell prompt running on the target

root@analog:/sys/bus/iio/devices/iio:device3# ls /lib/firmware/ad9*
ad9371_std_gaintable

root@analog:/sys/bus/iio/devices/iio:device3# cat /lib/firmware/ad9371_std_gaintable > gain_table_config

Gain control modes

The AD9371 Rx supports three modes of gain control. These modes are described in brief below:

Mode Description
Manual Gain Control (MGC) Provides the user full control over the current gain index. In MGC, the gain index can be controlled in two ways: through API commands and through GPIO signaling.
Hybrid Mode When the user sends a pulse to a GPIO pin enabled as the Hybrid Mode Gain Change pin, the AGC overload counters are polled to determine if a gain increase or decrease is necessary. When the pulse is registered by the gain control block a gain increase is made in the case of an underrange scenario, a gain decrease is made in the case of an overrange signal, or no gain change is made. This mode allows the user to determine when gain changes occur. The Hybrid Mode is a subset of AGC as Hybrid Mode uses many of the same circuits, thresholds, and counter parameters as AGC.
Automatic Gain Control (AGC) The AGC will determine when gain changes should be made. There are several configurations that can be used in AGC. Examples include the option to reduce gain as soon as an overrange has been detected (fast attack mode), change gain (if necessary) only at the expiry of a variable length counter (AGC gain update counter, operating without fast attack), synchronization of the counter to an external pulse (AGC enable sync pulse), and others. .

TIP:

  • Automatic Gain Control (AGC) and Hybrid Mode are available on RX1, RX2 and in OBS_SNIFFER, SN_A, SN_B and SN_C Observation Path Sources. (see in_voltage2_rf_port_select).
  • In ORX1_TX_LO, ORX2_TX_LO, ORX1_SN_LO, ORX2_SN_LO modes only MGC mode is available.


This specifies any shell prompt running on the target

root@analog:/sys/bus/iio/devices/iio:device3# cat in_voltage_gain_control_mode_available 
manual automatic hybrid

Querying or Setting a Gain Control Mode

This specifies any shell prompt running on the target

root:/sys/bus/iio/devices/iio:device3> cat in_voltage0_gain_control_mode
automatic
root:/sys/bus/iio/devices/iio:device3> echo manual > in_voltage0_gain_control_mode
root:/sys/bus/iio/devices/iio:device3> cat in_voltage0_gain_control_mode
manual

This specifies any shell prompt running on the target

root:/sys/bus/iio/devices/iio:device3> cat in_voltage1_gain_control_mode
automatic

Reading the current Gain

Supported in all available Gain control modes

This specifies any shell prompt running on the target

root:/sys/bus/iio/devices/iio:device3> cat in_voltage0_hardwaregain
30.000000 dB

This specifies any shell prompt running on the target

root:/sys/bus/iio/devices/iio:device3> cat in_voltage1_hardwaregain
30.000000 dB

MGC setting the current Gain

Only available in Manual Gain Control Mode (MGC)

Attribute Data Path
in_voltage0_hardwaregain RX1
in_voltage1_hardwaregain RX2
in_voltage2_hardwaregain OBS1 if in_voltage2_rf_port_select == ORX1_TX_LO or ORX1_SN_LO
in_voltage2_hardwaregain OBS2 if in_voltage2_rf_port_select == ORX2_TX_LO or ORX2_SN_LO
in_voltage2_hardwaregain OBS_SNIFFER if in_voltage2_rf_port_select == OBS_SNIFFER or SN_A, SN_B, SN_C

This specifies any shell prompt running on the target

root:/sys/bus/iio/devices/iio:device3> echo 20 > in_voltage0_hardwaregain
root:/sys/bus/iio/devices/iio:device3> cat in_voltage0_hardwaregain
20.000000 dB

Tx Attenuation Control

The TX attenuation/gain can be individually controlled for TX1 and TX2. The range is from 0 to -41.95 dB in programmable steps sizes. The nomenclature used here is gain instead of attenuation, so all values are expressed negative.

This specifies any shell prompt running on the target

root:/sys/bus/iio/devices/iio:device3> cat out_voltage0_hardwaregain
-10.000000 dB
root:/sys/bus/iio/devices/iio:device3> echo -40.25 >  out_voltage0_hardwaregain
root:/sys/bus/iio/devices/iio:device3> cat out_voltage0_hardwaregain
-40.250000 dB

This specifies any shell prompt running on the target

root:/sys/bus/iio/devices/iio:device3> cat out_voltage1_hardwaregain
-10.000000 dB

Received Signal Strength Indicator (RSSI)

This attribute will report RSSI - however currently it reports Decimated Power instead.

This specifies any shell prompt running on the target

root:/sys/bus/iio/devices/iio:device3> cat in_voltage0_rssi
12.75 dB

Calibration Tracking Controls

Tracking Calibrations: The ARM processor is tasked with ensuring that Quadrature Error Correction (QEC) and Local Oscillator Leakage (LOL) corrections are optimal throughout device operation, i.e. over time, attenuation, and temperature. It achieves this by performing calibrations at regular intervals. These calibrations are termed “tracking calibrations”, and utilize normal traffic data to update the path correction coefficients.

The host must set the ORx path source to INTERNALCALS by setting in_voltage2_rf_port_select. Setting the ORx path source to INTERNALCALS enables scheduling of regular tracking radio calibrations, such as Tx QEC and Tx local oscillator leakage (LOL) tracking along with DPD tracking. See the Observation Receiver (ORx) section for ORx channel setup details.

Writing 0, N or 1, Y to the below attributes either disables or enables the corresponding tracking option.

  • in_voltage0_quadrature_tracking_en
  • in_voltage1_quadrature_tracking_en
  • out_voltage0_lo_leakage_tracking_en
  • out_voltage0_quadrature_tracking_en
  • out_voltage1_lo_leakage_tracking_en
  • out_voltage1_quadrature_tracking_en
  • out_voltage0_dpd_tracking_en (AD9375 only)
  • out_voltage1_dpd_tracking_en (AD9375 only)
  • out_voltage0_clgc_tracking_en (AD9375 only)
  • out_voltage1_clgc_tracking_en (AD9375 only)
  • out_voltage0_vswr_tracking_en (AD9375 only)
  • out_voltage1_vswr_tracking_en (AD9375 only)

This specifies any shell prompt running on the target

root:/sys/bus/iio/devices/iio:device3> cat in_voltage_quadrature_tracking_en
1
root:/sys/bus/iio/devices/iio:device3> echo 0 > in_voltage0_quadrature_tracking_en
root:/sys/bus/iio/devices/iio:device3> cat in_voltage0_quadrature_tracking_en
0

AuxADC Reading

The AD9371 contains an auxiliary ADC that is multiplexed to four input pins (AUXADC_0 through AUXADC_3). This block can monitor system voltages without adding additional components. The auxiliary ADC is 12 bits with an input voltage range of 0.05 V to VDDA_3P3 - 0.05 V. When enabled, the auxiliary ADC is free running. Software reads of the output value provide the last value latched at the ADC output. TheAuxiliary ADCs can be read like any other IIO ADC.

Attributes are:

  • in_voltage3_offset
  • in_voltage3_raw
  • in_voltage3_scale

To obtain the reading in mV calculate: (in_voltage3_raw + in_voltage3_offset) * in_voltage3_scale

This specifies any shell prompt running on the target

root:/sys/bus/iio/devices/iio:device3> grep “” in_voltage3_*
in_voltage3_offset:45
in_voltage3_raw:66
in_voltage3_scale:0.775194

AuxDAC Writing

The AD9371 contains ten identical auxiliary DACs (AUXDAC_0 to AUXDAC_9) that can supply bias voltages, analog control voltages, or other system functionality. TheAuxiliary DACs can be accessed like any other IIO DAC.

Attributes are:

  • out_voltage2_raw
  • out_voltage2_scale
  • out_voltage3_raw
  • out_voltage3_scale

This specifies any shell prompt running on the target

root:/sys/bus/iio/devices/iio:device3> grep “” out_voltage2*
out_voltage2_offset:204
out_voltage2_raw:0
out_voltage2_scale:1.560671
root:/sys/bus/iio/devices/iio:device3> echo 1000 > out_voltage2_raw

Digital Predistortion Control (DPD) (AD9375 only)

The DPD is a feature available on the AD9375 that enables users to achieve higher power amplifier (PA) efficiency while still meeting adjacent channel leakage ratio (ACLR) requirements in the Tx signal chain for compliance with 3GPP and European Telecommunications Standards Institute (ETSI) standards for LTE and other technologies. The DPD works on the principle of predistorting the Tx data to cancel distortion caused by PA compression.

For more details please consult the AD9371/AD9375 System Development User Guide UG-992

DPD Tracking Controls

This control enabled the DPD tracking calibration. The user must set the ORx path source to INTERNALCALS by setting in_voltage2_rf_port_select.

Also see: Calibration tracking controls

Writing 0, N or 1, Y to the below attributes either disables or enables the corresponding tracking option.

  • out_voltage0_dpd_tracking_en
  • out_voltage1_dpd_tracking_en

This specifies any shell prompt running on the target

root:/sys/bus/iio/devices/iio:device3> cat out_voltage0_dpd_tracking_en
0
root:/sys/bus/iio/devices/iio:device3> echo 1 > out_voltage0_dpd_tracking_en
root:/sys/bus/iio/devices/iio:device3> cat out_voltage0_dpd_tracking_en
1

DPD Actuator Control

This control allows the user to bypass the DPD actuator on a given Tx channel. This control can be called in the radioOn state. However, it is recommended that the user suspend (pause) the DPD calibration before using this control to synchronize all internal ARM scheduler tasks. The DPD calibration can be resumed when this control has been successfully executed.

Writing 0, N or 1, Y to the below attributes either disables or enables the corresponding tracking option.

  • out_voltage0_dpd_actuator_en
  • out_voltage1_dpd_actuator_en

This specifies any shell prompt running on the target

root:/sys/bus/iio/devices/iio:device3>  cat out_voltage0_dpd_actuator_en
0
root:/sys/bus/iio/devices/iio:device3> echo 1 > out_voltage0_dpd_actuator_en
root:/sys/bus/iio/devices/iio:device3> cat out_voltage0_dpd_actuator_en
1

DPD Reset Control

This control allows the user to reset the DPD actuator on a given Tx channel. This control can be called in the radioOn state. However, it is recommended that the user suspend (pause) the DPD calibration before using this control to synchronize all internal ARM scheduler tasks. The DPD calibration can be resumed when this control has been successfully executed.

Writing 0, N or 1, Y to the below attributes either disables or enables the corresponding tracking option.

  • out_voltage0_dpd_reset_en
  • out_voltage1_dpd_reset_en

This specifies any shell prompt running on the target

root:/sys/bus/iio/devices/iio:device3> cat out_voltage0_dpd_reset_en
0
root:/sys/bus/iio/devices/iio:device3> echo 1 > out_voltage0_dpd_reset_en
root:/sys/bus/iio/devices/iio:device3> cat out_voltage0_dpd_reset_en
1

DPD Status

This control reads back the DPD calibration status from the ARM processor.

  • out_voltage0_dpd_status
  • out_voltage1_dpd_status
Value Description
0 No Error
1 Error: ORx disabled
2 Error: Tx disabled
3 Error: DPD initialization not run
4 Error: Path delay not setup
5 Error: ORx signal too low
6 Error: ORx signal saturated
7 Error: Tx signal too low
8 Error: Tx signal saturated
9 Error: Model error high
10 Error: AM AM outliers
11 Error: Invalid Tx profile
12 Error: ORx QEC Disabled

This specifies any shell prompt running on the target

root:/sys/bus/iio/devices/iio:device3> cat out_out_voltage0_dpd_status
0

DPD Model Error

This control reads back the percent error of the PA model ×10 to include 1 decimal place.

  • out_voltage0_dpd_model_error
  • out_voltage1_dpd_model_error

This specifies any shell prompt running on the target

root:/sys/bus/iio/devices/iio:device3> cat out_voltage0_dpd_model_error
120

DPD External Path Delay

This control reads back the external path delay from Tx output to ORx input, at 1/16 sample resolution of the ORx sample rate. Calculate true value by dividing this member.

  • out_voltage0_dpd_external_path_delay
  • out_voltage1_dpd_external_path_delay

This specifies any shell prompt running on the target

root:/sys/bus/iio/devices/iio:device3> cat out_voltage0_dpd_external_path_delay
2326

DPD Tracking Count

This control reads back the number of times the DPD has successfully run since DPD initialization calibration.

  • out_voltage0_dpd_track_count
  • out_voltage1_dpd_track_count

This specifies any shell prompt running on the target

root:/sys/bus/iio/devices/iio:device3> cat out_voltage0_dpd_track_count
42

Closed-Loop Gain Control (CLGC) (AD9375 only)

The closed-loop gain control (CLGC) feature in the AD9375 enables a constant gain level to be maintained at the ORx input (total gain from Tx output to ORx input) which translates to a constant output power (POUT) at the power amplifier (PA) for a given digital input level. The gain level is controlled by modifying the Tx attenuation and by specifying a desired loop gain value (here, gain means the net loop gain and attenuation combined, including all transceiver gain and attenuation blocks on-chip). Note that the CLGC must be enabled to establish the total desired loop gain in the system.

For more details please consult the AD9371/AD9375 System Development User Guide UG-992

CLGC Tracking Controls

This control enabled the CLGC tracking calibration. The user must set the ORx path source to INTERNALCALS by setting in_voltage2_rf_port_select.

Also see: Calibration tracking controls

Writing 0, N or 1, Y to the below attributes either disables or enables the corresponding tracking option.

  • out_voltage0_clgc_tracking_en
  • out_voltage1_clgc_tracking_en

This specifies any shell prompt running on the target

root:/sys/bus/iio/devices/iio:device3> cat out_voltage0_clgc_tracking_en
0
root:/sys/bus/iio/devices/iio:device3> echo 1 > out_voltage0_clgc_tracking_en
root:/sys/bus/iio/devices/iio:device3> cat out_voltage0_clgc_tracking_en
1

CLGC Desired Gain

This control configures the tx1DesiredGain/tx2DesiredGain parameter

Desired loop gain (can be negative if total attenuation is greater than amplification) from Tx output to ORx input. Desired GaindB = desiredGain/100

  • out_voltage0_clgc_desired_gain
  • out_voltage1_clgc_desired_gain

This specifies any shell prompt running on the target

root:/sys/bus/iio/devices/iio:device3> cat out_voltage0_clgc_desired_gain
-20000
root:/sys/bus/iio/devices/iio:device3> echo -6000 > out_voltage0_clgc_desired_gain
root:/sys/bus/iio/devices/iio:device3> cat out_voltage0_clgc_desired_gain
-6000

CLGC Current Gain

This control returns the

Current measured gain in 1/100ths dB scale. Current GaindB = currentGain/100

  • out_voltage0_clgc_current_gain
  • out_voltage1_clgc_current_gain

This specifies any shell prompt running on the target

root:/sys/bus/iio/devices/iio:device3> cat out_voltage0_clgc_current_gain
-19956

CLGC Tx Gain

This control returns the current Tx attenuation setting for a given channel in 0.05 dB resolution, as determined by the CLGC algorithm. However, this value is written to by the CLGC algorithm and may differ slightly from Tx attenuation returned by out_voltage0_hardwaregain/out_voltage1_hardwaregain due to these actions not being synchronous. Tx AttenuationdB = txGain/200

  • out_voltage0_clgc_tx_gain
  • out_voltage1_clgc_tx_gain

This specifies any shell prompt running on the target

root:/sys/bus/iio/devices/iio:device3> cat out_voltage0_clgc_tx_gain
4050

CLGC RMS Tx digital sample power

This control returns the RMS Tx digital sample power measured at the output of the DPD actuator. Measurement resolution is 0.01 dB. Prms dBFS = txRms/100.

  • out_voltage0_clgc_tx_rms
  • out_voltage1_clgc_tx_rms

This specifies any shell prompt running on the target

root:/sys/bus/iio/devices/iio:device3> cat out_voltage0_clgc_tx_rms
-1225

CLGC RMS ORx digital sample power

This control returns the RMS ORx digital sample power measured within the DPD block on the ORx side. Measuremen resolution is 0.01 dB. Prms dBFS = orxRms/100.

  • out_voltage0_clgc_orx_rms
  • out_voltage1_clgc_orx_rms

This specifies any shell prompt running on the target

root:/sys/bus/iio/devices/iio:device3> cat out_voltage0_clgc_orx_rms
-3214

CLGC Status

This control reads back the CLGC calibration status from the ARM processor.

  • out_voltage0_clgc_status
  • out_voltage1_clgc_status
Value Description
0 No Error
1 Error: TX is disabled
2 Error: ORx is disabled
3 Error: Loopback switch is closed
4 Error: Data measurement aborted during capture
5 Error: No initial calibration was done
6 Error: Path delay not setup
7 Error: No apply control is possible
8 Error: Control value is out of range
9 Error: CLGC feature is disabled
10 Error: TX attenuation is capped
11 Error: Gain measurement
12 Error: No GPIO configured in single ORx configuration
13 Error: Tx is not observable with any of the ORx Channels

This specifies any shell prompt running on the target

root:/sys/bus/iio/devices/iio:device3> cat out_voltage0_clgc_status
0

CLGC Tracking Count

This control reads back the number of times the CLGC has successfully run since CLGC initialization calibration.

  • out_voltage0_clgc_track_count
  • out_voltage1_clgc_track_count

This specifies any shell prompt running on the target

root:/sys/bus/iio/devices/iio:device3> cat out_voltage0_clgc_track_count
42

Voltage Standing Wave Ratio (VSWR) Measurement, (AD9375 only)

The voltage standing wave ratio (VSWR) on a transmission line is defined as the ratio of the voltage maxima to the voltage minima along the line. The VSWR measurement feature in the AD9375 facilitates the computation of this quantity by means of using the ORx path that is time multiplexed to measure both the forward and reflected voltages.

For more details please consult the AD9371/AD9375 System Development User Guide UG-992

VSWR Tracking Controls

This control enables voltage standing wave ratio (VSWR) measurement. The user must set the ORx path source to INTERNALCALS by setting in_voltage2_rf_port_select.

Also see: Calibration tracking controls

Writing 0, N or 1, Y to the below attributes either disables or enables the corresponding tracking option.

  • out_voltage0_vswr_tracking_en
  • out_voltage1_vswr_tracking_en

This specifies any shell prompt running on the target

root:/sys/bus/iio/devices/iio:device3> cat out_voltage0_vswr_tracking_en
0
root:/sys/bus/iio/devices/iio:device3> echo 1 > out_voltage0_vswr_tracking_en
root:/sys/bus/iio/devices/iio:device3> cat out_voltage0_vswr_tracking_en
1

VSWR Status

This control reads back the VSWR calibration status from the ARM processor.

  • out_voltage0_vswr_status
  • out_voltage1_vswr_status
Value Description
0 No Error
1 Error: TX disabled
2 Error: ORx disabled
3 Error: Loopback switch is closed
4 Error: No initial calibration was done
5 Error: Path delay not setup
6 Error: Data capture aborted
7 Error: VSWR is disabled
8 Error: Entering Cal
9 Error: No GPIO configured in single ORx configuration
10 Error: Tx is not observable with any of the ORx Channels

This specifies any shell prompt running on the target

root:/sys/bus/iio/devices/iio:device3> cat out_voltage0_vswr_status
0

VSWR Tracking Count

This control reads back the number of times the VSWR has successfully run since VSWR initialization calibration.

  • out_voltage0_vswr_track_count
  • out_voltage1_vswr_track_count

This specifies any shell prompt running on the target

root:/sys/bus/iio/devices/iio:device3> cat out_voltage0_vswr_track_count
54

VSWR Measurements

These controls provide various measurements. Elements are only listed for out_voltage0 but apply likewise for out_voltage1 as well.

Device file Description
out_voltage0_vswr_forward_gain Forward rms gain measured from Tx to ORx path (1 = 0.01 dB gain)
out_voltage0_vswr_forward_gain_imag Imaginary part of the forward path complex gain (1 = 0.01 linear gain)
out_voltage0_vswr_forward_gain_real Real part of the forward path complex gain (1 = 0.01 linear gain)
out_voltage0_vswr_forward_orx RMS ORx digital sample power measured at the DPD block for t.he ORx data in the forward measurement mode. Measurement resolution is 0.01 dB. Expect a 21 dB offset from the JESD204B dBFS value as well as from the txRms data reported by the CLGC. Prms dBFS = orxRms/100 +21 dB
out_voltage0_vswr_forward_tx RMS Tx digital sample power measured at the output of the DPD actuator in the forward measurement mode. Measurement resolution is 0.01 dB. Expect a 21 dB offset from the JESD204B dBFS value as well as from the txRms data reported by the CLGC. Prms dBFS = txRms/100 +21 dB
out_voltage0_vswr_reflected_gain Measured reflected path gain in rms (1 = 0.01 dB gain)
out_voltage0_vswr_reflected_gain_imag Imaginary part of the reflected path complex gain (1 = 0.01 linear gain)
out_voltage0_vswr_reflected_gain_real Real part of the reflected path complex gain (1 = 0.01 linear gain)
out_voltage0_vswr_reflected_orx RMS ORx digital sample power measured at the DPD block for the ORx data in the reverse measurement mode. Measurement resolution is 0.01 dB. Expect a 21 dB offset from the JESD204B dBFS value as well as from the orxRms data reported by the CLGC. Prms dBFS = orxRms/100 +21 dB
out_voltage0_vswr_reflected_tx RMS Tx digital sample power measured at the output of the DPD actuator for the reverse measurement. Measurement resolution is 0.01 dB. Expect a 21 dB offset from the JESD204B dBFS value as well as from the txRms data reported by the CLGC. Prms dBFS = txRms/100 +21 dB

This specifies any shell prompt running on the target

root:/sys/bus/iio/devices/iio:device3> cat out_voltage0_vswr_reflected_gain
123

Advanced Debug Facilities

The AD9371 driver supports a number of advanced debug controls via the kernel debugfs. How these device files/controls can be used is described here. The AD9371 Advanced Plugin directly controls these and adds a user friendly interface.

Runtime Device Driver Customization

There is a large number of AD9371 Device Driver Customization options available. Typically these are supplied via Devicetree. However for debug and evaluation purposes these can be changed during runtime. Please note that changes will be lost if the device is unbinded or the platform is rebooted. Changes will only take affect once the initialize attribute is written 1. It should also be noted that the AD9371 will take a RESET, so current settings done via the main IIO API will be lost. Accessing debugfs requires root privileges. Only device files prefixed with adi, are AD9371 Device Driver Customization Options.

In order to identify if the IIO device in question (ad9371-phy) you first need to identify the IIO device number. Therefore read the name attribute of each IIO device

This specifies any shell prompt running on the target

root@analog:~# grep "" /sys/bus/iio/devices/iio\:device*/name
/sys/bus/iio/devices/iio:device0/name:ad7291
/sys/bus/iio/devices/iio:device1/name:xadc
/sys/bus/iio/devices/iio:device2/name:ad9528-1
/sys/bus/iio/devices/iio:device3/name:ad9371-phy
/sys/bus/iio/devices/iio:device4/name:axi-ad9371-rx-obs-hpc
/sys/bus/iio/devices/iio:device5/name:axi-ad9371-tx-hpc
/sys/bus/iio/devices/iio:device6/name:axi-ad9371-rx-hpc
root@analog:~# 

Change directory to /sys/kernel/debug/iio/ iio:deviceX.

This specifies any shell prompt running on the target

root@analog:~# cd /sys/kernel/debug/iio/iio\:device3
root@analog:/sys/kernel/debug/iio/iio:device3# ls 
[--snip--]
adi,tx-settings-tx-atten-step-size
adi,tx-settings-tx-channels-enable
adi,tx-settings-tx-pll-lo-frequency_hz
adi,tx-settings-tx-pll-use-external-lo
adi,tx-settings-tx1-atten_mdb
adi,tx-settings-tx2-atten_mdb
bist_prbs_obs
bist_prbs_rx
bist_tone
direct_reg_access
initialize
loopback_tx_obs
loopback_tx_rx

Example to change from internal to external TX LO

This specifies any shell prompt running on the target

root@analog:/sys/kernel/debug/iio/iio:device3# cat adi,tx-settings-tx-pll-use-external-lo
0

root@analog:/sys/kernel/debug/iio/iio:device3# echo 1 > adi,tx-settings-tx-pll-use-external-lo
root@analog:/sys/kernel/debug/iio/iio:device3# echo 1 > initialize 

Build-In Self-Test (BIST)

Controling these attribute files directly take effect and therefore don’t require the initialize sequence. Test functionality exposed here is only meant to route or inject test patterns/data than can be used to validate the Digital Interface or functionality of the device.

BIST Tone

Digital numerically controlled oscillator (NCO) to create a CW test tone on the Tx1 and Tx2 RF outputs. The TxAttenuation is forced in this function to max analog output power, but the digital attenuation is backed off 6dB to make sure the digital filter does not clip and cause spurs in the tx spectrum.

SYNTAX:

bist_tone <Enable> <TX1 Tone Frequency in kHz> <TX2 Tone Frequency in kHz>

NCO Tone frequency Valid range from -IQrate/2 to IQrate/2

Enable
Value Function
0 Disable
1 Enable

Example: Inject 3MHz tone into TX1 and 5MHz into TX2

This specifies any shell prompt running on the target

root@analog:/sys/kernel/debug/iio/iio:device3# echo 1 3000 5000 > bist_tone 

PRBS

Pseudorandom Binary Sequence (PRBS) that can either injected into the RX or OBS path.

SYNTAX:

bist_prbs_rx <Value>
bist_prbs_obs <Value>

Injection Point
Value Function and polynomial order
0 Disable
1 PRBS7
2 PRBS15
3 PRBS31

Example: Inject PRBS15 into RX

This specifies any shell prompt running on the target

root@analog:/sys/kernel/debug/iio/iio:device3# echo 2 > bist_prbs_rx 

BIST Loopback

Allows either to digitally loopback TX data (IQ samples) into the RX or OBS path. For this to work correctly, the IQ data rate of the Tx data path must match the Rx or OBS IQ data rate.

SYNTAX:

loopback_tx_rx <Enable>
loopback_tx_obs <Enable>

Enable
Value Function
0 Disable
1 Enable

Example: Digital TX → Digital RX

This specifies any shell prompt running on the target

root@analog:/sys/kernel/debug/iio/iio:device3# echo 1 > loopback_tx_rx 

Monitor Output via GPIO

This debug attribute configures the monitor output function for the GPIOs

The monitor outputs are grouped in set of nibbles, the user can set individual nibbles for having the monitor output function across the available GPIO. In order to enable the GPIO monitor function following device tree attributes should have the proper setup:

  adi,gpio-oe-mask = <0xFF>; the first D7:D0 GPIOs will have the output enable
  adi,gpio-src-ctrl3_0 = <0>; // GPIO_MONITOR_MODE
  adi,gpio-src-ctrl7_4 = <0>; // GPIO_MONITOR_MODE

SYNTAX:

monitor_out <Monitor Index> <Monitor Mask>

Example: Enable all bits for Monitor Index: 0x01 (Name: AGC Monitor 1)

This specifies any shell prompt running on the target

root@analog:/sys/kernel/debug/iio/iio:device3# echo 1 255 > monitor_out 

Low level register access via debugfs (direct_reg_access)

Some IIO drivers feature an optional debug facility, allowing users to read or write registers directly. Special care needs to be taken when using this feature, since you can modify registers on the back of the driver.

To simplify direct register access you may want to use the libiio iio_reg command line utility.

Accessing debugfs requires root privileges.

In order to identify if the IIO device in question feature this option you first need to identify the IIO device number.

Therefore read the name attribute of each IIO device

This specifies any shell prompt running on the target

root@analog:~# grep "" /sys/bus/iio/devices/iio\:device*/name
/sys/bus/iio/devices/iio:device0/name:ad7291
/sys/bus/iio/devices/iio:device1/name:ad9361-phy
/sys/bus/iio/devices/iio:device2/name:xadc
/sys/bus/iio/devices/iio:device3/name:adf4351-udc-rx-pmod
/sys/bus/iio/devices/iio:device4/name:adf4351-udc-tx-pmod
/sys/bus/iio/devices/iio:device5/name:cf-ad9361-dds-core-lpc
/sys/bus/iio/devices/iio:device6/name:cf-ad9361-lpc
root@analog:~# 

Change directory to /sys/kernel/debug/iio/ iio:deviceX and check if the direct_reg_access file exists.

This specifies any shell prompt running on the target

root@analog:~# cd /sys/kernel/debug/iio/iio\:device1
root@analog:/sys/kernel/debug/iio/iio:device1# ls direct_reg_access 
direct_reg_access

Reading

This specifies any shell prompt running on the target

root@analog:/sys/kernel/debug/iio/iio:device1# echo 0x7 > direct_reg_access                                                                                                                                 
root@analog:/sys/kernel/debug/iio/iio:device1# cat direct_reg_access 
0x40

Writing

Write ADDRESS VALUE

This specifies any shell prompt running on the target

root@analog:/sys/kernel/debug/iio/iio:device1# echo 0x7 0x50  > direct_reg_access                                                                                                                            
root@analog:/sys/kernel/debug/iio/iio:device1# cat direct_reg_access 
0x50

Accessing HDL CORE registers

Special ADI device driver convention for devices that have both:

  • a SPI/I2C control interface
  • and some sort of HDL Core with registers (AXI)

In this case when accessing the HDL Core Registers always set BIT31.

The register map for typical ADI HDL cores can be found here: Register Map

This specifies any shell prompt running on the target

root@analog:/sys/kernel/debug/iio/iio:device6# echo 0x80000000 > direct_reg_access                                                                                                                           
root@analog:/sys/kernel/debug/iio/iio:device6# cat direct_reg_access 
0x80062

02 Mar 2011 15:16

More Information

resources/tools-software/linux-drivers/iio-transceiver/ad9371.1625214105.txt.gz · Last modified: 02 Jul 2021 10:21 by Michael Hennerich