This is an old revision of the document!
The AD9361 is a high performance, highly integrated RF Agile Transceiver™. Its programmability and wideband capability make it ideal for a broad range of transceiver applications. The device combines an RF front end with a flexible mixed-signal baseband section and integrated frequency synthesizers, simplifying design-in by providing a configurable digital interface to a processor.
This is a Linux industrial I/O (IIO) subsystem driver, targeting RF Transceivers. The industrial I/O subsystem provides a unified framework for drivers for many different types of converters and sensors using a number of different physical interfaces (i2c, spi, etc). See IIO for more information.
Function | File |
---|---|
driver | drivers/iio/adc/ad9361.c |
driver | drivers/iio/adc/ad9361_conv.c |
include | drivers/iio/adc/ad9361.h |
devicetree bindings | Documentation/devicetree/bindings/iio/adc/adi,ad9361.txt |
Function | File |
---|---|
driver | drivers/iio/adc/cf_axi_adc_core.c |
driver | drivers/iio/adc/cf_axi_adc_ring_stream.c |
include | drivers/iio/adc/cf_axi_adc.h |
Function | File |
---|---|
driver | drivers/iio/frequency/cf_axi_dds.c |
include | drivers/iio/frequency/cf_axi_dds.h |
Please follow the link here for detailed options and examples:
The AD9361 driver is a spi-bus driver and can currently only be instantiated via device tree.
Required devicetree properties:
Function | File |
---|---|
FMCOMMS2/3 Device Tree | adi-fmcomms2.dtsi |
FMCOMMS4 Device Tree | adi-fmcomms4.dtsi |
FMCOMMS5 Device Tree | adi-fmcomms5.dtsi |
Configure kernel with “make menuconfig” (alternatively use “make xconfig” or “make qconfig”)
The AD9361 driver depends on CONFIG_SPI
Configure kernel with “make menuconfig” (alternatively use “make xconfig” or “make qconfig”)
Linux Kernel Configuration Device Drivers ---> <*> Industrial I/O support ---> --- Industrial I/O support -*- Enable ring buffer support within IIO -*- Industrial I/O lock free software ring -*- Enable triggered sampling support *** Analog to digital converters *** [--snip--] <*> Analog Devices AD9467 AD9643 High-Speed AXI ADC driver [--snip--]
Each and every IIO device, typically a hardware chip, has a device folder under /sys/bus/iio/devices/iio:deviceX. Where X is the IIO index of the device. Under every of these directory folders reside a set of files, depending on the characteristics and features of the hardware device in question. These files are consistently generalized and documented in the IIO ABI documentation. In order to determine which IIO deviceX corresponds to which hardware device, the user can read the name file /sys/bus/iio/devices/iio:deviceX/name. In case the sequence in which the iio device drivers are loaded/registered is constant, the numbering is constant and may be known in advance.
TIP: An example program which uses the interface can be found here:
General attribute naming convention:
in_voltage0_[…]: targets RX1
in_voltage1_[…]: targets RX2 (AD9361 in 2RX2TX mode only)
out_voltage0_[…]: targets TX1
out_voltage1_[…]: targets TX2 (AD9361 in 2RX2TX mode only)
out_altvoltage0_[…]: targets RX LO
out_altvoltage1_[…]: targets TX LO
This specifies any shell prompt running on the target
root:/> cd /sys/bus/iio/devices/ root:/sys/bus/iio/devices> ls iio:device0 iio:device1 iio:device2 iio:device3 iio:device4 root:/sys/bus/iio/devices> cd iio:device1 root:/sys/bus/iio/devices/iio:device1# ls -l total 0 -rw-r--r-- 1 root root 4096 Jan 15 13:33 calib_mode -r--r--r-- 1 root root 4096 Jan 15 13:49 calib_mode_available -rw-r--r-- 1 root root 4096 Jan 15 13:32 dcxo_tune_coarse -rw-r--r-- 1 root root 4096 Jan 15 13:32 dcxo_tune_fine -r--r--r-- 1 root root 4096 Jan 15 13:49 dev -rw-r--r-- 1 root root 4096 Jan 15 13:33 ensm_mode -r--r--r-- 1 root root 4096 Jan 15 13:49 ensm_mode_available --w------- 1 root root 4096 Jan 15 13:49 filter_fir_config -rw-r--r-- 1 root root 4096 Jan 15 13:32 in_out_voltage_filter_fir_en -rw-r--r-- 1 root root 4096 Jan 15 13:49 in_temp0_input -rw-r--r-- 1 root root 4096 Jan 15 13:33 in_voltage0_gain_control_mode -rw-r--r-- 1 root root 4096 Jan 15 13:32 in_voltage0_hardwaregain -rw-r--r-- 1 root root 4096 Jan 15 13:33 in_voltage0_rf_port_select -rw-r--r-- 1 root root 4096 Jan 15 13:49 in_voltage0_rssi -rw-r--r-- 1 root root 4096 Jan 15 13:33 in_voltage1_gain_control_mode -rw-r--r-- 1 root root 4096 Jan 15 13:32 in_voltage1_hardwaregain -rw-r--r-- 1 root root 4096 Jan 15 13:49 in_voltage1_rf_port_select -rw-r--r-- 1 root root 4096 Jan 15 13:49 in_voltage1_rssi -rw-r--r-- 1 root root 4096 Jan 15 13:49 in_voltage2_offset -rw-r--r-- 1 root root 4096 Jan 15 13:49 in_voltage2_raw -rw-r--r-- 1 root root 4096 Jan 15 13:49 in_voltage2_scale -rw-r--r-- 1 root root 4096 Jan 15 13:32 in_voltage_bb_dc_offset_tracking_en -rw-r--r-- 1 root root 4096 Jan 15 13:32 in_voltage_filter_fir_en -r--r--r-- 1 root root 4096 Jan 15 13:49 in_voltage_gain_control_mode_available -rw-r--r-- 1 root root 4096 Jan 15 13:32 in_voltage_quadrature_tracking_en -rw-r--r-- 1 root root 4096 Jan 15 13:32 in_voltage_rf_bandwidth -rw-r--r-- 1 root root 4096 Jan 15 13:32 in_voltage_rf_dc_offset_tracking_en -r--r--r-- 1 root root 4096 Jan 15 13:49 in_voltage_rf_port_select_available -rw-r--r-- 1 root root 4096 Jan 15 13:33 in_voltage_sampling_frequency -r--r--r-- 1 root root 4096 Jan 15 13:49 name -rw-r--r-- 1 root root 4096 Jan 15 13:49 out_altvoltage0_RX_LO_fastlock_load -rw-r--r-- 1 root root 4096 Jan 15 13:49 out_altvoltage0_RX_LO_fastlock_recall -rw-r--r-- 1 root root 4096 Jan 15 13:49 out_altvoltage0_RX_LO_fastlock_save -rw-r--r-- 1 root root 4096 Jan 15 13:49 out_altvoltage0_RX_LO_fastlock_store -rw-r--r-- 1 root root 4096 Jan 15 13:33 out_altvoltage0_RX_LO_frequency -rw-r--r-- 1 root root 4096 Jan 15 13:49 out_altvoltage1_TX_LO_fastlock_load -rw-r--r-- 1 root root 4096 Jan 15 13:49 out_altvoltage1_TX_LO_fastlock_recall -rw-r--r-- 1 root root 4096 Jan 15 13:49 out_altvoltage1_TX_LO_fastlock_save -rw-r--r-- 1 root root 4096 Jan 15 13:49 out_altvoltage1_TX_LO_fastlock_store -rw-r--r-- 1 root root 4096 Jan 15 13:33 out_altvoltage1_TX_LO_frequency -rw-r--r-- 1 root root 4096 Jan 15 13:32 out_voltage0_hardwaregain -rw-r--r-- 1 root root 4096 Jan 15 13:33 out_voltage0_rf_port_select -r--r--r-- 1 root root 4096 Jan 15 13:49 out_voltage0_rssi -rw-r--r-- 1 root root 4096 Jan 15 13:32 out_voltage1_hardwaregain -rw-r--r-- 1 root root 4096 Jan 15 13:49 out_voltage1_rf_port_select -r--r--r-- 1 root root 4096 Jan 15 13:49 out_voltage1_rssi -rw-r--r-- 1 root root 4096 Jan 15 13:49 out_voltage2_raw -rw-r--r-- 1 root root 4096 Jan 15 13:49 out_voltage2_scale -rw-r--r-- 1 root root 4096 Jan 15 13:49 out_voltage3_raw -rw-r--r-- 1 root root 4096 Jan 15 13:49 out_voltage3_scale -rw-r--r-- 1 root root 4096 Jan 15 13:32 out_voltage_filter_fir_en -rw-r--r-- 1 root root 4096 Jan 15 13:32 out_voltage_rf_bandwidth -r--r--r-- 1 root root 4096 Jan 15 13:49 out_voltage_rf_port_select_available -rw-r--r-- 1 root root 4096 Jan 15 13:33 out_voltage_sampling_frequency drwxr-xr-x 2 root root 0 Jan 15 13:49 power -r--r--r-- 1 root root 4096 Jan 15 13:49 rx_path_rates lrwxrwxrwx 1 root root 0 Jan 15 13:49 subsystem -> ../../../../../../../../bus/iio -rw-r--r-- 1 root root 4096 Jan 15 13:33 trx_rate_governor -r--r--r-- 1 root root 4096 Jan 15 13:49 trx_rate_governor_available -r--r--r-- 1 root root 4096 Jan 15 13:49 tx_path_rates -rw-r--r-- 1 root root 4096 Jan 15 13:49 uevent root:/sys/bus/iio/devices/iio:device1#
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device1> cat name ad9361-phy
The AD9361 transceiver includes an Enable State Machine (ENSM), allowing real time control over the current state of the device. The ENSM has two possible control methods – SPI control (writing ensm_mode), and pin control (writing ensm_mode = pinctrl).
The ENSM is controlled asynchronously by writing SPI registers to advance the current state to the next state.
The ENABLE and TXNRX pins allow real time control of the current state.
The ENSM allows TDD or FDD operation depending on the configuration.
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device1> cat ensm_mode_available sleep wait alert fdd pinctrl pinctrl_fdd_indep
FDD Mode options:
TDD Mode options:
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device1> cat ensm_mode fdd root:/sys/bus/iio/devices/iio:device1> echo alert > ensm_mode root:/sys/bus/iio/devices/iio:device1> cat ensm_mode alert
NOTE:
Be aware if you you want to transition in TDD mode from RX to TX you have to go via ALERT.
(Recent driver releases - do this now automatically…)
You may want to checkout the ENSM Pin-Control test script here: test_ensm_pinctrl.sh
The AD9361 transceiver contains two identical RFPLL synthesizers to generate the required LO signals. One is programmed for the RX channel and the other for the TX channel. The tuning range supported by this driver covers 70MHz to 6GHz (AD9363: 325-3800 MHz) with 2Hz tuning granularity.
This specifies any shell prompt running on the target
cat out_altvoltage0_RX_LO_frequency 2400000000 root:/sys/bus/iio/devices/iio:device1> echo 2450000000 > out_altvoltage0_RX_LO_frequency root:/sys/bus/iio/devices/iio:device1> cat out_altvoltage0_RX_LO_frequency 2450000000
If both, the TX and RX Local Oscillators (LO) are set to the same frequency or very close to each other. The TX LO may leak into the RX path. Usually this is avoided in TDD mode, since always only one of the LOs is enabled at a given time. However sometimes it can be beneficial in FDD mode to turn the TX LO off. Care must be taken since TX LO in Power-down mode, will cause the TX QUAD calibration to fail.
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device1> echo 0 > out_altvoltage1_TX_LO_powerdown root:/sys/bus/iio/devices/iio:device1> cat out_altvoltage1_TX_LO_powerdown 0
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device1> cat out_altvoltage0_RX_LO_powerdown 1
The driver allows switching between external and internal LO on the fly. Writing 1 into out_altvoltage0_RX_LO_external/out_altvoltage1_TX_LO_external switches to external LO. Respectively writing 0 switches back to the internal synthesizer.
In case additional clocks are specified in the device tree (clock-names: “ext_tx_lo” “ext_rx_lo”). The driver automatically controls the external clock/PLL Synthesizer.
Example:
adc0_ad9361: ad9361-phy@0 { compatible = "adi,ad9361"; /* Clocks */ clocks = <&ad9361_clkin>, <&ad9361_ext_tx_lo>, <&ad9361_ext_rx_lo>; clock-names = "ad9361_ext_refclk", "ext_tx_lo", "ext_rx_lo"; clock-output-names = "rx_sampl_clk", "tx_sampl_clk";
This specifies any shell prompt running on the target
cat out_altvoltage0_RX_LO_frequency 2400000000 root:/sys/bus/iio/devices/iio:device1> echo 1 > out_altvoltage0_RX_LO_external root:/sys/bus/iio/devices/iio:device1> cat out_altvoltage0_RX_LO_external 1
The device includes a Fast Lock mode that makes it possible to achieve faster than normal frequency changes by storing sets of synthesizer programming information (called “profiles”) either into device registers or the BB processor’s memory space to be recalled at a later time. The Fast Lock mode eliminates most of the overhead of synthesizer programming by allowing up to 8 full RX profiles and 8 full TX profiles of frequency configuration information (including VCO cal results) to be stored in the device for faster frequency changes. In order to use a particular profile, first it must be configured. Typically, this would be accomplished at powerup, but a new or updated profile can be defined at any convenient time.
NOTE:
You may want to checkout the Fastlock Pin-Control test script here:
test_tx_fastlock_pinctrl.sh
To create a profile tune the synthesizer and then write the target profile number into out_altvoltageX_fastlock_store.
Valid profile range is from 0..7
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device1> echo 4242000000 > out_altvoltage0_RX_LO_frequency root:/sys/bus/iio/devices/iio:device1> echo 0 > out_altvoltage0_RX_LO_fastlock_store
To recall a profile write the target profile number into out_altvoltageX_fastlock_recall. Valid profile range is from 0..7.
Reading out_altvoltageX_fastlock_recall returns the current profile number or –EINVAL if in normal synthesizer mode.
When in fastlock pin select mode (adi,[tx|rx]-fastlock-pincontrol-enable). This file needs to be written once with a value, before the pin-control can be used. This will moves the device into fastlock mode.
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device1> echo 0 > out_altvoltage0_RX_LO_fastlock_recall
In order to use more than 8 Profiles – an existing profile can be read back and stored by the user application.
The format is: Profile# val0,val1,val2,…,val15
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device1> echo 0 > out_altvoltage0_RX_LO_fastlock_save root:/sys/bus/iio/devices/iio:device1> cat out_altvoltage0_RX_LO_fastlock_save 0 240,0,202,204,12,80,24,16,187,255,60,238,113,233,93,174
A previously saved profile can be loaded in any of the 8 available slots. Write the profile string into out_altvoltageX_fastlock_load
The format is: Profile# val0,val1,val2,…,val15
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device1> echo 0 240,0,202,204,12,80,24,16,187,255,60,238,113,233,93,174 > out_altvoltage0_RX_LO_fastlock_load
The AD9361 RX signal path passes downconverted signals (I and Q) to the baseband receiver section. The baseband RX signal path is composed of two programmable analog low-pass filters, a 12-bit ADC, and four stages of digital decimating filters. Each of the four decimating filters can be bypassed. The corner frequency for each low-pass filter is programmable via SPI registers. Figure below shows a block diagram for the AD9361 RX signal path. Note that both the I and Q paths are schematically identical to each other.
The high level in_voltage_sampling_frequency attribute effectively controls the BBPLL frequency the ADC Sample clock and all following decimating filter blocks except the FIR block which is handled upon user configuration. This IIO device attribute allows the user to control the Baseband (BB) Sample Rate in Hz granularity in the range from 521KSPS up to 61.44MSPS, also depending on the FIR filter decimation chosen. in_voltage_sampling_frequency as well as out_voltage_sampling_frequency are not entirely independent, by default the both need to match unless adi,fdd-rx-rate-2tx-enable is enabled. Then RX rate can be twice the TX rate.
NOTE:
In the minimum ADC rate is 25MSPS.
Baseband rates below 2.083 MSPS (25MSPS/12) require FIR decimation/interpolation to be set.
In other words the FIR filter needs to be configured and enabled.
The minimum baseband rate with the FIR filter (decimate by 4) enabled is: 25MSPS /(4*12) = 520.83 kSPS.
Some example filters can be found here:filters
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device1> cat in_voltage_sampling_frequency 30720000 root:/sys/bus/iio/devices/iio:device1> echo 10000000 > in_voltage_sampling_frequency root:/sys/bus/iio/devices/iio:device1> cat in_voltage_sampling_frequency 10000000
This attribute lists the current rates in the various digital blocks.
Stage | Description | Ratio |
---|---|---|
BBPLL | The Baseband PLL frequency | |
ADC | The ADC sample rate | BBPLL/ADC = BBPLL divider |
R2 | Rate of the HB3/DEC3 filter | ADC/R2 = HB3 decimation factor |
R1 | Rate of the HB2 filter | R2/R1 = HB2 decimation factor |
RF | Rate of the HB1 filter | R1/RF = HB1 decimation factor |
RXSAMP | RX sampling rate or baseband rate | RF/RXSAMP = FIR decimation factor |
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device1> cat rx_path_rates BBPLL:983040000 ADC:245760000 R2:122880000 R1:61440000 RF:30720000 RXSAMP:30720000
The AD9361 TX signal path receives 12-bit 2s complement data in I-Q format from the AD9361 digital interface, and each channel (I and Q) passes this data through four digital interpolating filters to a 12-bit DAC. Each of the four interpolating filters can be bypassed. The DAC’s analog output is passed through two low pass filters prior to the RF mixer. The corner frequency for each low-pass filter is programmable via SPI registers. Figure 1 shows a block diagram for the AD9361 TX signal path. Note that both the I and the Q paths are schematically identical to each other. The four blocks leading up to the DAC in shown figure below comprise the digital filtering for the transmit path. These programmable filters provide the bandwidth limiting required prior to conversion from digital to analog. They also provide interpolation to translate from the input data rate to the rate needed for proper digital to analog conversion. In each filter, interpolation is performed first, followed by the filter transfer function.
The high level out_voltage_sampling_frequency attribute effectively controls the BBPLL frequency the ADC Sample clock, the DAC clock and all following interpolation filter blocks except the FIR block which is handled upon user configuration. This IIO device attribute allows the user to control the Baseband (BB) Sample Rate in Hz granularity in the range from 218KSPS up to 61.44MSPS, also depending on the FIR filter decimation chosen. out_voltage_sampling_frequency as well as in_voltage_sampling_frequency are not entirely independent, by default the both need to match unless adi,fdd-rx-rate-2tx-enable is set. Then RX rate can be twice the TX rate, however this mode needs to be supported by the FPGA/Baseband-Processor. The feedback clock must be externally divided.
NOTE:
In the minimum ADC rate is 25MSPS.
Baseband rates below 2.083 MSPS (25MSPS/12) require FIR decimation/interpolation to be set.
In other words the FIR filter needs to be configured and enabled.
The minimum baseband rate with the FIR filter (decimate by 4) enabled is: 25MSPS /(4*12) = 520.83 kSPS.
Some example filters can be found here:filters
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device1> cat out_voltage_sampling_frequency 30720000 root:/sys/bus/iio/devices/iio:device1> echo 10000000 > out _voltage_sampling_frequency root:/sys/bus/iio/devices/iio:device1> cat out _voltage_sampling_frequency 10000000
This attribute lists the current rates in the various digital blocks.
Stage | Description | Ratio |
---|---|---|
TXSAMP | TX sample rate or baseband rate | TF/TXSAMP = FIR interpolation factor |
TF | Rate of the HB1 filter | T1/TF = HB1 interpolation factor |
T1 | Rate of the HB2 filter | T2/T1 = HB2 interpolation factor |
T2 | Rate of the HB3/INT3 filter | DAC/T2 = HB3 interpolation factor |
DAC | The DAC sample rate | ADC/DAC = DAC clock divider |
BBPLL | The Baseband PLL frequency | BBPLL/ADC = BBPLL divider |
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device1> cat tx_path_rates BBPLL:983040000 DAC:122880000 T2:122880000 T1:61440000 TF:30720000 TXSAMP:30720000
The rate governor option allows the user to influence the ADC sample rate and decimation/interpolation rates chosen in the followed digital blocks. It mainly influences whether RX HB3/DEC3/ and TX HB3/INT3 decimates/interpolates by 3 or 2, thus resulting in an higher oversampling rate. Decimate by 3 doesn’t necessarily produce higher performance. Therefore the default setting of Nominal is always a good option.
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device1> cat trx_rate_governor_available nominal highest_osr
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device1> cat trx_rate_governor highest_osr root:/sys/bus/iio/devices/iio:device1> echo nominal > trx_rate_governor root:/sys/bus/iio/devices/iio:device1> cat trx_rate_governor nominal
The first/last digital filter in the RX/TX signal path is a programmable poly-phase FIR filter. The RX/RX FIR filter can decimate/interpolate by a factor of 1, 2, or 4, or it can be bypassed if not needed. The filter taps are configurable in groups of 16 between a minimum of 16 and a maximum of 128 taps. The RX FIR also has a programmable gain of -12dB, -6dB, 0dB, or +6dB. The filter provides a fixed +6dB gain to maximize dynamic range, so the programmable gain is typically set to -6dB to produce a net gain of 0dB. The TX FIR also has a programmable gain setting of 0dB or -6dB. Be aware there are some limitations in terms of the maximum number of taps supported by the different clock ratios, please consult the AD9361 manual for more details. The AD9361 device driver will warn if a programmed filter doesn’t match the limits.
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device1> cat filter_fir_config FIR Rx 0,0 Tx 0,0
Return Value:
Rx <Num Taps>,<Decimation factor> Tx <Num Taps>,<Interpolation factor>
Query current filter Configuration
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device1> cat LTE20.txt > filter_fir_config root:/sys/bus/iio/devices/iio:device1> cat filter_fir_config FIR Rx 128,2 Tx 128,2
Each file requires a short header:
RX [1,2,3(both)] GAIN [-12, -6, 0, 6] DEC [1,2,4] TX [1,2,3(both)] GAIN [-6, 0] INT [1,2,4] [RRX <BBPLL ADC R2 R1 RF RXSAMP>] [RTX <BBPLL DAC T2 T1 TF TXSAMP>] [BWRX <RX RF Bandwidth>] [BWTX <RX TF Bandwidth>] <tx-coef0, rx-coef0> <tx-coef1, rx-coef1> <…, …> <tx-coefN-1, rx-coefN-1>
#RX [1,2,3(both)] GAIN [-12, -6, 0, 6] DEC [1,2,4] #TX [1,2,3(both)] GAIN [-6, 0] INT [1,2,4] #tx,rx RX 3 GAIN -6 DEC 2 TX 3 GAIN 0 INT 2 RTX 983040000 245760000 245760000 122880000 61440000 30720000 RRX 983040000 491520000 245760000 122880000 61440000 30720000 BWTX 19365438 BWRX 19365514 -5,49 0,217 --snip--
#RX [1,2,3(both)] GAIN [-12, -6, 0, 6] DEC [1,2,4] #TX [1,2,3(both)] GAIN [-6, 0] INT [1,2,4] #tx,rx RX 3 GAIN -6 DEC 2 -5 0 --snip--
#RX [1,2,3(both)] GAIN [-12, -6, 0, 6] DEC [1,2,4] #TX [1,2,3(both)] GAIN [-6, 0] INT [1,2,4] #tx,rx TX 3 GAIN 0 INT 2 49 217 --snip--
To enable or disable the RX or TX path filters simply write 0,N or 1,Y to one of below control files. Combo attribute in_out_voltage_filter_fir_en allows to simultaneously enable both filters. This might sometimes be necessary, depending on the RX/TX Path Sampling Frequency and FIR interpolation and decimation rates chosen.
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device1> cat in_voltage_filter_fir_en 0 root:/sys/bus/iio/devices/iio:device1> echo 1 > in_voltage_filter_fir_en root:/sys/bus/iio/devices/iio:device1> cat in_voltage_filter_fir_en 1
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device1> cat out_voltage_filter_fir_en 0
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device1> cat in_out_voltage_filter_fir_en 0
The AD9361 features several Rx Analog Filter Blocks (RX TIA LPF, RX BB LPF) Analog filtering before the ADC reduces spurious signal levels by removing mixer products and providing general low pass filtering prior to downconversion. The RX TIA LPF is a single-pole low-pass filter with a programmable 3dB corner frequency. The RX BB LPF is a third-order Butterworthlow-passfilter with a programmable 3dB corner frequency.
These filters can be set by writing a single device attribute (in_voltage_rf_bandwidth)
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device1> cat in_voltage_rf_bandwidth 18000000 root:/sys/bus/iio/devices/iio:device1> echo 9000000 > in_voltage_rf_bandwidth root:/sys/bus/iio/devices/iio:device1> cat in_voltage_rf_bandwidth 9000000
The AD9361 features several Tx Analog Filter Blocks (TX BB LPF, TX Secondary LPF) Analog filtering after the DAC reduces spurious outputs by removing sampling artifacts and providing general low pass filtering prior to upconversion. The TX BB LPF is a third-order Butterworth low-pass filter with a programmable 3dB corner frequency. The TX Secondary LPF is a single-polelow-passfilter with a programmable 3dB corner frequency.
These filters can be set by writing a single device attribute (out_voltage_rf_bandwidth)
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device1> cat out_voltage_rf_bandwidth 18000000 root:/sys/bus/iio/devices/iio:device1> echo 9000000 > out_voltage_rf_bandwidth root:/sys/bus/iio/devices/iio:device1> cat out_voltage_rf_bandwidth 9000000
The versatile and highly configurable AD9361 transceiver has several gain control modes that enable its use in a variety of applications. Fully automatic gain control (AGC) modes are available that address time division duplex (TDD) as well as frequency division duplex (FDD) scenarios. In addition, the AD9361 has manual gain control (MGC) options that allow the baseband processor (BBP) to control the gain.
The default ADI provided optimized gain tables in full table mode provide 77 entries and in split gain table mode 41. Each index results typically in a 1 dB monotonic gain step. There are a total of 3 different tables available for different RX LO frequency ranges. The tables are swapped in and out automatically by the driver based on RX LO settings.
Standard Tables:
RX LO Range | Min GAIN | Max Gain |
---|---|---|
70 … 1300 MHz | -1 dB | 73 dB |
1300 … 4000 MHz | -3 dB | 71 dB |
4000 … 6000 MHz | -10 dB | 62 dB |
Custom gain tables can be loaded automatically during driver probe or anytime later via the gain_table_config sysfs attribute. Tables must be stored in the /lib/firmware folder, or compiled into the kernel using the CONFIG_FIRMWARE_IN_KERNEL, CONFIG_EXTRA_FIRMWARE config options. The table loaded during driver probe can be specified using following device tree property:
adi,gaintable-name = “ad9361_std_gaintable”;
In case no table is specified or loaded, the driver will continue to use the provided standard gain tables.
Gain tables are stored in a human readable file, with the format specified below. Up to 15 gain tables (for different frequency ranges, or gain table modes) can be provided in a single file.
Example: ad9361_std_gaintable
<list> <gaintable [AD9361|AD9364] type=[FULL|SPLIT] dest=[1|2|3] start=FREQUENCY1_Hz end=FREQUENCY2_Hz> gain_in_dB, reg_0x131, reg_0x132, reg_0x133 gain_in_dB, reg_0x131, reg_0x132, reg_0x133 gain_in_dB, reg_0x131, reg_0x132, reg_0x133 … </gaintable> ... </list>
Assumptions:
This specifies any shell prompt running on the target
root@analog:/sys/bus/iio/devices/iio:device1# ls /lib/firmware/ad9* ad9361_std_gaintable root@analog:/sys/bus/iio/devices/iio:device1# cat /lib/firmware/ad9361_std_gaintable > gain_table_config
Reading the gain_table_config attribute returns the current gain table that is loaded into the transceiver IC. The printed format matches the format used in the gaintable file.
This specifies any shell prompt running on the target
root@analog:/sys/bus/iio/devices/iio:device1# cat gain_table_config <gaintable AD9361 type=FULL dest=3 start=1300000000 end=4000000000> -3, 0x00, 0x00, 0x20 -3, 0x00, 0x00, 0x00 -3, 0x00, 0x00, 0x00 -2, 0x00, 0x01, 0x00 -1, 0x00, 0x02, 0x00 0, 0x00, 0x03, 0x00 1, 0x00, 0x04, 0x00 2, 0x00, 0x05, 0x00 3, 0x01, 0x03, 0x20 4, 0x01, 0x04, 0x00 5, 0x01, 0x05, 0x00 6, 0x01, 0x06, 0x00 7, 0x01, 0x07, 0x00 8, 0x01, 0x08, 0x00 [--snip--] 69, 0x6D, 0x38, 0x20 70, 0x6E, 0x38, 0x20 71, 0x6F, 0x38, 0x20 </gaintable>
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device1> cat in_voltage_gain_control_mode_available manual fast_attack slow_attack hybrid
Mode | Description |
---|---|
manual | In MGC mode, the BBP controls the gain index pointer(s). In its simplest form, the BBP evaluates the digital signal level at the I/O port and then adjusts the gain appropriately. The BBP can control manual gain in one of two ways. The default method uses SPI writes (writing in_voltage[0,1]_hardwaregain) the total gain in dB. This results in different gain indices depending on the gain table loaded. Alternatively, the BBP can pulse the Control Input pins to move the gain indices. |
slow_attack | Slow Attack Mode is intended for slowly changing signals such as those found in some FDD applications such as WCDMA and FDD LTE. The Slow Attack AGC uses a 2nd order control loop with hysteresis that changes the gain in order to keep the average signal power within a programmable window |
hybrid | The AGC hybrid mode is the same as the slow AGC mode with the exception that the gain update counter is not used. Instead, gain updates occur when the BBP pulls the CTRL_IN2 signal high. The “hybrid” term arises because the BBP has taken some control of the algorithm away from the AD9361 so gain control is no longer completely automatic. |
fast_attack | Fast Attack Mode is intended for waveforms that “burst” on and off, such as those found in TDD applications or GSM/EDGE FDD applications. The AGC responds very quickly to overloads at the start of a burst so that the AGC can settle to an optimum gain index by the time the data portion of the signal arrives. |
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device1> cat in_voltage0_gain_control_mode slow_attack root:/sys/bus/iio/devices/iio:device1> echo manual > in_voltage0_gain_control_mode root:/sys/bus/iio/devices/iio:device1> cat in_voltage0_gain_control_mode manual
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device1> cat in_voltage1_gain_control_mode slow_attack
Supported in all available Gain control modes
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device1> cat in_voltage0_hardwaregain 61.000000 dB
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device1> cat in_voltage1_hardwaregain 71.000000 dB
Only available in Manual Gain Control Mode (MGC)
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device1> echo 42 > in_voltage0_hardwaregain root:/sys/bus/iio/devices/iio:device1> cat in_voltage0_hardwaregain 42.000000 dB
The TX attenuation/gain can be individually controlled for TX1 and TX2. The range is from 0 to -89.75 dB in 0.25dB steps. The nomenclature used here is gain instead of attenuation, so all values are expressed negative.
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device1> cat out_voltage0_hardwaregain -10.000000 dB root:/sys/bus/iio/devices/iio:device1> echo -42.25 > out_voltage0_hardwaregain root:/sys/bus/iio/devices/iio:device1> cat out_voltage0_hardwaregain -42.250000 dB
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device1> cat out_voltage1_hardwaregain -10.000000 dB
Given the wide variety of applications for which the AD9361 is suited, the received strength signal indicator (RSSI) may be setup in one of several configurations, allowing the user to optimize the RSSI to produce extremely accurate results with a minimum of BBP interaction. The AD9361 measures RSSI by measuring the power level in dB and compensating for the receive path gain. The various options available support both TDD and FDD applications. Note that the RSSI value is not in absolute units. Equating the RSSI read-back value to an absolute power level (e.g., in dBm) requires a system factory or bench calibration. To calibrate the RSSI word to an absolute reference, inject a signal into the antenna port of the completed system and read the RSSI word. From this test, generate a correction factor that equates the RSI word to the injected signal level at the antenna port.
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device1> cat in_voltage0_rssi 104.50 dB
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device1> cat in_voltage1_rssi 116.75 dB
Recognizing that in TDD systems the receiver and transmitter are not operating simultaneously, the AD9361 provides the ability to reuse the receiver circuitry by multiplexing the power detector into the receive path. The receiver RSSI circuitry is then turned on during the transmit burst and results in accurate Tx RSSI measurements.
NOTE:
This feature is only available in TX MONITOR MODE
set in_voltage0_rf_port_select to one of the following modes:
TX_MONITOR1, TX_MONITOR2 or TX_MONITOR1_2
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device1> cat out_voltage0_rssi 30.50 dB
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device1> cat out_voltage1_rssi 0.00 dB
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device1> cat calib_mode_available auto manual manual_tx_quad tx_quad rf_dc_offs rssi_gain_step
Option | Description |
---|---|
auto | Run RF DC and TX Quadrature Calibration when moving to a new carrier frequency that is more than 100 MHz away from the previous carrier frequency |
manual | Disables auto mode |
manual_tx_quad | Disables auto mode and also prevents any TX Quad Calibration unless manually invoked using tx_quad |
rf_dc_offs | Issue RF DC Offset Calibration |
tx_quad | Issue TX Quadrature Calibration (may have a second optional parameter (cal phase value 0..31) |
rssi_gain_step | Runs the RSSI gain step calibration. Before running this calibration, provide a single tone within the channel bandwidth and monitor the received data. Adjust the tone amplitude until the received data is within a few dB of full scale but not overloading. Once this calibration is done, calib_mode will be automatically set to its previous value. |
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device1> cat calib_mode auto
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device1> echo tx_quad > calib_mode
Please see the FAQ for more information
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device1> echo tx_quad 14 > calib_mode
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device1> echo tx_quad -2 > calib_mode
Writing 0, N or 1, Y to the below attributes either disables or enables the corresponding tracking option.
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device1> cat in_voltage_quadrature_tracking_en 1 root:/sys/bus/iio/devices/iio:device1> echo 0 > in_voltage_quadrature_tracking_en root:/sys/bus/iio/devices/iio:device1> cat in_voltage_quadrature_tracking_en 0
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device1> cat in_voltage_bb_dc_offset_tracking_en 1
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device1> cat in_voltage_rf_dc_offset_tracking_en 1
Each receive channel has 3 differential or 6 single ended inputs that can be multiplexed to the signal chain, likewise each transmitter has 2 differential outputs that can be chosen from.
NOTE: Switching the RF INPUT port:
Switching the RF input port:
During device driver initialization the driver runs the RF DC offset calibration only on the default RF input port specified with these attributes.
So if using the RF RX B or C inputs along with the RF RX A input, you should run the calibration also, once with other input band/port selected.
After calibrating each band, switching between from the A input to the B or C input should not require another calibration unless a large frequency change is made. Since the B and C inputs use the same calibration results, switching from input B to input C may require running the RF DC offset calibration.
See here: Calibration Mode Controls: rf_dc_offs
NOTE: Switching the RF OUTPUT port:
During device driver initialization the driver runs the TX Quadrature calibration only on the default RF output port specified with these attributes.
During regular operation TX Quadrature is only run on the select RF output.
However the TX quadrature calibration stores a separate set of calibration results for the RF TX_A and TX_B output path.
So if switching the output, the calibration must be once manually triggered.
See here: Calibration Mode Controls: tx_quad
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device1> cat out_voltage_rf_port_select_available A B root:/sys/bus/iio/devices/iio:device1> cat in_voltage_rf_port_select_available A_BALANCED B_BALANCED C_BALANCED A_N A_P B_N B_P C_N C_P TX_MONITOR1 TX_MONITOR2 TX_MONITOR1_2 root:/sys/bus/iio/devices/iio:device1> echo B_BALANCED > in_voltage0_rf_port_select
The AD9361 can either be clocked from an external clock source or a local crystal oscillator (XO). Since it's likely that a Crystal oscillator is not perfect - a digital correction (DCXO) can be used to tune the external component. This only works with AT cut fundamental mode crystal resonators with a load capacitance of less than 10pF which are connected between the XTALP and XTALN pins of the AD9361.
This is what ADI's FMCOMMS2, FMCOMMS3, and FMCOMMS4 boards are using.
By adjusting a capacitor within the AD9361, the resulting DCXO frequency can be adjusted to compensate for XO frequency tolerance and stability. dcxo_tune_coarse
sets a coarse capacitor value while dcxo_tune_fine
sets a fine capacitor value. Together, these two settings control the frequency of the DCXO. The resolution of the DCXO varies with coarse word with a worst case resolution (at coarse word = 0) of 0.0125 ppm. Using both coarse and fine words, the DCXO can vary the frequency over a ±60 ppm range.
After initialization (after the BBPLL and RFPLLs are programmed, calibrated, and locked), the DCXO words may be written at any time without disturbing the system.
The plot shows the variation of DCXO frequency over all possible variations of coarse and fine word. The XO nominal frequency used in this test was 40MHz.
The DCXO can be tuned using the coarse and fine tune attributes detailed below.
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device1> cat dcxo_tune_coarse 8
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device1> cat dcxo_tune_fine 5920 root:/sys/bus/iio/devices/iio:device1> echo 5930 > dcxo_tune_fine root:/sys/bus/iio/devices/iio:device1> cat dcxo_tune_fine 5930
For systems that are using single ended crystal oscillators, or an external clock source and driving it into the XTALN pin, some correction may be necessary. What happens in this case, is you digitally correct for the oscillator offset, by determining what the actual oscillator is, and then telling the system, so it can use that specific number in it's math for the PLL and sample rate calculations.
This is what the FMCOMMS5, ADI RF SOM1, ADI RF SOM2 and the PlutoSDR use.
Since every time this is written, it will re-calculate and re-program all the PLL settings (Tx LO, Rx LO, ADC and DAC sample rates), this should only be updated when disturbing the system is acceptable. (normally reprogramming the LO, or sample rates)
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device1> cat xo_correction 40000000 root:/sys/bus/iio/devices/iio:device1> echo 40000005 > xo_correction root:/sys/bus/iio/devices/iio:device1> cat xo_correction 40000005
For accurate results this read back requires a one-point factory calibration. Determine the offset between this readback in millidegree Celsius and the known device temperature. Then adjust the device tree property “adi,temp-sense-offset-signed” with a proper offset in degrees Celsius. In the OSC advanced plugin see AUX ADC/DAC/IO tab under Temp sensor offset. Also the absolute offset (signed char) is directly written into register 0x0B.
Example:
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device1> cat in_temp0_input 29825
There is an Auxiliary ADC on the chip - that can be read like any other IIO ADC.
Attributes are:
To obtain the reading in mV calculate: (in_voltage2_raw + in_voltage2_offset) * in_voltage2_scale
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device1> grep “” in_voltage2_* in_voltage2_offset:57 in_voltage2_raw:1494 in_voltage2_scale:0.305250
There are 2 Auxiliary DACs on the chip.
Attributes are:
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device1> grep “” out_voltage2* out_voltage3* out_voltage2_raw:306 out_voltage2_scale:1.000000 out_voltage3_raw:306 out_voltage3_scale:1.000000 root:/sys/bus/iio/devices/iio:device1> echo 1000 > out_voltage2_raw
The RSSI gain step calibration can be run by setting calib_mode to rssi_gain_step (See: calibration_mode_controls).
Once the calibration is done, the error tables can be read and loaded again anytime using the dedicated sysfs attribute. Since the gain step calibration register values are dependent on the LO frequency, specifying them is also possible (gain_step_calib_reg_val = Maximum LNA Gain LNA, Gain difference word for Index 0, LNA Gain difference word for Index 1, LNA Gain difference word for Index 2, LNA Gain difference word for Index 3).
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device1> cat rssi_gain_step_error lna_error: 0 15 14 0 mixer_error: 16 16 16 16 16 16 16 16 16 16 16 16 16 16 16 0 gain_step_calib_reg_val: 192 44 16 6 0
The AD9361 driver supports a number of advanced debug controls via the kernel debugfs. How these device files/controls can be used is described here. The FMCOMMS2/3/4/5 OSC Advanced Plugin directly controls these and adds a user friendly interface.
There is a large number of AD9361 Device Driver Customization options available. Typically these are supplied via Devicetree.
However for debug and evaluation purposes these can be changed during runtime. Please note that changes will be lost if the device is unbinded or the platform is rebooted. Changes will only take affect once the initialize
attribute is written 1
. It should also be noted that the AD9361 will take a RESET, so current settings done via the main IIO API will be lost. Accessing debugfs requires root privileges. Only device files prefixed with adi,
are AD9361 Device Driver Customization Options.
In order to identify if the IIO device in question (ad9361-phy) you first need to identify the IIO device number. Therefore read the name attribute of each IIO device
This specifies any shell prompt running on the target
root@analog:~# grep "" /sys/bus/iio/devices/iio\:device*/name /sys/bus/iio/devices/iio:device0/name:ad7291 /sys/bus/iio/devices/iio:device1/name:ad9361-phy /sys/bus/iio/devices/iio:device2/name:xadc /sys/bus/iio/devices/iio:device3/name:adf4351-udc-rx-pmod /sys/bus/iio/devices/iio:device4/name:adf4351-udc-tx-pmod /sys/bus/iio/devices/iio:device5/name:cf-ad9361-dds-core-lpc /sys/bus/iio/devices/iio:device6/name:cf-ad9361-lpc root@analog:~#
Change directory to /sys/kernel/debug/iio/ iio:deviceX.
This specifies any shell prompt running on the target
root@analog:~# cd /sys/kernel/debug/iio/iio\:device1 root@analog:/sys/kernel/debug/iio/iio:device1# ls [[--snip--]] adi,txmon-2-lo-cm adi,txmon-dc-tracking-enable adi,txmon-delay adi,txmon-duration adi,txmon-high-gain adi,txmon-low-gain adi,txmon-low-high-thresh adi,txmon-one-shot-mode-enable adi,update-tx-gain-in-alert-enable adi,xo-disable-use-ext-refclk-enable bist_prbs bist_timing_analysis bist_tone calibration_switch_control digital_tune direct_reg_access gaininfo_rx1 gaininfo_rx2 initialize loopback
This specifies any shell prompt running on the target
root@analog:/sys/kernel/debug/iio/iio:device1# cat adi,frequency-division-duplex-mode-enable 1 root@analog:/sys/kernel/debug/iio/iio:device1# cat /sys/bus/iio/devices/iio\:device1/ensm_mode_available sleep wait alert fdd pinctrl pinctrl_fdd_indep root@analog:/sys/kernel/debug/iio/iio:device1# echo 0 > adi,frequency-division-duplex-mode-enable root@analog:/sys/kernel/debug/iio/iio:device1# echo 1 > initialize root@analog:/sys/kernel/debug/iio/iio:device1# cat /sys/bus/iio/devices/iio\:device1/ensm_mode_available sleep wait alert rx tx pinctrl
Controling these attribute files directly take effect and therefore don’t require the initialize
sequence.
Test functionality exposed here is only meant to route or inject test patterns/data than can be used to validate the Digital Interface or functionality of the device.
User selectable tone (with frequency and level selection), that can either injected into the RX or TX path. A MASK can be supplied to disable certain channels. A masked channel (box check) is not driving any data.
SYNTAX:
bist_tone <Injection Point> <Tone Frequency> <Tone Level> <Channel Mask>
Injection Point | |
---|---|
Value | Function |
0 | Disable |
1 | Injection Point TX |
2 | Injection Point RX |
Tone Frequency | |
---|---|
Value | Function |
0 | FSample / 32 |
1 | FSample / 16 |
2 | FSample * 3 / 32 |
3 | FSample / 8 |
> 3 | Desired Tone Frquency in Hz (driver will internally choose the closest match |
Tone Level (dbFS) | |
---|---|
Value | Function |
0 | Full Scale (FS) |
6 | FS/2 |
12 | FS/4 |
18 | FS/8 |
Channel Mask | |
---|---|
Bit | Function |
0 | Mask Channel 1 I-data |
1 | Mask Channel 1 Q-data |
2 | Mask Channel 2 I-data |
3 | Mask Channel 2 Q-data |
Example: Inject -6dBFS tone at Fsample/32 into RX (all channels enabled)
This specifies any shell prompt running on the target
root@analog:/sys/kernel/debug/iio/iio:device1# echo 2 0 6 0 > bist_tone
Pseudorandom Binary Sequence (PRBS) that can either injected into the RX or TX path.
SYNTAX:
bist_prbs <Injection Point>
Injection Point | |
---|---|
Value | Function |
0 | Disable |
1 | Injection Point TX |
2 | Injection Point RX |
Example: Inject PRBS into RX
This specifies any shell prompt running on the target
root@analog:/sys/kernel/debug/iio/iio:device1# echo 2 > bist_prbs
Allows either to digitally loopback TX data into the RX path or vice versa.
SYNTAX:
loopback <Mode>
Value | Mode |
---|---|
0 | Disable |
1 | Digital TX → Digital RX |
2 | RF RX → RF TX |
Example: Digital TX → Digital RX
This specifies any shell prompt running on the target
root@analog:/sys/kernel/debug/iio/iio:device1# echo 1 > loopback
bist_timing_analysis: See here: Digital Interface Timing Verification
digital_tune: See here: Digital Interface Timing Verification
Some IIO drivers feature an optional debug facility, allowing users to read or write registers directly. Special care needs to be taken when using this feature, since you can modify registers on the back of the driver.
Accessing debugfs requires root privileges.
In order to identify if the IIO device in question feature this option you first need to identify the IIO device number.
Therefore read the name attribute of each IIO device
This specifies any shell prompt running on the target
root@analog:~# grep "" /sys/bus/iio/devices/iio\:device*/name /sys/bus/iio/devices/iio:device0/name:ad7291 /sys/bus/iio/devices/iio:device1/name:ad9361-phy /sys/bus/iio/devices/iio:device2/name:xadc /sys/bus/iio/devices/iio:device3/name:adf4351-udc-rx-pmod /sys/bus/iio/devices/iio:device4/name:adf4351-udc-tx-pmod /sys/bus/iio/devices/iio:device5/name:cf-ad9361-dds-core-lpc /sys/bus/iio/devices/iio:device6/name:cf-ad9361-lpc root@analog:~#
Change directory to /sys/kernel/debug/iio/ iio:deviceX and check if the direct_reg_access file exists.
This specifies any shell prompt running on the target
root@analog:~# cd /sys/kernel/debug/iio/iio\:device1 root@analog:/sys/kernel/debug/iio/iio:device1# ls direct_reg_access direct_reg_access
Reading
This specifies any shell prompt running on the target
root@analog:/sys/kernel/debug/iio/iio:device1# echo 0x7 > direct_reg_access root@analog:/sys/kernel/debug/iio/iio:device1# cat direct_reg_access 0x40
Writing
Write ADDRESS VALUE
This specifies any shell prompt running on the target
root@analog:/sys/kernel/debug/iio/iio:device1# echo 0x7 0x50 > direct_reg_access root@analog:/sys/kernel/debug/iio/iio:device1# cat direct_reg_access 0x50
Accessing HDL CORE registers
Special ADI device driver convention for devices that have both:
In this case when accessing the HDL Core Registers always set BIT31.
The register map for typical ADI HDL cores can be found here: Register Map
This specifies any shell prompt running on the target
root@analog:/sys/kernel/debug/iio/iio:device6# echo 0x80000000 > direct_reg_access root@analog:/sys/kernel/debug/iio/iio:device6# cat direct_reg_access 0x80062