This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:tools-software:linux-drivers:iio-transceiver:ad9361 [19 Jan 2018 09:56] – rename xcomm_zynq -> master Alexandru Ardelean | resources:tools-software:linux-drivers:iio-transceiver:ad9361 [13 Feb 2018 09:45] – [FASTLOCK MODE] Michael Hennerich | ||
---|---|---|---|
Line 374: | Line 374: | ||
or –EINVAL if in normal synthesizer mode. | or –EINVAL if in normal synthesizer mode. | ||
- | When in fastlock pin select mode (adi,[t]rx-fastlock-pincontrol-enable). | + | When in fastlock pin select mode (adi,[tx|rx]-fastlock-pincontrol-enable). |
- | This file needs to be written with a value, before | + | This file needs to be written |
+ | This will moves the device into fastlock mode. | ||
<WRAP box bggreen>< | <WRAP box bggreen>< |