This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:tools-software:linux-drivers:iio-transceiver:ad9361 [28 Oct 2021 22:07] – [Driver testing / API] Robin Getz | resources:tools-software:linux-drivers:iio-transceiver:ad9361 [12 Feb 2022 01:49] (current) – Reading RX gain table is dependent on the RX_LO setting Terry Carpenter | ||
---|---|---|---|
Line 770: | Line 770: | ||
Reading the gain_table_config attribute returns the current gain table that is loaded into the transceiver IC. | Reading the gain_table_config attribute returns the current gain table that is loaded into the transceiver IC. | ||
The printed format matches the format used in the gaintable file. | The printed format matches the format used in the gaintable file. | ||
+ | |||
+ | Reading the gain table only displays the gain table that will be used with the current RX_LO frequency setting. | ||
+ | <WRAP box bggreen>< | ||
+ | < | ||
+ | root:/ | ||
+ | root:/ | ||
+ | 2450000000 | ||
+ | </ | ||
<WRAP box bggreen>< | <WRAP box bggreen>< |