Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision |
resources:tools-software:linux-drivers:iio-transceiver:ad9361-customization [20 Jun 2017 13:40] – [Linux/No-OS device driver comparison] Michael Hennerich | resources:tools-software:linux-drivers:iio-transceiver:ad9361-customization [19 Sep 2017 09:02] – Michael Hennerich |
---|
^ Base Configuration ^^^ | ^ Base Configuration ^^^ |
| adi,2rx-2tx-mode-enable | two_rx_two_tx_mode_enable | Use 2Rx2Tx mode - default 1Rx1Tx (AD9364 must clear this) | | | adi,2rx-2tx-mode-enable | two_rx_two_tx_mode_enable | Use 2Rx2Tx mode - default 1Rx1Tx (AD9364 must clear this) | |
| | adi,1rx-1tx-mode-use-rx-num | one_rx_one_tx_mode_use_rx_num | Valid only in 1Rx1Tx mode for AD9361 and AD9363, Selects which RX channel is used | |
| | adi,1rx-1tx-mode-use-tx-num | one_rx_one_tx_mode_use_tx_num | Valid only in 1Rx1Tx mode for AD9361 and AD9363, Selects which TX channel is used | |
| adi,frequency-division-duplex-mode-enable | frequency_division_duplex_mode_enable | Use FDD mode - default TDD | | | adi,frequency-division-duplex-mode-enable | frequency_division_duplex_mode_enable | Use FDD mode - default TDD | |
| adi,tdd-use-dual-synth-mode-enable | tdd_use_dual_synth_mode_enable | In TDD mode use Dual Synth mode - default only one Synth is enabled | | | adi,tdd-use-dual-synth-mode-enable | tdd_use_dual_synth_mode_enable | In TDD mode use Dual Synth mode - default only one Synth is enabled | |