This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:linux-drivers:iio-resolver:ad2s90 [05 Sep 2012 14:06] – [Status] Michael Hennerich | resources:tools-software:linux-drivers:iio-resolver:ad2s90 [20 Nov 2015 16:31] (current) – [Description] Lars-Peter Clausen | ||
---|---|---|---|
Line 7: | Line 7: | ||
===== Description ===== | ===== Description ===== | ||
- | {{scrape> | + | {{scrape> |
* [[adi> | * [[adi> | ||
- | * {{scrape> | ||
- | |||
This is a Linux industrial I/O ([[software: | This is a Linux industrial I/O ([[software: | ||
The industrial I/O subsystem provides a unified framework for drivers for many different types of converters and sensors using a number of different physical interfaces (i2c, spi, etc). | The industrial I/O subsystem provides a unified framework for drivers for many different types of converters and sensors using a number of different physical interfaces (i2c, spi, etc). | ||
Line 20: | Line 18: | ||
===== Status ===== | ===== Status ===== | ||
- | ^ Source | + | ^ Source ^ Mainlined? ^ |
- | | [[git.linux.org> | + | | [[git.linux.org> |
===== Files ===== | ===== Files ===== | ||
Line 33: | Line 31: | ||
"make qconfig" | "make qconfig" | ||
- | <note> | + | <WRAP round help> |
The Driver depends on **CONFIG_SPI** | The Driver depends on **CONFIG_SPI** | ||
- | </note> | + | </WRAP> |
< | < |