Wiki

This version is outdated by a newer approved version.DiffThis version (13 Jan 2020 18:56) was approved by Robin Getz.The Previously approved version (20 Dec 2019 10:31) is available.Diff

This is an old revision of the document!


LTC6952 Ultralow Jitter, 4.5GHz PLL, JESD204B/JESD204C Linux Driver

Supported Devices

Description

The LTC6952 is a high performance, ultralow jitter, JESD204B/C clock generation and distribution IC. It includes a Phase Locked Loop (PLL) core, consisting of a reference divider, phase-frequency detector (PFD) with a phase-lock indicator, ultralow noise charge pump and integer feedback divider.

The LTC6952’s eleven outputs can be configured is up to five JESD204B/C subclass 1 device clock/SYSREF pairs plus one general purpose output, or simply eleven general purpose clock outputs for non-JESD204B/C applications.

This is a Linux industrial I/O (IIO) subsystem driver, targeting serial interface PLL Synthesizers. The industrial I/O subsystem provides a unified framework for drivers for many different types of converters and sensors using a number of different physical interfaces (i2c, spi, etc). See IIO for more information.

Source Code

Status

Source Mainlined?
drivers/iio/frequency/ltc6952.c No

Files

Enabling the driver

Configure kernel with “make menuconfig” (alternatively use “make xconfig” or “make qconfig”)

The LTC6952 Driver depends on CONFIG_SPI

Linux Kernel Configuration
    Device Drivers  --->
    <*>  Industrial I/O support --->
             Frequency Synthesizers DDS/PLL  ---> 
                 Clock Generator/Distribution  --->
                 <*> Analog Devices LTC6952 Clock Ultralow Jitter with JESD204B/C

Adding a device tree entry

Available properties

Required properties:
  • compatible: Should be “adi,ltc6952”.
  • reg: SPI chip select number.
  • spi-max-frequency: Max SPI frequency to use (⇐ 20000000).
  • adi,vco-frequency-hz: The frequency of the VCO.
  • adi,ref-frequency-hz: Reference input frequency. This is fed in the reference divider.
  • clock-output-names: An array of 11 elements, representing the names of the output clocks.

Adding channels

Channels can be specified using child nodes. The following properties are applicable to them:

  • reg: The identifier of the channel.
  • adi,extended-name: Descriptive channel name.
  • adi,divider: Channel divider. This divides the incoming VCO frequency.
  • adi,digital-delay: Each output divider can have the start time of the output delayed by integer multiples of half of the VCO period after a synchronization event.
  • adi,analog-delay: Each output has a fine analog delay feature to further adjust its output delay time (tADELx) in small steps.

Device tree example

The following example instantiates the hmc7044 driver for a HMC7044 device connected on the SPI bus to the chip-select line 0.

ltc6952@0 {
       compatible = "adi,ltc6952";
       reg = <0>;
       #address-cells = <1>;
       #size-cells = <0>;
       spi-max-frequency = <10000000>;
       clock-output-names = "ltc6952_out0", "ltc6952_out1", "ltc6952_out2",
         "ltc6952_out3", "ltc6952_out4", "ltc6952_out5", "ltc6952_out6",
         "ltc6952_out7", "ltc6952_out8", "ltc6952_out9", "ltc6952_out10";
       #clock-cells = <1>;
       adi,vco-frequency-hz = <4000000000>;
       adi,ref-frequency-hz = <100000000>;
       ltc6952_c0: channel@0 {
         reg = <0>;
         adi,extended-name = "REF_CLK";
         adi,divider = <10>;
         adi,digital-delay = <100>;
         adi,analog-delay = <0>;
       };
       ltc6952_c1: channel@1 {
         reg = <1>;
         adi,extended-name = "TEST_CLK";
         adi,divider = <10>;
       };
     };
resources/tools-software/linux-drivers/iio-pll/ltc6952.1578938178.txt.gz · Last modified: 13 Jan 2020 18:56 by Robin Getz