This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:tools-software:linux-drivers:iio-inertial-measurement-units:adis16480 [02 Apr 2019 10:30] – Added ADIS16490 support Stefan Popa | resources:tools-software:linux-drivers:iio-inertial-measurement-units:adis16480 [14 Jan 2021 05:38] (current) – use wiki interwiki links Robin Getz | ||
---|---|---|---|
Line 169: | Line 169: | ||
====== Hardware configuration ====== | ====== Hardware configuration ====== | ||
- | The [[adi> | + | The [[adi> |
Here is an example of basic connection from the ADIS1649X interface connector to the host (microprocessor): | Here is an example of basic connection from the ADIS1649X interface connector to the host (microprocessor): | ||
ADIS1649X | ADIS1649X |