This shows you the differences between two versions of the page.
Both sides previous revision Previous revision | |||
resources:tools-software:linux-drivers:iio-inertial-measurement-units:adis16480 [02 Apr 2019 10:30] Stefan Popa Added ADIS16490 support |
resources:tools-software:linux-drivers:iio-inertial-measurement-units:adis16480 [14 Jan 2021 05:38] Robin Getz use wiki interwiki links |
||
---|---|---|---|
Line 169: | Line 169: | ||
====== Hardware configuration ====== | ====== Hardware configuration ====== | ||
- | The [[adi>EVAL-ADIS16IMU1|ADIS16IMU1/PCBZ]] is the primary breakout board for the ADIS1649x products. This breakout board simplifies the process of connecting an ADIS1649x IMU to an embedded processor system using a 16-pin, 1mm ribbon cable. For a detailed description, please see: [[https://wiki.analog.com/resources/eval/user-guides/inertial-mems/imu/adis1649x]] | + | The [[adi>EVAL-ADIS16IMU1|ADIS16IMU1/PCBZ]] is the primary breakout board for the ADIS1649x products. This breakout board simplifies the process of connecting an ADIS1649x IMU to an embedded processor system using a 16-pin, 1mm ribbon cable. For a detailed description, please see: [[/resources/eval/user-guides/inertial-mems/imu/adis1649x]] |
Here is an example of basic connection from the ADIS1649X interface connector to the host (microprocessor): | Here is an example of basic connection from the ADIS1649X interface connector to the host (microprocessor): | ||
ADIS1649X HOST MICROPROCESSOR | ADIS1649X HOST MICROPROCESSOR |