This is a Linux industrial I/O (IIO) subsystem driver, targeting serial interface Inertial Measurement Units (IMU). The industrial I/O subsystem provides a unified framework for drivers for many different types of converters and sensors using a number of different physical interfaces (i2c, spi, etc). See IIO for more information.
Function | File |
---|---|
driver | drivers/iio/imu/adis16475.c |
Analog Devices ADIS16475 and similar IMUs
imu@0 { compatible = "adi,adis16475-3"; reg = <0>; spi-cpha; spi-cpol; spi-max-frequency = <2000000>; interrupts = <4 IRQ_TYPE_EDGE_RISING>; interrupt-parent = <&gpio>; };
For more supported devicetree properties take a look to dt-bindings.
Configure kernel with “make menuconfig” (alternatively use “make xconfig” or “make qconfig”)
The adis16475 driver depends on CONFIG_SPI_MASTER
Linux Kernel Configuration Device Drivers ---> <*> Industrial I/O support ---> --- Industrial I/O support [*] Enable buffer support within IIO -*- Industrial I/O buffering based on kfifo -*- Enable triggered sampling support [--snip--] Inertial measurement units ---> [--snip--] <*> Analog Devices ADIS16475 and similar IMU driver [--snip--]
The evaluation kits simplify the process of connecting an IMU to an embedded processor system using a 16-pin, 1mm ribbon cable. For a detailed description check the links (on the beginning of the page) for the appropriated evaluation kit. Here is an example of basic connection from one ADIS device interface connector to the host:(microprocessor):
DEVICE HOST MICROPROCESSOR * DR ———————> IRQ GPIO * CS <——————— SPI_SEL * SCLK <——————— SPI_SCLK * DIN <——————— SPI_MOSI * DOUT ———————> SPI_MISO
Each and every IIO device, typically a hardware chip, has a device folder under /sys/bus/iio/devices/iio:deviceX. Where X is the IIO index of the device. Under every of these directory folders reside a set of files, depending on the characteristics and features of the hardware device in question. These files are consistently generalized and documented in the IIO ABI documentation. In order to determine which IIO deviceX corresponds to which hardware device, the user can read the name file /sys/bus/iio/devices/iio:deviceX/name. In case the sequence in which the iio device drivers are loaded/registered is constant, the numbering is constant and may be known in advance.
TIP: An example program which uses the interface can be found here:
This specifies any shell prompt running on the target
root:/> cd /sys/bus/iio/devices/ root:/sys/bus/iio/devices> ls iio:device0 trigger0 root:/sys/bus/iio/devices> cd iio:device0 root:/sys/bus/iio/devices/iio:device0> ls -l total 0 drwxr-xr-x 2 root root 0 Jul 12 10:17 buffer -rw-r--r-- 1 root root 4096 Jul 12 10:17 current_timestamp_clock -r--r--r-- 1 root root 4096 Jul 12 10:17 dev -rw-r--r-- 1 root root 4096 Jul 12 10:17 filter_low_pass_3db_frequency -rw-r--r-- 1 root root 4096 Jul 12 10:17 in_accel_scale -rw-r--r-- 1 root root 4096 Jul 12 10:17 in_accel_x_calibbias -rw-r--r-- 1 root root 4096 Jul 12 10:17 in_accel_x_raw -rw-r--r-- 1 root root 4096 Jul 12 10:17 in_accel_y_calibbias -rw-r--r-- 1 root root 4096 Jul 12 10:17 in_accel_y_raw -rw-r--r-- 1 root root 4096 Jul 12 10:17 in_accel_z_calibbias -rw-r--r-- 1 root root 4096 Jul 12 10:17 in_accel_z_raw -rw-r--r-- 1 root root 4096 Jul 12 10:17 in_anglvel_scale -rw-r--r-- 1 root root 4096 Jul 12 10:17 in_anglvel_x_calibbias -rw-r--r-- 1 root root 4096 Jul 12 10:17 in_anglvel_x_raw -rw-r--r-- 1 root root 4096 Jul 12 10:17 in_anglvel_y_calibbias -rw-r--r-- 1 root root 4096 Jul 12 10:17 in_anglvel_y_raw -rw-r--r-- 1 root root 4096 Jul 12 10:17 in_anglvel_z_calibbias -rw-r--r-- 1 root root 4096 Jul 12 10:17 in_anglvel_z_raw -rw-r--r-- 1 root root 4096 Jul 12 10:17 in_temp0_raw -rw-r--r-- 1 root root 4096 Jul 12 10:17 in_temp0_scale -r--r--r-- 1 root root 4096 Jul 12 10:17 name lrwxrwxrwx 1 root root 0 Jul 12 10:17 of_node -> ../../../../../../../../firmware/devicetree/base/soc/spi@7e204000/adis16475@0 drwxr-xr-x 2 root root 0 Jul 12 10:17 power -rw-r--r-- 1 root root 4096 Jul 12 10:17 sampling_frequency drwxr-xr-x 2 root root 0 Jul 12 10:17 scan_elements lrwxrwxrwx 1 root root 0 Jul 12 10:17 subsystem -> ../../../../../../../../bus/iio drwxr-xr-x 2 root root 0 Jul 12 10:17 trigger -rw-r--r-- 1 root root 4096 Jul 12 10:17 uevent root:/sys/bus/iio/devices/iio:device0>
For a detailed description please see: Documentation/ABI/testing/sysfs-bus-iio
3-Axis Accelerometer related device files | Description |
---|---|
in_accel_scale | Scale for the accelerometer channels. |
in_accel_x_calibbias | Calibration offset for the X-axis accelerometer channel. |
in_accel_x_raw | Raw X-axis accelerometer channel value. |
in_accel_y_calibbias | Calibration offset for the Y-axis accelerometer channel. |
in_accel_y_raw | Raw Y-axis accelerometer channel value. |
in_accel_z_calibbias | Calibration offset for the Z-axis accelerometer channel. |
in_accel_z_raw | Raw Z-axis accelerometer channel value. |
3-Axis Gyro related device files | Description |
in_anglvel_scale | Scale for the gyroscope channels. |
in_anglvel_x_calibbias | Calibration offset for the X-axis gyroscope channel. |
in_anglvel_x_raw | Raw X-axis gyroscope channel value. |
in_anglvel_y_calibbias | Calibration offset for the Y-axis gyroscope channel. |
in_anglvel_y_raw | Raw Y-axis gyroscope channel value. |
in_anglvel_z_calibbias | Calibration offset for the Z-axis gyroscope channel. |
in_anglvel_z_raw | Raw Z-axis gyroscope channel value. |
Temperature sensor related files | Description |
in_temp0_raw | Raw temperature channel value. |
in_temp0_scale | Scale for the temperature sensor channel. |
Miscellaneous device files | Description |
name | Name of the IIO device. |
sampling_frequency | Currently selected sample rate. |
filter_low_pass_3db_frequency | Bandwidth for the accelerometer and gyroscope channels. |
burst_mode_enable | Enables reading of the data with a SPI burst read. |
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device0> cat name adis16477-1
The sampling frequency of the device can be set by writing the desired value to the sampling_frequency
file. The driver will automatically round up to the nearest supported sampling frequency.
Example:
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device0> cat sampling_frequency 2000.000000 pi@raspberrypi:/s root:/sys/bus/iio/devices/iio:device0> echo 1000 > sampling_frequency root:/sys/bus/iio/devices/iio:device0> cat sampling_frequency 1000.000000
A channel value can be read from its _raw
attribute. The value returned by the _raw
attribute is the raw value as reported by the device. To get the processed value of the channel in a standardized unit add the channels _offset
attribute to the _raw
value and multiply the result by _scale
attribute. If no _offset
attribute is present assume 0 for the offset.
processed value = (raw + offset) * scale
The units by the IIO framework are:
Example:
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device0> cat in_accel_z_raw 52612913 root:/sys/bus/iio/devices/iio:device0> cat in_accel_scale 0.000000187
Z-axis acceleration = in_accel_z_raw * in_accel_scale = 52612913 * 0.000000187 m/s^2 = 9.838 m/s^2
The gyro and accel bandwidth can be set by writing the desired value to the filter_low_pass_3db_frequency
attribute. The driver will automatically round up to the nearest supported bandwidth.
Example:
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device0> cat filter_low_pass_3db_frequency 720.000000 root:/sys/bus/iio/devices/iio:device0> echo 360 > filter_low_pass_3db_frequency root:/sys/bus/iio/devices/iio:device0> cat filter_low_pass_3db_frequency 360.000000
This driver only supports it's own default trigger source adis16477-1-dev0
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device0> cat trigger/current_trigger adis16477-1-dev0
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device0/buffer> ls data_available enable length watermark
The Industrial I/O subsystem provides support for various ring buffer based data acquisition methods. Apart from device specific hardware buffer support, the user can chose between two different software ring buffer implementations. One is the IIO lock free software ring, and the other is based on Linux kfifo. Devices with buffer support feature an additional sub-folder in the /sys/bus/iio/devices/deviceX/ folder hierarchy. Called deviceX:bufferY, where Y defaults to 0, for devices with a single buffer.
Every buffer implementation features a set of files:
length
Get/set the number of sample sets that may be held by the buffer.
enable
Enables/disables the buffer. This file should be written last, after length and selection of scan elements.
watermark
A single positive integer specifying the maximum number of scan
elements to wait for.
Poll will block until the watermark is reached.
Blocking read will wait until the minimum between the requested
read amount or the low water mark is available.
Non-blocking read will retrieve the available samples from the
buffer even if there are less samples then watermark level. This
allows the application to block on poll with a timeout and read
the available samples after the timeout expires and thus have a
maximum delay guarantee.
data_available
A read-only value indicating the bytes of data available in the
buffer. In the case of an output buffer, this indicates the
amount of empty space available to write data to. In the case of
an input buffer, this indicates the amount of data available for
reading.
length_align_bytes
Using the high-speed interface. DMA buffers may have an alignment requirement for the buffer length.
Newer versions of the kernel will report the alignment requirements
associated with a device through the `length_align_bytes` property.
scan_elements
The scan_elements directory contains interfaces for elements that will be captured for a single triggered sample set in the buffer.
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device0/scan_elements> ls -l total 0 -rw-r--r-- 1 root root 4096 Jul 12 10:17 in_accel_x_en -r--r--r-- 1 root root 4096 Jul 12 10:17 in_accel_x_index -r--r--r-- 1 root root 4096 Jul 12 10:17 in_accel_x_type -rw-r--r-- 1 root root 4096 Jul 12 10:17 in_accel_y_en -r--r--r-- 1 root root 4096 Jul 12 10:17 in_accel_y_index -r--r--r-- 1 root root 4096 Jul 12 10:17 in_accel_y_type -rw-r--r-- 1 root root 4096 Jul 12 10:17 in_accel_z_en -r--r--r-- 1 root root 4096 Jul 12 10:17 in_accel_z_index -r--r--r-- 1 root root 4096 Jul 12 10:17 in_accel_z_type -rw-r--r-- 1 root root 4096 Jul 12 10:17 in_anglvel_x_en -r--r--r-- 1 root root 4096 Jul 12 10:17 in_anglvel_x_index -r--r--r-- 1 root root 4096 Jul 12 10:17 in_anglvel_x_type -rw-r--r-- 1 root root 4096 Jul 12 10:17 in_anglvel_y_en -r--r--r-- 1 root root 4096 Jul 12 10:17 in_anglvel_y_index -r--r--r-- 1 root root 4096 Jul 12 10:17 in_anglvel_y_type -rw-r--r-- 1 root root 4096 Jul 12 10:17 in_anglvel_z_en -r--r--r-- 1 root root 4096 Jul 12 10:17 in_anglvel_z_index -r--r--r-- 1 root root 4096 Jul 12 10:17 in_anglvel_z_type -rw-r--r-- 1 root root 4096 Jul 12 10:17 in_flags0_en -r--r--r-- 1 root root 4096 Jul 12 10:17 in_flags0_index -r--r--r-- 1 root root 4096 Jul 12 10:17 in_flags0_type -rw-r--r-- 1 root root 4096 Jul 12 10:17 in_flags1_crc_en -r--r--r-- 1 root root 4096 Jul 12 10:17 in_flags1_crc_index -r--r--r-- 1 root root 4096 Jul 12 10:17 in_flags1_crc_type -rw-r--r-- 1 root root 4096 Jul 12 10:17 in_temp0_en -r--r--r-- 1 root root 4096 Jul 12 10:17 in_temp0_index -r--r--r-- 1 root root 4096 Jul 12 10:17 in_temp0_type -rw-r--r-- 1 root root 4096 Jul 12 10:17 in_timestamp_en -r--r--r-- 1 root root 4096 Jul 12 10:17 in_timestamp_index -r--r--r-- 1 root root 4096 Jul 12 10:17 in_timestamp_type root:/sys/bus/iio/devices/iio:device0/scan_elements>
From the above list, note the following 2 elements:
in_voltageX_en / in_voltageX-voltageY_en / timestamp_en:
Scan element control for triggered data capture.
Writing 1 will enable the scan element, writing 0 will disable it
in_voltageX_type / in_voltageX-voltageY_type / timestamp_type:
Description of the scan element data storage within the buffer
and therefore in the form in which it is read from user-space.
Form is [s|u]bits/storage-bits. s or u specifies if signed
(2's complement) or unsigned. bits is the number of bits of
data and storage-bits is the space (after padding) that it
occupies in the buffer. Note that some devices will have
additional information in the unused bits so to get a clean
value, the bits value must be used to mask the buffer output
value appropriately. The storage-bits value also specifies the
data alignment. So u12/16 will be a unsigned 12 bit integer
stored in a 16 bit location aligned to a 16 bit boundary.
For other storage combinations this attribute will be extended
appropriately.
in_voltageX_index / in_voltageX-voltageY_index / timestamp_index:
A single positive integer specifying the position of this
scan element in the buffer. Note these are not dependent on
what is enabled and may not be contiguous. Thus for user-space
to establish the full layout these must be used in conjunction
with all _en attributes to establish which channels are present,
and the relevant _type attributes to establish the data storage
format.