This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:linux-drivers:iio-gyroscope:adis16130 [30 Aug 2011 10:32] – [Driver testing] Michael Hennerich | resources:tools-software:linux-drivers:iio-gyroscope:adis16130 [11 Feb 2016 21:02] (current) – [Status] Lars-Peter Clausen | ||
---|---|---|---|
Line 3: | Line 3: | ||
===== Supported Devices ===== | ===== Supported Devices ===== | ||
- | This driver supports the\\ | + | * [[adi> |
- | [[adi> | + | |
===== Description ===== | ===== Description ===== | ||
Line 16: | Line 15: | ||
===== Status ===== | ===== Status ===== | ||
- | ^ Source | + | ^ Source ^ Mainlined? ^ |
- | | [[bfgit>linux-kernel?drivers/ | + | | [[git.linux.org>drivers/ |
===== Files ===== | ===== Files ===== | ||
Line 63: | Line 62: | ||
"make qconfig" | "make qconfig" | ||
- | <note> | + | <WRAP round help> |
The ADIS16130 Driver depends on **CONFIG_SPI** | The ADIS16130 Driver depends on **CONFIG_SPI** | ||
- | </note> | + | </WRAP> |
< | < | ||
Line 93: | Line 92: | ||
{{page> | {{page> | ||
- | < | + | <WRAP box bggreen>< |
< | < | ||
root:/> **cd / | root:/> **cd / | ||
Line 110: | Line 109: | ||
-rw-r--r-- | -rw-r--r-- | ||
root:/ | root:/ | ||
- | </ | + | </ |
=== Show device name === | === Show device name === | ||
- | < | + | <WRAP box bggreen>< |
< | < | ||
root:/ | root:/ | ||
adis16130 | adis16130 | ||
- | </ | + | </ |
=== ADIS16130 device attributes === | === ADIS16130 device attributes === |