Wiki

This version is outdated by a newer approved version.DiffThis version (24 Mar 2020 21:42) was approved by Robin Getz.The Previously approved version (29 Oct 2019 08:45) is available.Diff

This is an old revision of the document!


AXI DAC HDL Linux Driver

Supported Devices

Supported Boards

Supported HDL Cores

Sub device Documentation (linked mode)

Description

The AXI DAC DDS HDL driver is the driver for various HDL interface cores which are used on different FPGA designs. The driver is implemented as an Linux IIO driver. It's register map can be found here: Base register map (common to all cores)

This driver is independent from the physical layer. So it's being used with CMOS or LVDS type interfaces or the JESD204 Interface Framework.

There are basically two use case scenarios for this driver, in which this driver controls only the HDL/FPGA transport layer capture core. This mode is called standalone mode, and the converter is fully configured and controlled by a separate driver. The Linux common clock framework is utilized so that this driver knows the sampling frequency of the connected converter DAC device. Alternatively this driver can also be used in a linked mode, where the converter device typically a SPI device must instantiate first. If this has happened this AXI-DAC driver will then probe as well. (Deferred probe mechanism) Finally both the HDL core platform device together with the converter SPI device will register a common IIO device, which will then exhibit a common set of attributes and channels. The converter SPI device driver is handled in a separate source file, which can be found in the same directory this driver exists. The device tree phandle “spibus-connected” is used to connect the AXI-DAC driver with the SPI control driver.

Sometimes there is a common HDL/FPGA transport layer core, which handles both RX/TX or ADC/DMA. This single physical core is then handled by two independent IIO drivers each for one transport data direction. It’s physical address register space is then also split or divided, typically spaced by 0x4000. A good example for this case is the AXI_AD9361 HDL core.

The HDL/FPGA transport layer capture core driver portion implements a polyphase dual tone DDS core per channel together with an DMA based waveform buffer mechanism. The buffer can be filled by arbitrary data, which is then typically cyclically repeated or used in a streaming fashion.

Source Code

Status

Files

Example platform device initialization

The AXI DAC/DDS driver is a platform driver and can only be instantiated via device tree.

Required devicetree properties:

  • compatible: Should always be one of these:
    • adi,axi-ad9122-6.00.a
    • adi,axi-ad9136-1.0
    • adi,axi-ad9144-1.0
    • adi,axi-ad9162-1.0
    • adi,axi-ad9172-1.0
    • adi,axi-ad9361x2-dds-6.00.a
    • adi,axi-ad9361-dds-6.00.a
    • adi,axi-ad9364-dds-6.00.a
    • adi,axi-ad9371-tx-1.0
    • adi,axi-ad9739a-8.00.b
    • adi,axi-ad9963-dds-1.00.a
    • adi,axi-adrv9009-tx-1.0
  • reg: Base address and register area size. This parameter expects a register range.

Optional Parameters:

  • adi,axi-dds-default-scale: The power up DDS scale in 16-bit fractional representation. On driver probe the default mode is DDS with some default frequency at 0.25 Full Scale. Often this behavior is undesired. The best way to mute the DDS on startup is to set this to 0.
  • adi,axi-dds-default-frequency: The power up DDS frequency for all tones.
  • adi,axi-dds-parity-enable: If set the HDL core uses Parity Mode. (Default is Frame Mode)
  • adi,axi-dds-parity-type-odd: If set the HDL core use odd parity. (Default is even)
  • adi,axi-dds-1-rf-channel: If set the HDL core expects 1 RF channel. (Default 2 channels)
  • adi,axi-interpolation-core-available: If the FPGA system features an additional interpolation filter, this attribute should be set.
  • adi,axi-pl-fifo-enable: If the FPGA system features a PL FIFO (Programmable Logic), this attribute should be set.
  • dmas: DMA specifiers for the tx dma. See the DMA client binding: Documentation/devicetree/bindings/dma/dma.txt
  • dma-names: DMA request name. Should be “tx” if a dma is present.
  • spibus-connected: Phandle to the SPI device (control interface) on which the DAC can be found

Example:

&spi0 {
	status = "okay";

	adc0_ad9361: ad9361-phy@0 {
		#address-cells = <1>;
		#size-cells = <0>;
		#clock-cells = <1>;
		compatible = "ad9361";

		/* SPI Setup */
		reg = <0>;
		spi-cpha;
		spi-max-frequency = <10000000>;

		/* Clocks */
		clocks = <&ad9361_clkin 0>;
		clock-names = "ad9361_ext_refclk";
		clock-output-names = "rx_sampl_clk", "tx_sampl_clk";

	[--- snip ---]

	}
}

&fpga_axi {
	tx_dma: dma@7c420000 {
		compatible = "adi,axi-dmac-1.00.a";
		reg = <0x7c420000 0x10000>;
		#dma-cells = <1>;
		interrupts = <0 56 0>;
		clocks = <&clkc 16>;

		dma-channel {
			adi,source-bus-width = <64>;
			adi,destination-bus-width = <64>;
			adi,type = <1>;
			adi,cyclic;
		};
	};

	cf_ad9361_dac_core_0: cf-ad9361-dds-core-lpc@79024000 {
		compatible = "adi,axi-ad9361-dds-6.00.a";
		reg = <0x79024000 0x1000>;
		clocks = <&adc0_ad9361 13>;
		clock-names = "sampl_clk";
		dmas = <&tx_dma 0>;
		dma-names = "tx";
		adi,axi-dds-default-scale = <0>;
	};
};	

Enabling Linux driver support

Configure kernel with “make menuconfig” (alternatively use “make xconfig” or “make qconfig”)

The AXI ADC HDL driver may depend on CONFIG_SPI

Adding Linux driver support

Configure kernel with “make menuconfig” (alternatively use “make xconfig” or “make qconfig”)

Linux Kernel Configuration
	Device Drivers  --->
	<*>     Industrial I/O support --->
	    --- Industrial I/O support
	    -*-   Enable ring buffer support within IIO
	    -*-     Industrial I/O lock free software ring
	    -*-   Enable triggered sampling support

	          *** Direct Digital Synthesis ***
	    [--snip--]

		<*>   Analog Devices CoreFPGA AXI DDS driver
		<*>   Analog Devices AD9122 DAC

	    [--snip--]

Hardware configuration

In case the driver probes successfully and the device gets instantiated. Your systems kernel messages should include a line, which may look like the one shown below.

cf_axi_dds 79024000.cf-ad9361-dds-core-lpc: Analog Devices CF_AXI_DDS_DDS MASTER (8.00.b) at 0x79024000 mapped to 0xf0998000, probed DDS AD9361

Driver testing

Each and every IIO device, typically a hardware chip, has a device folder under /sys/bus/iio/devices/iio:deviceX. Where X is the IIO index of the device. Under every of these directory folders reside a set of files, depending on the characteristics and features of the hardware device in question. These files are consistently generalized and documented in the IIO ABI documentation. In order to determine which IIO deviceX corresponds to which hardware device, the user can read the name file /sys/bus/iio/devices/iio:deviceX/name. In case the sequence in which the iio device drivers are loaded/registered is constant, the numbering is constant and may be known in advance.

02 Mar 2011 15:16

Some device attributes control the DDS HDL Core, others features of the DAC and associated clock providers.

This specifies any shell prompt running on the target

analog:/sys/bus/iio/devices/iio:device2# cd /sys/bus/iio/devices/
root@analog:/sys/bus/iio/devices# ls
iio:device0  iio:device1  iio:device2  iio:device3
root@analog:/sys/bus/iio/devices#

root@analog:/sys/bus/iio/devices# cd iio\:device2
root@analog:/sys/bus/iio/devices/iio:device2# ls -l
total 0
drwxr-xr-x 5 root root    0 Jan  1 00:00 .
drwxr-xr-x 4 root root    0 Jan  1 00:00 ..
drwxrwxrwx 2 root root    0 Jan  1 00:00 buffer
-rw-rw-rw- 1 root root 4096 Jan  1 00:00 dev
-rw-rw-rw- 1 root root 4096 Jan  1 00:00 name
lrwxrwxrwx 1 root root    0 Jan  1 00:00 of_node -> ../../../../../firmware/devicetree/base/fpga-axi@0/cf-ad9361-dds-core-lpc@79024000
-rw-rw-rw- 1 root root 4096 Jan  1 00:00 out_altvoltage0_TX1_I_F1_frequency
-rw-rw-rw- 1 root root 4096 Jan  1 00:00 out_altvoltage0_TX1_I_F1_phase
-rw-rw-rw- 1 root root 4096 Jan  1 00:00 out_altvoltage0_TX1_I_F1_raw
-rw-rw-rw- 1 root root 4096 Jan  1 00:00 out_altvoltage0_TX1_I_F1_scale
-rw-rw-rw- 1 root root 4096 Jan  1 00:00 out_altvoltage1_TX1_I_F2_frequency
-rw-rw-rw- 1 root root 4096 Jan  1 00:00 out_altvoltage1_TX1_I_F2_phase
-rw-rw-rw- 1 root root 4096 Jan  1 00:00 out_altvoltage1_TX1_I_F2_raw
-rw-rw-rw- 1 root root 4096 Jan  1 00:00 out_altvoltage1_TX1_I_F2_scale
-rw-rw-rw- 1 root root 4096 Jan  1 00:00 out_altvoltage2_TX1_Q_F1_frequency
-rw-rw-rw- 1 root root 4096 Jan  1 00:00 out_altvoltage2_TX1_Q_F1_phase
-rw-rw-rw- 1 root root 4096 Jan  1 00:00 out_altvoltage2_TX1_Q_F1_raw
-rw-rw-rw- 1 root root 4096 Jan  1 00:00 out_altvoltage2_TX1_Q_F1_scale
-rw-rw-rw- 1 root root 4096 Jan  1 00:00 out_altvoltage3_TX1_Q_F2_frequency
-rw-rw-rw- 1 root root 4096 Jan  1 00:00 out_altvoltage3_TX1_Q_F2_phase
-rw-rw-rw- 1 root root 4096 Jan  1 00:00 out_altvoltage3_TX1_Q_F2_raw
-rw-rw-rw- 1 root root 4096 Jan  1 00:00 out_altvoltage3_TX1_Q_F2_scale
-rw-rw-rw- 1 root root 4096 Jan  1 00:00 out_altvoltage4_TX2_I_F1_frequency
-rw-rw-rw- 1 root root 4096 Jan  1 00:00 out_altvoltage4_TX2_I_F1_phase
-rw-rw-rw- 1 root root 4096 Jan  1 00:00 out_altvoltage4_TX2_I_F1_raw
-rw-rw-rw- 1 root root 4096 Jan  1 00:00 out_altvoltage4_TX2_I_F1_scale
-rw-rw-rw- 1 root root 4096 Jan  1 00:00 out_altvoltage5_TX2_I_F2_frequency
-rw-rw-rw- 1 root root 4096 Jan  1 00:00 out_altvoltage5_TX2_I_F2_phase
-rw-rw-rw- 1 root root 4096 Jan  1 00:00 out_altvoltage5_TX2_I_F2_raw
-rw-rw-rw- 1 root root 4096 Jan  1 00:00 out_altvoltage5_TX2_I_F2_scale
-rw-rw-rw- 1 root root 4096 Jan  1 00:00 out_altvoltage6_TX2_Q_F1_frequency
-rw-rw-rw- 1 root root 4096 Jan  1 00:00 out_altvoltage6_TX2_Q_F1_phase
-rw-rw-rw- 1 root root 4096 Jan  1 00:00 out_altvoltage6_TX2_Q_F1_raw
-rw-rw-rw- 1 root root 4096 Jan  1 00:00 out_altvoltage6_TX2_Q_F1_scale
-rw-rw-rw- 1 root root 4096 Jan  1 00:00 out_altvoltage7_TX2_Q_F2_frequency
-rw-rw-rw- 1 root root 4096 Jan  1 00:00 out_altvoltage7_TX2_Q_F2_phase
-rw-rw-rw- 1 root root 4096 Jan  1 00:00 out_altvoltage7_TX2_Q_F2_raw
-rw-rw-rw- 1 root root 4096 Jan  1 00:00 out_altvoltage7_TX2_Q_F2_scale
-rw-rw-rw- 1 root root 4096 Jan  1 00:00 out_altvoltage_sampling_frequency
-rw-rw-rw- 1 root root 4096 Jan  1 00:00 out_voltage0_calibphase
-rw-rw-rw- 1 root root 4096 Jan  1 00:00 out_voltage0_calibscale
-rw-rw-rw- 1 root root 4096 Jan  1 00:00 out_voltage1_calibphase
-rw-rw-rw- 1 root root 4096 Jan  1 00:00 out_voltage1_calibscale
-rw-rw-rw- 1 root root 4096 Jan  1 00:00 out_voltage2_calibphase
-rw-rw-rw- 1 root root 4096 Jan  1 00:00 out_voltage2_calibscale
-rw-rw-rw- 1 root root 4096 Jan  1 00:00 out_voltage3_calibphase
-rw-rw-rw- 1 root root 4096 Jan  1 00:00 out_voltage3_calibscale
-rw-rw-rw- 1 root root 4096 Jan  1 00:00 out_voltage_sampling_frequency
drwxrwxrwx 2 root root    0 Jan  1 00:00 power
drwxrwxrwx 2 root root    0 Jan  1 00:00 scan_elements
lrwxrwxrwx 1 root root    0 Jan  1 00:00 subsystem -> ../../../../../bus/iio
-rw-rw-rw- 1 root root 4096 Jan  1 00:00 uevent
root@analog:/sys/bus/iio/devices/iio:device2#

Show device name

This specifies any shell prompt running on the target

root@analog:/sys/bus/iio/devices/iio:device2# cat name
cf-ad9361-dds-core-lpc

Show/Set DDS frequency

Values are in Hz.

This specifies any shell prompt running on the target

root@analog:/sys/bus/iio/devices/iio:device2# cat out_altvoltage0_TX1_I_F1_frequency
9279985
root@analog:/sys/bus/iio/devices/iio:device2# echo 500000 > out_altvoltage0_TX1_I_F1_frequency
root@analog:/sys/bus/iio/devices/iio:device2# cat out_altvoltage0_TX1_I_F1_frequency
500163

Show/Set DDS Phase

Values are in milli degrees.

This specifies any shell prompt running on the target

root@analog:/sys/bus/iio/devices/iio:device2# cat out_altvoltage0_TX1_I_F1_phase
89995
root@analog:/sys/bus/iio/devices/iio:device2# echo 91000 > out_altvoltage0_TX1_I_F1_phase
root@analog:/sys/bus/iio/devices/iio:device2# cat out_altvoltage0_TX1_I_F1_phase
90995

Enable/Disable DDS Channel

1 for enable, 0 for disable.

With the introduction of the big channel MUX (REG_CHAN_CNTRL_7, DAC_DDS_SEL) starting with HDV Version > 7.00, the RAW attribute has some side effects, that need to be understood. In many situations for example when the Buffer mode is used, it’s not desirable to write this attribute.

HDL Version < 7.00.a

HDL Version > 7.00.a

This specifies any shell prompt running on the target

root@analog:/sys/bus/iio/devices/iio:device2# cat out_altvoltage0_TX1_I_F1_raw
1

Show/Set DDS Scale

DDS amplitude: range 0.00 … 1.00 (relative to full scale)

When disabling the DAC Buffer/DMA mode and a transition into DDS tone output mode is not desired - Scale of all channels should be set to 0.00. See also device tree attribute: adi,axi-dds-default-scale

This specifies any shell prompt running on the target

root@analog:/sys/bus/iio/devices/iio:device2# cat out_altvoltage0_TX1_I_F1_scale
0.500000
root@analog:/sys/bus/iio/devices/iio:device2# cat out_altvoltage0_TX1_I_F1_scale
1.000000 0.500000 0.250000 0.125000 ...
root@analog:/sys/bus/iio/devices/iio:device2# echo 0.25 > out_altvoltage0_TX1_I_F1_scale
root@analog:/sys/bus/iio/devices/iio:device2# cat out_altvoltage0_TX1_I_F1_scale
0.250000

DAC internal or external Gain, DC Offset, and Phase adjustments

Depending on the platform. These attributes may control converter internal or external processing blocks.

The AD9122 features Gain, DC Offset, and Phase adjustment for sideband suppression. These features can be controlled via following attributes:

  • out_voltage0_calibbias
  • out_voltage0_calibscale
  • out_voltage0_phase
  • out_voltage1_calibbias
  • out_voltage1_calibscale
  • out_voltage1_phase

This specifies any shell prompt running on the target

root@analog:/sys/bus/iio/devices/iio:device2# grep “” out_voltage* 
out_voltage0_calibbias:0
out_voltage0_calibscale:505
out_voltage0_phase:0
out_voltage1_calibbias:0
out_voltage1_calibscale:505
out_voltage1_phase:0

Buffer management

This specifies any shell prompt running on the target

root:/sys/bus/iio/devices/iio:device3> ls -l buffer
total 0
-rw-r--r--    1 root     root          4096 Jan  1 00:12 enable
-rw-r--r--    1 root     root          4096 Jan  1 00:12 length
-r--r--r--    1 root     root          4096 Jan  1 00:12 watermark

The Industrial I/O subsystem provides support for various ring buffer based data acquisition methods. Apart from device specific hardware buffer support, the user can chose between two different software ring buffer implementations. One is the IIO lock free software ring, and the other is based on Linux kfifo. Devices with buffer support feature an additional sub-folder in the /sys/bus/iio/devices/deviceX/ folder hierarchy. Called deviceX:bufferY, where Y defaults to 0, for devices with a single buffer.

Every buffer implementation features a set of files:

length
Get/set the number of sample sets that may be held by the buffer.

enable
Enables/disables the buffer. This file should be written last, after length and selection of scan elements.

watermark
A single positive integer specifying the maximum number of scan elements to wait for. Poll will block until the watermark is reached. Blocking read will wait until the minimum between the requested read amount or the low water mark is available. Non-blocking read will retrieve the available samples from the buffer even if there are less samples then watermark level. This allows the application to block on poll with a timeout and read the available samples after the timeout expires and thus have a maximum delay guarantee.

data_available
A read-only value indicating the bytes of data available in the buffer. In the case of an output buffer, this indicates the amount of empty space available to write data to. In the case of an input buffer, this indicates the amount of data available for reading.

length_align_bytes
Using the high-speed interface. DMA buffers may have an alignment requirement for the buffer length. Newer versions of the kernel will report the alignment requirements associated with a device through the `length_align_bytes` property.

scan_elements
The scan_elements directory contains interfaces for elements that will be captured for a single triggered sample set in the buffer.

02 Mar 2011 15:16

This specifies any shell prompt running on the target

root:/sys/bus/iio/devices/iio:device3> ls -l scan_elements
total 0
-rw-r--r--    1 root     root          4096 Jan  1 00:00 out_voltage0_en
-r--r--r--    1 root     root          4096 Jan  1 00:00 out_voltage0_index
-r--r--r--    1 root     root          4096 Jan  1 00:00 out_voltage0_type
-rw-r--r--    1 root     root          4096 Jan  1 00:00 out_voltage1_en
-r--r--r--    1 root     root          4096 Jan  1 00:00 out_voltage1_index
-r--r--r--    1 root     root          4096 Jan  1 00:00 out_voltage1_type

in_voltageX_en / in_voltageX-voltageY_en / timestamp_en:
Scan element control for triggered data capture. Writing 1 will enable the scan element, writing 0 will disable it

in_voltageX_type / in_voltageX-voltageY_type / timestamp_type:
Description of the scan element data storage within the buffer and therefore in the form in which it is read from user-space. Form is [s|u]bits/storage-bits. s or u specifies if signed (2's complement) or unsigned. bits is the number of bits of data and storage-bits is the space (after padding) that it occupies in the buffer. Note that some devices will have additional information in the unused bits so to get a clean value, the bits value must be used to mask the buffer output value appropriately. The storage-bits value also specifies the data alignment. So u12/16 will be a unsigned 12 bit integer stored in a 16 bit location aligned to a 16 bit boundary. For other storage combinations this attribute will be extended appropriately.

in_voltageX_index / in_voltageX-voltageY_index / timestamp_index:
A single positive integer specifying the position of this scan element in the buffer. Note these are not dependent on what is enabled and may not be contiguous. Thus for user-space to establish the full layout these must be used in conjunction with all _en attributes to establish which channels are present, and the relevant _type attributes to establish the data storage format.

02 Mar 2011 15:16

Low level register access

Some IIO drivers feature an optional debug facility, allowing users to read or write registers directly. Special care needs to be taken when using this feature, since you can modify registers on the back of the driver.

To simplify direct register access you may want to use the libiio iio_reg command line utility.

Accessing debugfs requires root privileges.

In order to identify if the IIO device in question feature this option you first need to identify the IIO device number.

Therefore read the name attribute of each IIO device

This specifies any shell prompt running on the target

root@analog:~# grep "" /sys/bus/iio/devices/iio\:device*/name
/sys/bus/iio/devices/iio:device0/name:ad7291
/sys/bus/iio/devices/iio:device1/name:ad9361-phy
/sys/bus/iio/devices/iio:device2/name:xadc
/sys/bus/iio/devices/iio:device3/name:adf4351-udc-rx-pmod
/sys/bus/iio/devices/iio:device4/name:adf4351-udc-tx-pmod
/sys/bus/iio/devices/iio:device5/name:cf-ad9361-dds-core-lpc
/sys/bus/iio/devices/iio:device6/name:cf-ad9361-lpc
root@analog:~# 

Change directory to /sys/kernel/debug/iio/ iio:deviceX and check if the direct_reg_access file exists.

This specifies any shell prompt running on the target

root@analog:~# cd /sys/kernel/debug/iio/iio\:device1
root@analog:/sys/kernel/debug/iio/iio:device1# ls direct_reg_access 
direct_reg_access

Reading

This specifies any shell prompt running on the target

root@analog:/sys/kernel/debug/iio/iio:device1# echo 0x7 > direct_reg_access                                                                                                                                 
root@analog:/sys/kernel/debug/iio/iio:device1# cat direct_reg_access 
0x40

Writing

Write ADDRESS VALUE

This specifies any shell prompt running on the target

root@analog:/sys/kernel/debug/iio/iio:device1# echo 0x7 0x50  > direct_reg_access                                                                                                                            
root@analog:/sys/kernel/debug/iio/iio:device1# cat direct_reg_access 
0x50

Accessing HDL CORE registers

Special ADI device driver convention for devices that have both:

  • a SPI/I2C control interface
  • and some sort of HDL Core with registers (AXI)

In this case when accessing the HDL Core Registers always set BIT31.

The register map for typical ADI HDL cores can be found here: Register Map

This specifies any shell prompt running on the target

root@analog:/sys/kernel/debug/iio/iio:device6# echo 0x80000000 > direct_reg_access                                                                                                                           
root@analog:/sys/kernel/debug/iio/iio:device6# cat direct_reg_access 
0x80062

02 Mar 2011 15:16

AD9122 Clocking concept

There are three different clocks associated with the DAC.

  • Data/Interface Clock (DCI)
  • DAC Clock (DACCLK)
  • Reference Clock (REFCLK)

The Data/Interface Clock (DCI) is shared with the DDS HDL Core.

The default AD9122 driver configuration uses a concept called Direct Clocking. This means an external clock provider must supply DCI and DACCLK. In case the DAC interpolation feature is not used and the DAC operates in Word-Mode then DCI = DACCLK.

When N interpolation is used following equation must be satisfied.

N = {1, 2, 4, 8}

DACCLK = N * DCI and DACCLK ⇐ 1230MHz

The out_altvoltage_interpolation_frequency_available attribute allows you to query the supported interpolation frequencies for a given Interface Clock (out_altvoltage_X_sampling_frequency) by exercising possible settings on the clock provider. In case the clock provider is not capable providing exactly the requested rate, the mode is removed from the list.

So following example:

Assuming the clock provider can only provide following rates: 1000MHz / X, X = {1..1023}.

This results in following rates:

1000, 500, 333.33, 250, 200, 166.66, 142.85, 125, 111.11, …

  • In case the interface clock is set to 125MHz, then 1x, 2x, 4x and 8x interpolation is possible.
  • Assuming the interface clock is set to 166.66MHz, then only 1x, 2x interpolation is possible. 4x interpolation won't work since 666.66MHz cannot be supplied by the clock provider.

The half-band interpolation filters have selectable pass bands that allow the center frequencies to be moved in increments of one-half their input data rate. The premodulation block provides a digital upconversion of the incoming waveform by one-half the incoming data rate, fDATA. This can be used to frequency-shift base- band input data to the center of the interpolation filter pass band.

The available center shift frequencies for a given Interface Clock (out_altvoltage_X_sampling_frequency), can be queried using the out_altvoltage_interpolation_center_shift_frequency_available attribute.

This specifies any shell prompt running on the target

 
root@linaro-ubuntu-desktop:/sys/bus/iio/devices/iio:device4# cat out_altvoltage_1A_sampling_frequency
491520000

root@linaro-ubuntu-desktop:/sys/bus/iio/devices/iio:device4# cat out_altvoltage_interpolation_frequency_available
491520000 983040000

root@linaro-ubuntu-desktop:/sys/bus/iio/devices/iio:device4# cat out_altvoltage_interpolation_frequency
491520000

root@linaro-ubuntu-desktop:/sys/bus/iio/devices/iio:device4# cat out_altvoltage_interpolation_center_shift_frequency
0

This specifies any shell prompt running on the target


[ Set data clock to 122.88 MHz ]

root@linaro-ubuntu-desktop:/sys/bus/iio/devices/iio:device4# echo 122880000 > out_altvoltage_1A_sampling_frequency

[ List available interpolation DAC frequencies ]

root@linaro-ubuntu-desktop:/sys/bus/iio/devices/iio:device4# cat out_altvoltage_interpolation_frequency_available
122880000 245760000 491520000 983040000

[ Select 8x interpolation ]

root@linaro-ubuntu-desktop:/sys/bus/iio/devices/iio:device4# echo 983040000 > out_altvoltage_interpolation_frequency

[ List available center shift frequencies ]

root@linaro-ubuntu-desktop:/sys/bus/iio/devices/iio:device4# cat out_altvoltage_interpolation_center_shift_frequency_available
0 61440000 122880000 184320000 245760000 307200000 368640000 430080000 491520000 552960000 614400000 675840000 737280000 798720000 860160000 921600000

[ Select 2x interpolation ]

root@linaro-ubuntu-desktop:/sys/bus/iio/devices/iio:device4# echo 245760000 > out_altvoltage_interpolation_frequency

[ List available center shift frequencies ]

root@linaro-ubuntu-desktop:/sys/bus/iio/devices/iio:device4# cat out_altvoltage_interpolation_center_shift_frequency_available
0 61440000 122880000 184320000

[ Select center shift frequencies ]

root@linaro-ubuntu-desktop:/sys/bus/iio/devices/iio:device4# echo 61440000 > out_altvoltage_interpolation_center_shift_frequency

More Information

resources/tools-software/linux-drivers/iio-dds/axi-dac-dds-hdl.1581449016.txt.gz · Last modified: 11 Feb 2020 20:23 by liam beguin