Wiki

This version (22 May 2023 16:53) was approved by Paul Pop.The Previously approved version (19 May 2023 18:53) is available.Diff

AD3552R Dual Channel, 16-Bit, 33 MUPS, Multispan, Multi-IO SPI DAC Linux device driver

The AD3552R is a low drift, dual channel, ultra-fast, 16-bit accuracy, current output digital-to-analog converter (DAC) that can be configured in multiple voltage span ranges. The AD3552R operates with a fixed 2.5 V reference. Each DAC incorporates three drift compensating feedback resistors for the required external transimpedance amplifier (TIA) that scales the output voltage. Offset and gain scaling registers allow for generation of multiple output span ranges, such as 0 V to 2.5 V, 0 V to 5 V, 0 V to 10 V, −5 V to +5 V, and −10 V to +10 V, and custom intermediate ranges with full 16-bit resolution. The DAC can operate in fast mode for maximum speed or precision mode for maximum accuracy.

Supported Devices

Evaluation Boards

Description

This is a Linux industrial I/O (IIO) subsystem driver, targeting RF Transceivers. The industrial I/O subsystem provides a unified framework for drivers for many different types of converters and sensors using a number of different physical interfaces (i2c, spi, etc). See IIO for more information.

Source Code

Status

Source Mainlined?
git No

Files

Function File
driver drivers/iio/dac/axi-ad3552r.c

Example Linux Device-Tree Initialization

Required devicetree properties:

  • compatible: Should always be “adi,axi-ad3552r”
  • clocks: define reference clock See Documentation/devicetree/bindings/clock/clock-bindings.txt

Optional properties:

  • reset-gpios : a GPIO spec for the Reset pin.

Example:

&fpga_axi {
	axi_ad3552r: axi-ad3552r@44a74000 {
		compatible = "adi,axi-ad3552r";
		reg = <0x44a74000 0x1000>;

		reset-gpios = <&gpio0 92 GPIO_ACTIVE_LOW>;		
		clocks = <&ref_clk>;

		dmas = <&dac_tx_dma 0>;
		dma-names = "tx";
	};
};

Enabling Linux driver support

Configure kernel with “make menuconfig” (alternatively use “make xconfig” or “make qconfig”)

Adding Linux driver support

Configure kernel with “make menuconfig” (alternatively use “make xconfig” or “make qconfig”)

Linux Kernel Configuration
	Device Drivers  --->
	<*>     Industrial I/O support --->
	    --- Industrial I/O support
	    -*-   Enable ring buffer support within IIO
	    -*-     Industrial I/O lock free software ring
	    -*-   Enable triggered sampling support

	          *** Digital to analog converters ***
	    [--snip--]

		<*>   Analog Devices AXI_AD3552R DAC driver 

	    [--snip--]

Hardware configuration

Driver testing / API

Each and every IIO device, typically a hardware chip, has a device folder under /sys/bus/iio/devices/iio:deviceX. Where X is the IIO index of the device. Under every of these directory folders reside a set of files, depending on the characteristics and features of the hardware device in question. These files are consistently generalized and documented in the IIO ABI documentation. In order to determine which IIO deviceX corresponds to which hardware device, the user can read the name file /sys/bus/iio/devices/iio:deviceX/name. In case the sequence in which the iio device drivers are loaded/registered is constant, the numbering is constant and may be known in advance.

02 Mar 2011 15:16

This specifies any shell prompt running on the target

root@analog:/> cd /sys/bus/iio/devices/
root@analog:/sys/bus/iio/device> ls -l

iio:device0 -> ../../../devices/soc0/axi/f8007100.adc/iio:device0
iio:device1 -> ../../../devices/soc0/fpga-axi@0/44a74000.axi-ad3552r/iio:device1
iio_sysfs_trigger -> ../../../devices/iio_sysfs_trigger

root:/sys/bus/iio/devices> cd iio:device1

root@analog:/sys/bus/iio/devices/iio:device1# ls -l
drwxr-xr-x 2 root root    0 May 16 07:42 buffer
drwxr-xr-x 2 root root    0 May 15 15:04 buffer0
-r--r--r-- 1 root root 4096 May 16 07:42 dev
-rw-r--r-- 1 root root 4096 May 16 07:42 input_source
-r--r--r-- 1 root root 4096 May 16 07:42 input_source_available
-r--r--r-- 1 root root 4096 May 15 15:04 name
lrwxrwxrwx 1 root root    0 May 16 07:42 of_node -> ../../../../../firmware/devicetree/base/fpga-axi@0/axi-ad3552r@44a74000
-rw-r--r-- 1 root root 4096 May 16 07:42 output_range
-r--r--r-- 1 root root 4096 May 16 07:42 output_range_available
-rw-r--r-- 1 root root 4096 May 16 07:42 out_voltage0_raw
-rw-r--r-- 1 root root 4096 May 16 07:42 out_voltage1_raw
drwxr-xr-x 2 root root    0 May 15 15:04 power
-rw-r--r-- 1 root root 4096 May 16 07:42 sampling_frequency
drwxr-xr-x 2 root root    0 May 15 15:04 scan_elements
-rw-r--r-- 1 root root 4096 May 16 07:42 stream_status
-r--r--r-- 1 root root 4096 May 16 07:42 stream_status_available
lrwxrwxrwx 1 root root    0 May 16 07:42 subsystem -> ../../../../../bus/iio
-rw-r--r-- 1 root root 4096 May 16 07:42 uevent
root:/sys/bus/iio/devices/iio:device1#

Show device name

This specifies any shell prompt running on the target

root:/sys/bus/iio/devices/iio:device1> cat name
axi-ad3552r

DAC sampling rate (sampling_frequency)

Read only attribute which returns the DAC sampling rate in Hz.

This specifies any shell prompt running on the target

root@analog:/sys/bus/iio/devices/iio:device1# cat sampling_frequency
16666667
root@analog:/sys/bus/iio/devices/iio:device1# echo 15000000 > sampling_frequency
-bash: echo: write error: Invalid argument
root@analog:/sys/bus/iio/devices/iio:device1#

More Information

resources/tools-software/linux-drivers/iio-dac/axi-ad3552r.txt · Last modified: 22 May 2023 16:51 by Marcelo Schmitt