resources:tools-software:linux-drivers:iio-dac:ad5758 [23 May 2018 10:54]
Stefan Popa Files
resources:tools-software:linux-drivers:iio-dac:ad5758 [15 Oct 2018 16:25] (current)
Stefan Popa adc->dac
Line 21: Line 21:
  
 ^ Source ^ Mainlined? ^ ^ Source ^ Mainlined? ^
-| [[https://​github.com/​analogdevicesinc/​linux/blob/rpi-4.9.y/drivers/​iio/​dac/​ad5758.c|git]] | [In progress...] |+| [[git.linux.org>drivers/​iio/​dac/​ad5758.c|git]] | [[git.linux.org>​drivers/​iio/​dac/​ad5758.c|Yes] |
  
 ===== Files ===== ===== Files =====
  
 ^ Function ^ File ^ ^ Function ^ File ^
-| driver ​ | [[https://github.com/analogdevicesinc/linux/blob/rpi-4.9.y/drivers/iio/dac/ad5758.c]] |+| driver ​ | [[git.linux.org>​drivers/iio/dac/ad5758.c]] | 
 + 
 +===== Devicetree ===== 
 + 
 +Required properties for the AD5758: 
 +  * compatible: Must be "​adi,​ad5758"​ 
 +  * reg: SPI chip select number for the device 
 +  * spi-max-frequency:​ Max SPI frequency to use (< 50000000) 
 +  * spi-cpha: is the only mode that is supported 
 + 
 +Optional properties:​ 
 + 
 +   * reset-gpios : GPIO spec for the RESET pin. If specified, it will be asserted during driver probe. 
 +   * adi,​dc-dc-mode:​ Mode of operation of the dc-to-dc converter 
 +   * adi,​dc-dc-ilim:​ The dc-to-dc converter current limit 
 +   * adi,slew: Array of slewrate settings should contain 3 fields: 
 +   * adi,range: The output range 
 + 
 +<​code>​ 
 + #​address-cells = <​1>;​ 
 + #​size-cells = <​0>;​ 
 + status = "​okay";​ 
 + 
 + ad5758@0 { 
 +                compatible = "​adi,​ad5758";​ 
 +                reg = <​0>;​ 
 +                spi-max-frequency = <​1000000>;​ 
 +                spi-cpha; 
 + 
 +                reset-gpios = <&​gpio 22 0>;  ​/* optional */ 
 + 
 +                adi,​dc-dc-mode = <​2>;​ 
 +                adi,​dc-dc-ilim = <​200>;​ 
 +                adi,slew = <1 200000 12>; 
 +                adi,range = <​1>;​ 
 +</code> 
 + 
 +====== Driver testing ====== 
 + 
 +<WRAP box bggreen><​wrap info>​This specifies any shell prompt running on the target</wrap> 
 +<​xterm>​ 
 +root:/> **cd /​sys/​bus/​iio/​devices/​** 
 +root:/​sys/​bus/​iio/​devices>​ ls 
 +iio:​device0 
 + 
 +root:/​sys/​bus/​iio/​devices>​ **cd iio\:​device0** 
 + 
 +root:/​sys/​bus/​iio/​devices/​iio:​device0>​ **ls -l** 
 +-r--r--r-- 1 root root 4096 May 23 09:14 dev 
 +-rw-r--r-- 1 root root 4096 May 23 09:14 out_voltage0_powerdown 
 +-rw-r--r-- 1 root root 4096 May 23 09:14 out_voltage0_raw 
 +-rw-r--r-- 1 root root 4096 May 23 09:14 out_voltage_scale 
 +-r--r--r-- 1 root root 4096 May 23 09:14 name 
 +drwxr-xr-x 2 root root    0 May 23 09:14 power 
 +lrwxrwxrwx 1 root root    0 May 23 09:14 subsystem -> ../../​../​../​../​../​../​../​bus/iio 
 +-rw-r--r-- 1 root root 4096 May 23 09:14 uevent 
 +</xterm><​/WRAP> 
 + 
 +=== Show device name === 
 + 
 +<WRAP box bggreen><​wrap info>​This specifies any shell prompt running on the target</​wrap>​ 
 +<​xterm>​ 
 +root:/​sys/​bus/​iio/​devices/​iio:​device0>​ **cat name** 
 +ad5758 
 +</​xterm></​WRAP>​ 
 + 
 +=== Show scale === 
 + 
 +**Description:​**\\ 
 +scale to be applied to in_voltage0_raw in order to obtain the measured voltage in millivolts. 
 + 
 +<WRAP box bggreen><​wrap info>​This specifies any shell prompt running on the target</​wrap>​ 
 +<​xterm>​ 
 +root:/​sys/​bus/​iio/​devices/​iio:​device0>​ **cat out_voltage_scale ** 
 +0.152587890 
 +</​xterm></​WRAP>​ 
 + 
 +=== Set channel 0 output voltage === 
 + 
 +**Description:​**\\ 
 +/​sys/​bus/​iio/​devices/​deviceX/​out_voltage0_raw\\ 
 + 
 +Raw (unscaled, no bias etc.) output voltage for 
 +channel 0. 
 + 
 + 
 +<WRAP box bggreen><​wrap info>​This specifies any shell prompt running on the target</​wrap>​ 
 +<​xterm>​ 
 +root:/​sys/​bus/​iio/​devices/​iio:​device0>​ **echo 32767 > out_voltage0_raw** 
 +</​xterm></​WRAP>​ 
 + 
 +**U** = //​out_voltage0_raw * out_voltage_scale//​ = 32767 * 0.152587890 = **4999.84 //mV//** 
 + 
 +=== Enable power down mode on output 0 === 
 + 
 +/​sys/​bus/​iio/​devices/​deviceX/​out_voltage0_powerdown 
 + 
 +**Description:​**\\ 
 +Writing 1 causes output 0 to enter the power down mode. Clearing returns to 
 +normal operation. 
 + 
 +<WRAP box bggreen><​wrap info>​This specifies any shell prompt running on the target</​wrap>​ 
 +<​xterm>​ 
 +root:/​sys/​bus/​iio/​devices/​iio:​device0>​ **echo 1 > out_voltage0_powerdown** 
 +root:/​sys/​bus/​iio/​devices/​iio:​device0> ​ **cat out_voltage0_powerdown** 
 +
 +root:/​sys/​bus/​iio/​devices/​iio:​device0>​ **echo 0 > out_voltage0_powerdown** 
 +root:/​sys/​bus/​iio/​devices/​iio:​device0> ​ **cat out_voltage0_powerdown** 
 +
 +</​xterm></​WRAP>​ 
 + 
 +====== More Information ====== 
 + 
 +{{page>​software:​linux:​docs:​iio:​iio_snippets#​iio pointers&​noheader&​firstseconly&​noeditbtn}} 
resources/tools-software/linux-drivers/iio-dac/ad5758.1527065649.txt.gz · Last modified: 23 May 2018 10:54 by Stefan Popa