resources:tools-software:linux-drivers:iio-adc:ad7998 [28 Apr 2011 18:15]
Robin Getz only avalible via git
resources:tools-software:linux-drivers:iio-adc:ad7998 [05 Jan 2021 16:01]
Ioana Chelaru Removed old references
Line 1: Line 1:
-====== AD7998 ​driver ​======+====== AD7998 ​IIO ADC Linux Driver ​======
  
 ===== Supported Devices ===== ===== Supported Devices =====
  
-This driver supports the +  * [[adi>​AD7991]] 
-[[:​analog-to-digital-converters:​ad-converters:​ad7991]] +  ​* ​[[adi>​AD7992]] 
-[[:​analog-to-digital-converters:​ad-converters:​ad7992]] +  ​* ​[[adi>​AD7993]] 
-[[:​analog-to-digital-converters:​ad-converters:​ad7993]] +  ​* ​[[adi>​AD7994]] 
-[[:analog-to-digital-converters:​ad-converters:​ad7994]] +  * [[adi>​AD7995]] 
-[[:analog-to-digital-converters:​ad-converters:​ad7995]] +  * [[adi>​AD7997]] 
-[[:analog-to-digital-converters:​ad-converters:​ad7997]] +  * [[adi>​AD7998]] 
-[[:analog-to-digital-converters:​ad-converters:​ad7998]] +  * [[adi>​AD7999]] 
-[[:analog-to-digital-converters:​ad-converters:​ad7999]]+ 
 + 
 +===== Reference Circuits ===== 
 + 
 +  * [[adi>​CN0288]] 
 +  * [[adi>​CN0301]] 
 + 
 +===== Evaluation Boards ===== 
 + 
 +  * [[adi>​EVAL-AD7991EBZ]] 
 +  ​* ​[[adi>EVAL-AD7992EBZ]] 
 +  ​* ​[[adi>EVAL-AD7993EBZ]] 
 +  ​* ​[[adi>EVAL-AD7994EBZ]] 
 +  ​* ​[[adi>EVAL-AD7995EBZ]] 
 +  ​* ​[[adi>EVAL-AD7997EBZ]] 
 +  * [[adi>​EVAL-AD7998EBZ]]
  
 ===== Description ===== ===== Description =====
Line 23: Line 38:
 ===== Status ===== ===== Status =====
  
- Source ​  Mainlined? ​ +^ Source ^ Mainlined? ^ 
-| [[bfgit>linux-kernel?drivers/staging/iio/adc/ad799x_core.c|git]] |  [[git.linux.org>​drivers/staging/iio/adc/ad799x_core.c|Yes]] ​ |+| [[git.linux.org>drivers/​iio/​adc/​ad799x.c|git]] | [[git.linux.org>​drivers/​iio/​adc/​ad799x.c|Yes]] |
 ===== Files ===== ===== Files =====
  
 ^ Function ^ File ^ ^ Function ^ File ^
-| driver ​ | [[git.linux.org>​drivers/staging/iio/adc/ad799x_core.c]] | +| driver ​ | [[git.linux.org>​drivers/​iio/​adc/​ad799x.c]] | 
-| driver ​ | [[git.linux.org>​drivers/​staging/​iio/​adc/​ad799x_ring.c]] | +
-| include | [[git.linux.org>​drivers/​staging/​iio/​adc/​ad799x.h]] |+
  
 ====== Example platform device initialization ====== ====== Example platform device initialization ======
Line 36: Line 50:
 {{page>​software/​linux/​docs/​platform_and_bus_model#​Platform Data&​noheader&​firstseconly&​noeditbtn}} {{page>​software/​linux/​docs/​platform_and_bus_model#​Platform Data&​noheader&​firstseconly&​noeditbtn}}
  
-The reference volatage may vary between boards and models. The platform_data for the device'​s "​struct device"​ holds this information. 
  
-<source trunk/drivers/​staging/​iio/​adc/​ad799x.h:​ad799x_platform_data{} c linux-kernel>+===== Specifying reference voltage via the regulator framework ===== 
 + 
 +<WRAP tip> 
 +In case the AD799x on-chip reference is not used,  
 +this driver requires specifying the reference voltage, by using the Linux regulator framework. 
 +</WRAP> 
 + 
 +Below example specifies a 2.5 Volt reference for the I2C device 0-0024 on I2C-Bus 0. (**0-0024**)
  
 <code c> <code c>
-static struct ​ad799x_platform_data ad7998_pdata ​= { +#if defined(CONFIG_REGULATOR_FIXED_VOLTAGE) || defined(CONFIG_REGULATOR_FIXED_VOLTAGE_MODULE) 
- .vref_mv = 2500,+static struct ​regulator_consumer_supply ad7998_consumer_supplies[] ​= { 
 + REGULATOR_SUPPLY("​vref",​ "​0-0024"​),
 }; };
 +
 +static struct regulator_init_data board_avdd_reg_init_data = {
 + .constraints = {
 + .name = "​2V5",​
 + .valid_ops_mask = REGULATOR_CHANGE_STATUS,​
 + },
 + .consumer_supplies = ad7998_consumer_supplies,​
 + .num_consumer_supplies = ARRAY_SIZE(ad7998_consumer_supplies),​
 +};
 +
 +static struct fixed_voltage_config board_vref_pdata = {
 + .supply_name = "​board-2V5",​
 + .microvolts = 2500000,
 + .gpio = -EINVAL,
 + .enabled_at_boot = 0,
 + .init_data = &​board_avdd_reg_init_data,​
 +};
 +static struct platform_device brd_voltage_regulator = {
 + .name = "​reg-fixed-voltage",​
 + .id = -1,
 + .num_resources = 0,
 + .dev = {
 + .platform_data = &​board_vref_pdata,​
 + },
 +};
 +#endif
 </​code>​ </​code>​
  
-<note tip+<code c
-In case platform_data is not present or set to NULLthe driver will use the AD7998 internal reference. +static struct platform_device *board_devices[] __initdata = { 
-</note>+#if defined(CONFIG_REGULATOR_FIXED_VOLTAGE) || defined(CONFIG_REGULATOR_FIXED_VOLTAGE_MODULE) 
 + &​brd_voltage_regulator 
 +#endif 
 +}; 
 +</​code>​ 
 + 
 +<code c> 
 +static int __init board_init(void) 
 +
 + [--snip--] 
 + 
 + platform_add_devices(board_devicesARRAY_SIZE(board_devices));​ 
 + 
 + [--snip--] 
 + 
 + return 0; 
 +
 +arch_initcall(board_init);​ 
 +</code>
  
 {{page>​software/​linux/​docs/​platform_and_bus_model#​Declaring I2C devices&​firstseconly&​noeditbtn}} {{page>​software/​linux/​docs/​platform_and_bus_model#​Declaring I2C devices&​firstseconly&​noeditbtn}}
Line 59: Line 124:
  {  {
  I2C_BOARD_INFO("​ad7998",​ 0x24),  I2C_BOARD_INFO("​ad7998",​ 0x24),
- .platform_data = (void *)&​ad799x_pdata,​+ .platform_data = &​ad799x_pdata,​
  .irq = IRQ_PG0,  .irq = IRQ_PG0,
  },  },
Line 78: Line 143:
 } }
 arch_initcall(board_init);​ arch_initcall(board_init);​
 +</​code>​
 +
 +===== Devicetree =====
 +
 +Required devicetree properties:
 +  * compatible: Needs to be "​adi,"​ followed by the name of the device. E.g. "​adi,​ad7798"​
 +  * reg: The slave address used for the device
 +  * vcc-supply: Phandle to the supply regulator
 +
 +<​code>​
 +       ​adc_supply:​ fixedregulator {
 +               ​compatible = "​regulator-fixed";​
 +               ​regulator-name = "​fixed-supply";​
 +               ​regulator-min-microvolt = <​3300000>;​
 +               ​regulator-max-microvolt = <​3300000>;​
 +       };
 +
 +       ​adc_vref:​ fixedregulator {
 +               ​compatible = "​regulator-fixed";​
 +               ​regulator-name = "​fixed-supply";​
 +               ​regulator-min-microvolt = <​2500000>;​
 +               ​regulator-max-microvolt = <​2500000>;​
 +       };
 +       
 +       i2c: i2c@e0007000 {
 +               #​address-cells = <1>;
 +               #​size-cells = <0>;
 +               ​compatible = "​xlnx,​xps-iic-2.00.a";​
 +               ...
 +
 +               ​ad7798@24 {
 +                       ​compatible = "​adi,​ad7798";​
 +                       reg = <​0x24>;​
 +                       ​vcc-supply = <&​adc_supply>;​
 +                       ​vref-supply = <&​adc_vref>;​
 +               };
 +        };
 </​code>​ </​code>​
  
Line 85: Line 187:
 "make qconfig"​) "make qconfig"​)
  
-<note>+<WRAP round help>
 The AD7998 Driver depends on **CONFIG_I2C** The AD7998 Driver depends on **CONFIG_I2C**
-</note>+</WRAP>
  
 <​code>​ <​code>​
Line 116: Line 218:
 {{page>​software:​linux:​docs:​iio:​iio_snippets#​iio device files&​noheader&​firstseconly&​noeditbtn}} {{page>​software:​linux:​docs:​iio:​iio_snippets#​iio device files&​noheader&​firstseconly&​noeditbtn}}
  
-<​box ​100% green|shell prompt running on the target>+<WRAP box bggreen><​wrap info>​This specifies any shell prompt running on the target</wrap>
 <​xterm>​ <​xterm>​
 root:/> **cd /​sys/​bus/​iio/​devices/​** root:/> **cd /​sys/​bus/​iio/​devices/​**
 root:/​sys/​bus/​iio/​devices>​ ls root:/​sys/​bus/​iio/​devices>​ ls
-device0 ​                 ​device0:​buffer0:​access0  ​trigger0 +iio:device0 ​                 trigger0 
-device0:​buffer0 ​         device0:​buffer0:​event0+
  
 root:/​sys/​bus/​iio/​devices>​ **cd device0** root:/​sys/​bus/​iio/​devices>​ **cd device0**
  
-root:/​sys/​devices/​platform/​i2c-bfin-twi.0/​i2c-0/​0-0024/​device0>​ **ls -l** +root:/​sys/​devices/​platform/​i2c-bfin-twi.0/​i2c-0/​0-0024/​iio:device0> **ls -l** 
-drwxr-xr-x ​   5 root     ​root ​            0 Jan  1 00:00 device0:​buffer0 +drwxr-xr-x ​   5 root     ​root ​            0 Jan  1 00:00 buffer 
-drwxr-xr-x ​   2 root     ​root ​            0 Jan  1 00:00 device0:​event0 +drwxr-xr-x ​   2 root     ​root ​            0 Jan  1 00:00 events 
--r--r--r-- ​   1 root     ​root ​         4096 Jan  1 00:00 in0_raw +-r--r--r-- ​   1 root     ​root ​         4096 Jan  1 00:00 in_voltage0_raw 
--r--r--r-- ​   1 root     ​root ​         4096 Jan  1 00:00 in1_raw +-r--r--r-- ​   1 root     ​root ​         4096 Jan  1 00:00 in_voltage1_raw 
--r--r--r-- ​   1 root     ​root ​         4096 Jan  1 00:00 in2_raw +-r--r--r-- ​   1 root     ​root ​         4096 Jan  1 00:00 in_voltage2_raw 
--r--r--r-- ​   1 root     ​root ​         4096 Jan  1 00:00 in3_raw +-r--r--r-- ​   1 root     ​root ​         4096 Jan  1 00:00 in_voltage3_raw 
--r--r--r-- ​   1 root     ​root ​         4096 Jan  1 00:00 in4_raw +-r--r--r-- ​   1 root     ​root ​         4096 Jan  1 00:00 in_voltage4_raw 
--r--r--r-- ​   1 root     ​root ​         4096 Jan  1 00:00 in5_raw +-r--r--r-- ​   1 root     ​root ​         4096 Jan  1 00:00 in_voltage5_raw 
--r--r--r-- ​   1 root     ​root ​         4096 Jan  1 00:00 in6_raw +-r--r--r-- ​   1 root     ​root ​         4096 Jan  1 00:00 in_voltage6_raw 
--r--r--r-- ​   1 root     ​root ​         4096 Jan  1 00:00 in7_raw +-r--r--r-- ​   1 root     ​root ​         4096 Jan  1 00:00 in_voltage7_raw 
--r--r--r-- ​   1 root     ​root ​         4096 Jan  1 00:00 in_scale+-r--r--r-- ​   1 root     ​root ​         4096 Jan  1 00:00 in_voltage_scale
 -r--r--r-- ​   1 root     ​root ​         4096 Jan  1 00:00 name -r--r--r-- ​   1 root     ​root ​         4096 Jan  1 00:00 name
 lrwxrwxrwx ​   1 root     ​root ​            0 Jan  1 00:00 subsystem -> ../​../​../​../​../​../​bus/​iio lrwxrwxrwx ​   1 root     ​root ​            0 Jan  1 00:00 subsystem -> ../​../​../​../​../​../​bus/​iio
 drwxr-xr-x ​   2 root     ​root ​            0 Jan  1 00:00 trigger drwxr-xr-x ​   2 root     ​root ​            0 Jan  1 00:00 trigger
 -rw-r--r-- ​   1 root     ​root ​         4096 Jan  1 00:00 uevent -rw-r--r-- ​   1 root     ​root ​         4096 Jan  1 00:00 uevent
-</​xterm></​box>+</​xterm></​WRAP>
  
 === Show device name === === Show device name ===
  
-<​box ​100% green|shell prompt running on the target>+<WRAP box bggreen><​wrap info>​This specifies any shell prompt running on the target</wrap>
 <​xterm>​ <​xterm>​
-root:/​sys/​devices/​platform/​i2c-bfin-twi.0/​i2c-0/​0-0024/​device0>​ **cat name**+root:/​sys/​devices/​platform/​i2c-bfin-twi.0/​i2c-0/​0-0024/​iio:device0> **cat name**
 ad7998 ad7998
-</​xterm></​box>+</​xterm></​WRAP>
  
 === Show scale === === Show scale ===
  
 **Description:​**\\ **Description:​**\\
-scale to be applied to in0_raw ​in order to obtain the measured voltage in millivolts.+scale to be applied to in_voltage0_raw ​in order to obtain the measured voltage in millivolts.
  
-<​box ​100% green|shell prompt running on the target>+<WRAP box bggreen><​wrap info>​This specifies any shell prompt running on the target</wrap>
 <​xterm>​ <​xterm>​
-root:/​sys/​devices/​platform/​i2c-bfin-twi.0/​i2c-0/​0-0024/​device0>​ **cat in_scale**+root:/​sys/​devices/​platform/​i2c-bfin-twi.0/​i2c-0/​0-0024/​iio:device0> **cat in_voltage_scale**
 1.000 1.000
-</​xterm></​box>+</​xterm></​WRAP>
  
 === Show channel 0 measurement === === Show channel 0 measurement ===
Line 167: Line 269:
 Raw unscaled voltage measurement on channel 0 Raw unscaled voltage measurement on channel 0
  
-<​box ​100% green|shell prompt running on the target>+<WRAP box bggreen><​wrap info>​This specifies any shell prompt running on the target</wrap>
 <​xterm>​ <​xterm>​
-root:/​sys/​devices/​platform/​i2c-bfin-twi.0/​i2c-0/​0-0024/​device0>​ **cat in0_raw**+root:/​sys/​devices/​platform/​i2c-bfin-twi.0/​i2c-0/​0-0024/​iio:device0> **cat in_voltage0_raw**
 1491 1491
-</​xterm></​box>+</​xterm></​WRAP>
  
-**U** = //in0_raw ​in_scale// = 1491 * 1.000 = **1491,00 //mV//**+**U** = //in_voltage0_raw ​in_voltage_scale// = 1491 * 1.000 = **1491,00 //mV//**
  
 ===== Trigger management ===== ===== Trigger management =====
Line 185: Line 287:
 ===== Buffer management ===== ===== Buffer management =====
  
-<​box ​100% green|shell prompt running on the target>+<WRAP box bggreen><​wrap info>​This specifies any shell prompt running on the target</wrap>
 <​xterm>​ <​xterm>​
-root:/​sys/​devices/​platform/​i2c-bfin-twi.0/​i2c-0/​0-0024/​device0/​device0:​buffer0> **ls** +root:/​sys/​devices/​platform/​i2c-bfin-twi.0/​i2c-0/​0-0024/​iio:device0/buffer> **ls** 
-**bytes_per_datum** ​         ​**enable** ​                  subsystem +**enable** ​ **length** 
-device0:​buffer0:​access0 ​ ​**length**                   ​uevent +root:/​sys/​devices/​platform/​i2c-bfin-twi.0/​i2c-0/​0-0024/​iio:device0/buffer
-device0:​buffer0:​event0 ​  ​**scan_elements** +</​xterm></​WRAP>
-root:/​sys/​devices/​platform/​i2c-bfin-twi.0/​i2c-0/​0-0024/​device0/​device0:​buffer0+
-</​xterm></​box>+
  
 {{page>​software:​linux:​docs:​iio:​iio_snippets#​Buffer management&​noheader&​firstseconly&​noeditbtn}} {{page>​software:​linux:​docs:​iio:​iio_snippets#​Buffer management&​noheader&​firstseconly&​noeditbtn}}
  
-<​box ​100% green|shell prompt running on the target>+<WRAP box bggreen><​wrap info>​This specifies any shell prompt running on the target</wrap>
 <​xterm>​ <​xterm>​
-root:/​sys/​devices/​platform/​i2c-bfin-twi.0/​i2c-0/​0-0024/​device0/​device0:​buffer0/​scan_elements>​ **ls** +root:/​sys/​devices/​platform/​i2c-bfin-twi.0/​i2c-0/​0-0024/​iio:device0/​scan_elements>​ **ls** 
-in0_en ​          ​in2_index ​       in5_en ​          ​in7_index +in_voltage0_en ​          ​in_voltage2_index ​       in_voltage5_en ​          ​in_voltage7_index 
-in0_index ​       in3_en ​          ​in5_index ​       in_type +in_voltage0_index ​       in_voltage3_en ​          ​in_voltage5_index ​       in_voltage_type 
-in1_en ​          ​in3_index ​       in6_en ​          timestamp_en +in_voltage1_en ​          ​in_voltage3_index ​       in_voltage6_en ​          timestamp_en 
-in1_index ​       in4_en ​          ​in6_index ​       ​timestamp_index +in_voltage1_index ​       in_voltage4_en ​          ​in_voltage6_index ​       ​timestamp_index 
-in2_en ​          ​in4_index ​       in7_en ​          timestamp_type +in_voltage2_en ​          ​in_voltage4_index ​       in_voltage7_en ​          timestamp_type 
-root:/​sys/​devices/​platform/​i2c-bfin-twi.0/​i2c-0/​0-0024/​device0/​device0:​buffer0/​scan_elements>​ +root:/​sys/​devices/​platform/​i2c-bfin-twi.0/​i2c-0/​0-0024/​iio:device0/​scan_elements>​ 
-</​xterm></​box>+</​xterm></​WRAP>
  
  
resources/tools-software/linux-drivers/iio-adc/ad7998.txt · Last modified: 05 Jan 2021 16:01 by Ioana Chelaru