Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:tools-software:linux-drivers:iio-adc:ad7887 [11 Feb 2016 20:46] – [Status] Lars-Peter Clausenresources:tools-software:linux-drivers:iio-adc:ad7887 [27 Apr 2016 17:12] (current) – [Example platform device initialization] Fix typo Lars-Peter Clausen
Line 37: Line 37:
 {{page>software/linux/docs/platform_and_bus_model#Platform Data&noheader&firstseconly&noeditbtn}} {{page>software/linux/docs/platform_and_bus_model#Platform Data&noheader&firstseconly&noeditbtn}}
  
-The reference volatage may vary between boards and models. The platform_data for the device's "struct device" holds this information.+The reference voltage may vary between boards and models. The platform_data for the device's "struct device" holds this information.
  
 <code c> <code c>
Line 46: Line 46:
   false the device is used in single channel mode and AIN1/Vref is used as   false the device is used in single channel mode and AIN1/Vref is used as
   VREF input.   VREF input.
- * @use_onchip_ref: Whether to use the onchip reference. If set to true the+ * @use_onchip_ref: Whether to use the on-chip reference. If set to true the
   internal 2.5V reference is used. If set to false a external reference is   internal 2.5V reference is used. If set to false a external reference is
   used.   used.
resources/tools-software/linux-drivers/iio-adc/ad7887.txt · Last modified: 27 Apr 2016 17:12 by Lars-Peter Clausen