This is an old revision of the document!
This is a Linux industrial I/O (IIO) subsystem driver, targeting multi channel serial interface ADCs. The industrial I/O subsystem provides a unified framework for drivers for many different types of converters and sensors using a number of different physical interfaces (i2c, spi, etc). See IIO for more information.
Function | File |
---|---|
driver | drivers/iio/adc/ad7793.c |
include | include/linux/platform_data/ad7793.h |
For compile time configuration, it’s common Linux practice to keep board- and application-specific configuration out of the main driver file, instead putting it into the board support file.
For devices on custom boards, as typical of embedded and SoC-(system-on-chip) based hardware, Linux uses platform_data to point to board-specific structures describing devices and how they are connected to the SoC. This can include available ports, chip variants, preferred modes, default initialization, additional pin roles, and so on. This shrinks the board-support packages (BSPs) and minimizes board and application specific #ifdefs in drivers.
The reference voltage may vary between boards and models. The platform_data for the device's “struct device” holds this information.
/** * enum ad7793_clock_source - AD7793 clock source selection * @AD7793_CLK_SRC_INT: Internal 64 kHz clock, not available at the CLK pin. * @AD7793_CLK_SRC_INT_CO: Internal 64 kHz clock, available at the CLK pin. * @AD7793_CLK_SRC_EXT: Use external clock. * @AD7793_CLK_SRC_EXT_DIV2: Use external clock divided by 2. */ enum ad7793_clock_source { AD7793_CLK_SRC_INT, AD7793_CLK_SRC_INT_CO, AD7793_CLK_SRC_EXT, AD7793_CLK_SRC_EXT_DIV2, }; /** * enum ad7793_bias_voltage - AD7793 bias voltage selection * @AD7793_BIAS_VOLTAGE_DISABLED: Bias voltage generator disabled * @AD7793_BIAS_VOLTAGE_AIN1: Bias voltage connected to AIN1(-). * @AD7793_BIAS_VOLTAGE_AIN2: Bias voltage connected to AIN2(-). * @AD7793_BIAS_VOLTAGE_AIN3: Bias voltage connected to AIN3(-). * Only valid for AD7795/AD7796. */ enum ad7793_bias_voltage { AD7793_BIAS_VOLTAGE_DISABLED, AD7793_BIAS_VOLTAGE_AIN1, AD7793_BIAS_VOLTAGE_AIN2, AD7793_BIAS_VOLTAGE_AIN3, }; /** * enum ad7793_refsel - AD7793 reference voltage selection * @AD7793_REFSEL_REFIN1: External reference applied between REFIN1(+) * and REFIN1(-). * @AD7793_REFSEL_REFIN2: External reference applied between REFIN2(+) and * and REFIN1(-). Only valid for AD7795/AD7796. * @AD7793_REFSEL_INTERNAL: Internal 1.17 V reference. */ enum ad7793_refsel { AD7793_REFSEL_REFIN1 = 0, AD7793_REFSEL_REFIN2 = 1, AD7793_REFSEL_INTERNAL = 2, }; /** * enum ad7793_current_source_direction - AD7793 excitation current direction * @AD7793_IEXEC1_IOUT1_IEXEC2_IOUT2: Current source IEXC1 connected to pin * IOUT1, current source IEXC2 connected to pin IOUT2. * @AD7793_IEXEC1_IOUT2_IEXEC2_IOUT1: Current source IEXC2 connected to pin * IOUT1, current source IEXC1 connected to pin IOUT2. * @AD7793_IEXEC1_IEXEC2_IOUT1: Both current sources connected to pin IOUT1. * Only valid when the current sources are set to 10 uA or 210 uA. * @AD7793_IEXEC1_IEXEC2_IOUT2: Both current sources connected to Pin IOUT2. * Only valid when the current ources are set to 10 uA or 210 uA. */ enum ad7793_current_source_direction { AD7793_IEXEC1_IOUT1_IEXEC2_IOUT2 = 0, AD7793_IEXEC1_IOUT2_IEXEC2_IOUT1 = 1, AD7793_IEXEC1_IEXEC2_IOUT1 = 2, AD7793_IEXEC1_IEXEC2_IOUT2 = 3, }; /** * enum ad7793_excitation_current - AD7793 excitation current selection * @AD7793_IX_DISABLED: Excitation current Disabled. * @AD7793_IX_10uA: Enable 10 micro-ampere excitation current. * @AD7793_IX_210uA: Enable 210 micro-ampere excitation current. * @AD7793_IX_1mA: Enable 1 milli-Ampere excitation current. */ enum ad7793_excitation_current { AD7793_IX_DISABLED = 0, AD7793_IX_10uA = 1, AD7793_IX_210uA = 2, AD7793_IX_1mA = 3, }; /** * struct ad7793_platform_data - AD7793 platform data * @clock_src: Clock source selection * @burnout_current: If set to true the 100nA burnout current is enabled. * @boost_enable: Enable boost for the bias voltage generator. * @buffered: If set to true configure the device for buffered input mode. * @unipolar: If set to true sample in unipolar mode, if set to false sample in * bipolar mode. * @refsel: Reference voltage selection * @bias_voltage: Bias voltage selection * @exitation_current: Excitation current selection * @current_source_direction: Excitation current direction selection */ struct ad7793_platform_data { enum ad7793_clock_source clock_src; bool burnout_current; bool boost_enable; bool buffered; bool unipolar; enum ad7793_refsel refsel; enum ad7793_bias_voltage bias_voltage; enum ad7793_excitation_current exitation_current; enum ad7793_current_source_direction current_source_direction; };
static struct ad7793_platform_data ad7793_pdata = { .clock_src = AD7793_CLK_SRC_EXT, .unipolar = true, .buffered = true, .refsel = AD7793_REFSEL_INTERNAL, };
Unlike PCI or USB devices, SPI devices are not enumerated at the hardware level. Instead, the software must know which devices are connected on each SPI bus segment, and what slave selects these devices are using. For this reason, the kernel code must instantiate SPI devices explicitly. The most common method is to declare the SPI devices by bus number.
This method is appropriate when the SPI bus is a system bus, as in many embedded systems, wherein each SPI bus has a number which is known in advance. It is thus possible to pre-declare the SPI devices that inhabit this bus. This is done with an array of struct spi_board_info, which is registered by calling spi_register_board_info().
For more information see: Documentation/spi/spi-summary.rst
Depending on the converter IC used, you may need to set the modalias accordingly, matching your part name. It may also required to adjust max_speed_hz. Please consult the datasheet, for maximum spi clock supported by the device in question.
static struct spi_board_info board_spi_board_info[] __initdata = { #if defined(CONFIG_AD7793) \ || defined(CONFIG_AD7793_MODULE) { .modalias = "ad7793", .max_speed_hz = 1000000, /* max spi clock (SCK) speed in HZ */ .bus_num = 0, .chip_select = 3, /* CS, change it for your board */ .platform_data = &ad7793_pdata, /* No spi_driver specific config */ .mode = SPI_MODE_3, .irq = IRQ_PF6, }, #endif };
static int __init board_init(void) { [--snip--] spi_register_board_info(board_spi_board_info, ARRAY_SIZE(board_spi_board_info)); [--snip--] return 0; } arch_initcall(board_init);
Configure kernel with “make menuconfig” (alternatively use “make xconfig” or “make qconfig”)
The AD7793 Driver depends on CONFIG_SPI
Linux Kernel Configuration Device Drivers ---> ... <*> Industrial I/O support ---> --- Industrial I/O support ... Analog to digital converters ---> ... <*> Analog Devices AD7793 and similar ADCs driver ... ... ...
Each and every IIO device, typically a hardware chip, has a device folder under /sys/bus/iio/devices/iio:deviceX. Where X is the IIO index of the device. Under every of these directory folders reside a set of files, depending on the characteristics and features of the hardware device in question. These files are consistently generalized and documented in the IIO ABI documentation. In order to determine which IIO deviceX corresponds to which hardware device, the user can read the name file /sys/bus/iio/devices/iio:deviceX/name. In case the sequence in which the iio device drivers are loaded/registered is constant, the numbering is constant and may be known in advance.
This specifies any shell prompt running on the target
root:/> cd /sys/bus/iio/devices/ root:/sys/bus/iio/devices> ls device0 trigger0 root:/sys/bus/iio/devices> cd iio:device0 root:/sys/devices/platform/bfin-spi.0/spi0.3/iio:device0> ls -l drwxr-xr-x 4 root root 0 Jan 4 09:29 device0:buffer0 -rw-r--r-- 1 root root 4096 Jan 4 09:30 in_voltage-in_voltage_scale -r--r--r-- 1 root root 4096 Jan 4 09:30 in_voltage-in_voltage_scale_available -r--r--r-- 1 root root 4096 Jan 4 09:30 in_voltage0-in_voltage0_raw -r--r--r-- 1 root root 4096 Jan 4 09:30 in_voltage0-in_voltage0_shorted_raw -r--r--r-- 1 root root 4096 Jan 4 09:30 in_voltage1-in_voltage1_raw -r--r--r-- 1 root root 4096 Jan 4 09:30 in_voltage2-in_voltage2_raw -r--r--r-- 1 root root 4096 Jan 4 09:30 in_voltage4_supply_raw -rw-r--r-- 1 root root 4096 Jan 4 09:30 in_voltage4_supply_scale -r--r--r-- 1 root root 4096 Jan 4 09:30 name drwxr-xr-x 2 root root 0 Jan 4 09:30 power -rw-r--r-- 1 root root 4096 Jan 4 09:30 sampling_frequency -r--r--r-- 1 root root 4096 Jan 4 09:30 sampling_frequency_available lrwxrwxrwx 1 root root 0 Jan 4 09:30 subsystem -> ../../../../../bus/iio -r--r--r-- 1 root root 4096 Jan 4 09:30 in_temp0_raw -rw-r--r-- 1 root root 4096 Jan 4 09:30 in_temp0_scale drwxr-xr-x 2 root root 0 Jan 4 09:30 trigger -rw-r--r-- 1 root root 4096 Jan 4 09:30 uevent root:/sys/devices/platform/bfin-spi.0/spi0.3/iio:device0>
This specifies any shell prompt running on the target
root:/sys/devices/platform/bfin-spi.0/spi0.3/iio:device0> cat name ad7793
This specifies any shell prompt running on the target
root:/sys/devices/platform/bfin-spi.0/spi0.3/iio:device0> cat sampling_frequency_available 470 242 123 62 50 39 33 19 17 16 12 10 8 6 4
This specifies any shell prompt running on the target
root:/sys/devices/platform/bfin-spi.0/spi0.3/iio:device0> cat sampling_frequency 10 root:/sys/devices/platform/bfin-spi.0/spi0.3/iio:device0> echo 50 > sampling_frequency root:/sys/devices/platform/bfin-spi.0/spi0.3/iio:device0> cat sampling_frequency 50 root:/sys/devices/platform/bfin-spi.0/spi0.3/iio:device0>
Description:
Shows the AVDD supply voltage
This specifies any shell prompt running on the target
root:/sys/devices/platform/bfin-spi.0/spi0.3/iio:device0> cat in_voltage4_supply_raw 7817399 root:/sys/devices/platform/bfin-spi.0/spi0.3/iio:device0> cat in_voltage4_supply_scale 0.000418420
U = in_voltage4_supply_raw * in_voltage4_supply_scale = 7817399 * 0.000418420 = 3270.95608958 mV
Lists all available scales for the differential input pairs:
ADC Input Pair | Channel name |
---|---|
AIN1(+) - AIN1(-) | in_voltage0-in_voltage0_raw |
AIN2(+) - AIN2(-) | in_voltage1-in_voltage1_raw |
AIN3(+) - AIN3(-) | in_voltage1-in_voltage1_raw |
AIN1(-) - AIN1(-) | in_voltage0-in_voltage0_shorted_raw |
Setting these directly influences the ADC input range, by altering the GAIN amplifier.
This specifies any shell prompt running on the target
root:/sys/devices/platform/bfin-spi.0/spi0.3/iio:device0> cat in_voltage-in_voltage_scale_available 0.000149010 0.000074500 0.000037250 0.000018620 0.000009310 0.000004650 0.000002320 0.000001160
Scale to be applied to in_voltage0-in_voltage0_raw, in_voltage1-in_voltage1_raw, in_voltage2-in_voltage2_raw in order to obtain the measured voltage in millivolts. Allows the user to select one scale out of the available scales. If the written scale differs from the current scale. The driver performs full and zero offset calibration on all differential input channels.
This specifies any shell prompt running on the target
root:/sys/devices/platform/bfin-spi.0/spi0.3/iio:device0> cat in_voltage-in_voltage_scale 0.000149010 root:/sys/devices/platform/bfin-spi.0/spi0.3/iio:device0> echo 0.000074500 > in_voltage-in_voltage_scale root:/sys/devices/platform/bfin-spi.0/spi0.3/iio:device0> cat in_voltage-in_voltage_scale 0.000074500
Description:
Raw unscaled voltage measurement
ADC Input Pair | Channel name |
---|---|
AIN1(+) - AIN1(-) | in_voltage0-in_voltage0_raw |
AIN2(+) - AIN2(-) | in_voltage1-in_voltage1_raw |
AIN3(+) - AIN3(-) | in_voltage2-in_voltage2_raw |
AIN4(+) - AIN4(-) | in_voltage3-in_voltage3_raw |
AIN5(+) - AIN5(-) | in_voltage4-in_voltage4_raw |
AIN6(+) - AIN6(-) | in_voltage5-in_voltage5_raw |
AIN1(-) - AIN1(-) | in_voltage0-in_voltage0_shorted_raw |
This specifies any shell prompt running on the target
root:/sys/devices/platform/bfin-spi.0/spi0.3/iio:device0> cat in_voltage0-in_voltage0_raw 6710665
U = in_voltage0-in_voltage0_raw * in_voltage-in_voltage_scale = 6710665 * 0.000149010 = 999.95619165 mV
This driver only supports it's own default trigger source ad7793-dev0
This specifies any shell prompt running on the target
root:/sys/devices/platform/bfin-spi.0/spi0.3/device0> cat trigger/current_trigger ad7793-dev0
This specifies any shell prompt running on the target
root:/sys/devices/platform/bfin-spi.0/spi0.3/device0/buffer> ls enable length root:/sys/devices/platform/bfin-spi.0/spi0.3/device0/buffer>
The Industrial I/O subsystem provides support for various ring buffer based data acquisition methods. Apart from device specific hardware buffer support, the user can chose between two different software ring buffer implementations. One is the IIO lock free software ring, and the other is based on Linux kfifo. Devices with buffer support feature an additional sub-folder in the /sys/bus/iio/devices/deviceX/ folder hierarchy. Called deviceX:bufferY, where Y defaults to 0, for devices with a single buffer.
Every buffer implementation features a set of files:
length
Get/set the number of sample sets that may be held by the buffer.
enable
Enables/disables the buffer. This file should be written last, after length and selection of scan elements.
watermark
A single positive integer specifying the maximum number of scan
elements to wait for.
Poll will block until the watermark is reached.
Blocking read will wait until the minimum between the requested
read amount or the low water mark is available.
Non-blocking read will retrieve the available samples from the
buffer even if there are less samples then watermark level. This
allows the application to block on poll with a timeout and read
the available samples after the timeout expires and thus have a
maximum delay guarantee.
data_available
A read-only value indicating the bytes of data available in the
buffer. In the case of an output buffer, this indicates the
amount of empty space available to write data to. In the case of
an input buffer, this indicates the amount of data available for
reading.
length_align_bytes
Using the high-speed interface. DMA buffers may have an alignment requirement for the buffer length.
Newer versions of the kernel will report the alignment requirements
associated with a device through the `length_align_bytes` property.
scan_elements
The scan_elements directory contains interfaces for elements that will be captured for a single triggered sample set in the buffer.
This specifies any shell prompt running on the target
root:/sys/devices/platform/bfin-spi.0/spi0.3/device0/scan_elements> ls in_voltage0-in_voltage0_en in_voltage1-in_voltage1_index in_voltage4_supply_type in_voltage0-in_voltage0_index in_voltage1-in_voltage1_type temp0_en in_voltage0-in_voltage0_shorted_en in_voltage2-in_voltage2_en temp0_index in_voltage0-in_voltage0_shorted_index in_voltage2-in_voltage2_index temp0_type in_voltage0-in_voltage0_shorted_type in_voltage2-in_voltage2_type timestamp_en in_voltage0-in_voltage0_type in_voltage4_supply_en timestamp_index in_voltage1-in_voltage1_en in_voltage4_supply_index timestamp_type root:/sys/devices/platform/bfin-spi.0/spi0.3/device0/scan_elements>
in_voltageX_en / in_voltageX-voltageY_en / timestamp_en:
Scan element control for triggered data capture.
Writing 1 will enable the scan element, writing 0 will disable it
in_voltageX_type / in_voltageX-voltageY_type / timestamp_type:
Description of the scan element data storage within the buffer
and therefore in the form in which it is read from user-space.
Form is [s|u]bits/storage-bits. s or u specifies if signed
(2's complement) or unsigned. bits is the number of bits of
data and storage-bits is the space (after padding) that it
occupies in the buffer. Note that some devices will have
additional information in the unused bits so to get a clean
value, the bits value must be used to mask the buffer output
value appropriately. The storage-bits value also specifies the
data alignment. So u12/16 will be a unsigned 12 bit integer
stored in a 16 bit location aligned to a 16 bit boundary.
For other storage combinations this attribute will be extended
appropriately.
in_voltageX_index / in_voltageX-voltageY_index / timestamp_index:
A single positive integer specifying the position of this
scan element in the buffer. Note these are not dependent on
what is enabled and may not be contiguous. Thus for user-space
to establish the full layout these must be used in conjunction
with all _en attributes to establish which channels are present,
and the relevant _type attributes to establish the data storage
format.