Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
resources:tools-software:linux-drivers:iio-adc:ad7768 [05 Jul 2018 14:27]
Stefan Popa Example Linux Device-Tree Initialization
resources:tools-software:linux-drivers:iio-adc:ad7768 [05 Jul 2018 15:07] (current)
Stefan Popa More Information
Line 27: Line 27:
 ^ Function ^ File ^ ^ Function ^ File ^
 | driver ​ | [[linux.github>​master/​drivers/​iio/​adc/​ad7768.c]] | | driver ​ | [[linux.github>​master/​drivers/​iio/​adc/​ad7768.c]] |
 +| devicetree bindings | [[linux.github>​master?​Documentation/​devicetree/​bindings/​iio/​adc/​adi,​ad7768.txt | Documentation/​devicetree/​bindings/​iio/​adc/​adi,​ad7768.txt]] |
 +| hdl project | [[https://​github.com/​analogdevicesinc/​hdl/​tree/​hdl_2017_r1/​projects/​ad7768evb | hdl]] |
  
 ====== Example Linux Device-Tree Initialization ====== ====== Example Linux Device-Tree Initialization ======
Line 41: Line 43:
 | AD7768 Device Tree  | [[linux.github>​master?​arch/​arm/​boot/​dts/​zynq-zed-adv7511-ad7768.dts | AD7768 Device Tree  | [[linux.github>​master?​arch/​arm/​boot/​dts/​zynq-zed-adv7511-ad7768.dts
 | zynq-zed-adv7511-ad7768.dts]] | | zynq-zed-adv7511-ad7768.dts]] |
 +
 +====== Driver testing ======
 +
 +{{page>​software:​linux:​docs:​iio:​iio_snippets#​iio device files&​noheader&​firstseconly&​noeditbtn}}
 +
 +<WRAP top tip round box 60%>​**TIP:​**
 +An example program which uses the interface can be found here:
 +  * [[resources:​tools-software:​linux-software:​iio_oscilloscope|IIO Oscilloscope]]
 +</​WRAP>​\\
 +
 +<WRAP box bggreen><​wrap info>​This specifies any shell prompt running on the target</​wrap>​
 +<​xterm>​
 +root:/> **cd /​sys/​bus/​iio/​devices/​**
 +root:/​sys/​bus/​iio/​devices>​ ls
 +iio:device0
 +
 +root:/​sys/​bus/​iio/​devices>​ **cd iio\:​device0**
 +
 +root:/​sys/​bus/​iio/​devices/​iio:​device0>​ **ls -l**
 +drwxrwxrwx 2 root root    0 Jan  1 00:02 buffer
 +-rw-rw-rw- 1 root root 4096 Jan  1 00:02 dev
 +-rw-rw-rw- 1 root root 4096 Jan  1 00:02 in_voltage_scale
 +-rw-rw-rw- 1 root root 4096 Jan  1 00:02 name
 +lrwxrwxrwx 1 root root    0 Jan  1 00:02 of_node -> ../​../​../​../​../​../​../​../​firmware/​devicetree/​base/​amba/​spi@e0006000/​adc@0
 +drwxrwxrwx 2 root root    0 Jan  1 00:02 power
 +drwxrwxrwx 2 root root    0 Jan  1 00:02 scan_elements
 +lrwxrwxrwx 1 root root    0 Jan  1 00:02 subsystem -> ../​../​../​../​../​../​../​../​bus/​iio
 +-rw-rw-rw- 1 root root 4096 Jan  1 00:02 uevent
 +</​xterm></​WRAP>​
 +
 +=== Show device name ===
 +
 +<WRAP box bggreen><​wrap info>​This specifies any shell prompt running on the target</​wrap>​
 +<​xterm>​
 +root:/​sys/​bus/​iio/​devices/​iio:​device0>​ **cat name**
 +ad7768
 +</​xterm></​WRAP>​
 +
 +=== Show scale ===
 +
 +**Description:​**\\
 +scale to be applied to in_voltage0_raw in order to obtain the measured voltage in millivolts.
 +
 +<WRAP box bggreen><​wrap info>​This specifies any shell prompt running on the target</​wrap>​
 +<​xterm>​
 +root:/​sys/​bus/​iio/​devices/​iio:​device0>​ **cat in_voltage_scale **
 +0.000488281
 +</​xterm></​WRAP>​
 +
 +====== More Information ======
 +
 +{{page>​software:​linux:​docs:​iio:​iio_snippets#​iio pointers&​noheader&​firstseconly&​noeditbtn}}
resources/tools-software/linux-drivers/iio-adc/ad7768.1530793675.txt.gz · Last modified: 05 Jul 2018 14:27 by Stefan Popa