Wiki

This version is outdated by a newer approved version.DiffThis version (05 Jul 2018 14:12) is a draft.
Approvals: 0/1

This is an old revision of the document!


AD7768 IIO Precision ADC Linux Driver

Supported Devices

This driver supports the

Evaluation Boards

Description

This is a Linux industrial I/O (IIO) subsystem driver, targeting single channel serial interface ADCs. The industrial I/O subsystem provides a unified framework for drivers for many different types of converters and sensors using a number of different physical interfaces (i2c, spi, etc). See IIO for more information.

Source Code

Status

Source Mainlined?
git [In progress…]
resources/tools-software/linux-drivers/iio-adc/ad7768.1530792762.txt.gz · Last modified: 05 Jul 2018 14:12 by Stefan Popa