Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:tools-software:linux-drivers:iio-adc:ad7768 [06 Nov 2023 11:16] – changed device info Ana-Maria Cuscoresources:tools-software:linux-drivers:iio-adc:ad7768 [06 Nov 2023 11:41] (current) – Add note about adi,datalines property Ana-Maria Cusco
Line 47: Line 47:
   * adi,data-lines: Number of DOUTx pins channels data is output on. Default value: 1.   * adi,data-lines: Number of DOUTx pins channels data is output on. Default value: 1.
  
 +**NOTE:** The //adi,data-lines// value is determined by the configuration of the AD7768/AD7768-4 chip's FORMATx pins. These pins are read on power-up and dictate the number of data lines (DOUTx) on which the ADC conversions are output. 
 ^ Function ^ File ^ ^ Function ^ File ^
 | AD7768 Device Tree  | [[linux.github>master?arch/arm/boot/dts/zynq-zed-adv7511-ad7768.dts | AD7768 Device Tree  | [[linux.github>master?arch/arm/boot/dts/zynq-zed-adv7511-ad7768.dts
resources/tools-software/linux-drivers/iio-adc/ad7768.txt · Last modified: 06 Nov 2023 11:41 by Ana-Maria Cusco