Wiki

This version is outdated by a newer approved version.DiffThis version (19 Jan 2018 10:00) was approved by Alexandru Ardelean.The Previously approved version (22 Feb 2017 19:18) is available.Diff

This is an old revision of the document!


AD6676 Wideband IF Receiver Subsystem Linux device driver

The AD6676 is a highly integrated IF subsystem that can digitize radio frequency (RF) bands up to 160 MHz in width centered on an intermediate frequency (IF) of 70 MHz to 450 MHz.

Supported Devices

Reference Circuits

Evaluation Boards

Description

This is a Linux industrial I/O (IIO) subsystem driver, targeting RF Transceivers. The industrial I/O subsystem provides a unified framework for drivers for many different types of converters and sensors using a number of different physical interfaces (i2c, spi, etc). See IIO for more information.

Source Code

Status

Source Mainlined?
git No

Files

Example Linux Device-Tree Initialization

The AD6676 driver is a spi-bus driver and can currently only be instantiated via device tree.

Required devicetree properties:

  • compatible: Should always be “ad6676”
  • reg: SPI slave select number
Function File
AD6676-EBZ Device Tree zynq-zc706-adv7511-ad6676-fmc.dts

Device Driver Customization

Devicetree Property Description
adi,adc-frequency-hz Initial ADC frequency in Hz
adi,adc-frequency-fixed-enable Prevents ADC frequency changes after initial setup
adi,use-external-clk-enable Use external CLK
adi,decimation Initial decimation rate [12, 16, 24, 32]
adi,intermediate-frequency-hz Initial IF in Hz
adi,intermediate-frequency-min-hz Allowed minimum IF in Hz
adi,intermediate-frequency-max-hz Allowed maximum IF in Hz
adi,bandwidth-hz Initial bandwidth in Hz
adi,bandwidth-margin-low-mhz Initial bandwidth margin low in Hz
adi,bandwidth-margin-high-mhz Initial bandwidth margin high in Hz
adi,bandwidth-margin-if-mhz Initial bandwidth margin IF in Hz
adi,external-inductance-l-nh The inductance of the external inductors in nH
adi,idac1-fullscale-adjust Initial IDAC_FS [64..16]
adi,shuffler-control Initial shuffler control setting
adi,shuffler-thresh Initial shuffler threshold
adi,jesd-scrambling-enable Enables JESD204B link scrambling
adi,jesd-use-lvds-syncb-enable Use LVDS SYNCB
adi,jesd-powerdown-sysref-enable Powerdown SYSREF
adi,jesd-l-lanes Number of JESD204B lanes
adi,jesd-f-frames-per-multiframe Number of frames per multiframe
adi,spi-3wire-enable Enables SPI 3-WIRE mode

Enabling Linux driver support

Configure kernel with “make menuconfig” (alternatively use “make xconfig” or “make qconfig”)

The AD6676 driver depends on CONFIG_SPI

Adding Linux driver support

Configure kernel with “make menuconfig” (alternatively use “make xconfig” or “make qconfig”)

Linux Kernel Configuration
	Device Drivers  --->
	<*>     Industrial I/O support --->
	    --- Industrial I/O support
	    -*-   Enable ring buffer support within IIO
	    -*-     Industrial I/O lock free software ring
	    -*-   Enable triggered sampling support

	          *** Analog to digital converters ***
	    [--snip--]

		<*>   Analog Devices AD9467 AD9643 High-Speed AXI ADC driver

	    [--snip--]

Hardware configuration

Driver testing / API

Each and every IIO device, typically a hardware chip, has a device folder under /sys/bus/iio/devices/iio:deviceX. Where X is the IIO index of the device. Under every of these directory folders reside a set of files, depending on the characteristics and features of the hardware device in question. These files are consistently generalized and documented in the IIO ABI documentation. In order to determine which IIO deviceX corresponds to which hardware device, the user can read the name file /sys/bus/iio/devices/iio:deviceX/name. In case the sequence in which the iio device drivers are loaded/registered is constant, the numbering is constant and may be known in advance.

02 Mar 2011 15:16

TIP: An example program which uses the interface can be found here:


This specifies any shell prompt running on the target

root:/> cd /sys/bus/iio/devices/
root:/sys/bus/iio/devices> ls
iio:device0  iio:device1

root:/sys/bus/iio/devices> cd iio:device1

root:/sys/bus/iio/devices/iio:device1# ls -l
drwxr-xr-x 5 root root    0 Jan 22 08:19 .
drwxr-xr-x 4 root root    0 Jan 22 08:19 ..
drwxr-xr-x 2 root root    0 Jan 22 08:19 buffer
-r--r--r-- 1 root root 4096 Jan 22 08:19 dev
-rw-r--r-- 1 root root 4096 Jan 22 08:19 in_voltage_adc_frequency
-rw-r--r-- 1 root root 4096 Jan 22 08:19 in_voltage_bandwidth
-rw-r--r-- 1 root root 4096 Jan 22 08:19 in_voltage_bw_margin_high
-rw-r--r-- 1 root root 4096 Jan 22 08:19 in_voltage_bw_margin_if
-rw-r--r-- 1 root root 4096 Jan 22 08:19 in_voltage_bw_margin_low
-rw-r--r-- 1 root root 4096 Jan 22 08:19 in_voltage_hardwaregain
-rw-r--r-- 1 root root 4096 Jan 22 08:19 in_voltage_intermediate_frequency
-rw-r--r-- 1 root root 4096 Jan 22 08:19 in_voltage_sampling_frequency
-rw-r--r-- 1 root root 4096 Jan 22 08:19 in_voltage_scale
-rw-r--r-- 1 root root 4096 Jan 22 08:19 in_voltage_shuffler_control
-r--r--r-- 1 root root 4096 Jan 22 08:19 in_voltage_shuffler_control_available
-rw-r--r-- 1 root root 4096 Jan 22 08:19 in_voltage_shuffler_thresh
-r--r--r-- 1 root root 4096 Jan 22 08:19 in_voltage_shuffler_thresh_available
-rw-r--r-- 1 root root 4096 Jan 22 08:19 in_voltage_test_mode
-r--r--r-- 1 root root 4096 Jan 22 08:19 in_voltage_test_mode_available
-r--r--r-- 1 root root 4096 Jan 22 08:19 name
drwxr-xr-x 2 root root    0 Jan 22 08:19 power
drwxr-xr-x 2 root root    0 Jan 22 08:19 scan_elements
lrwxrwxrwx 1 root root    0 Jan 22 08:19 subsystem -> ../../../../../bus/iio
-rw-r--r-- 1 root root 4096 Jan 22 08:19 uevent

root:/sys/bus/iio/devices/iio:device1#

Show device name

This specifies any shell prompt running on the target

root:/sys/bus/iio/devices/iio:device1> cat name
axi-ad6676-hpc

ADC frequency FADC (in_voltage_adc_frequency)

The clock frequency of the ADC. Maximizing the clock frequency is helpful when the IF or bandwidth are high. A lower clock frequency reduces power consumption and is appropriate for low IFs and narrow bandwidths.

Range using external synthesizer [2.0,3.2] GHz in Hz Range using internal synthesizer [2.925,3.2] GHz in Hz

This specifies any shell prompt running on the target

root@analog:/sys/bus/iio/devices/iio:device1# cat in_voltage_adc_frequency
3200000000
root@analog:/sys/bus/iio/devices/iio:device1# echo 3000000000 > in_voltage_adc_frequency
-bash: echo: write error: Invalid argument

TIP: If writing this attribute returns “Invalid argument” (-EINVAL) this means that the underlying HDL or Hardware's JESD204B Core and Gigabit Transceiver (GT) doesn't support changing the JESD204B Lane Rate.


Complex IQ Data Rate (in_voltage_sampling_frequency)

The complex (I/Q) data rate in SPS. The AD6676 supports decimation factors (DFs) of 12, 16, 24 and 32. The complex (I/Q) data rate at the JESD204B outputs is FADC / DF.

In case the underlying HDL or Hardware's JESD204B Core and Gigabit Transceiver (GT) support arbitrary JESD204B Lane Rates. This attribute can be writable. And it will select the appropriate AD6676 supported DFs.

This specifies any shell prompt running on the target

root@analog:/sys/bus/iio/devices/iio:device1# cat in_voltage_sampling_frequency
200000000

IF intermediate frequency (in_voltage_intermediate_frequency)

The IF (intermediate frequency) to which the ADC is tuned. The AD6676 supports IFs from 70 to 450 MHz provided the external inductors are chosen appropriately. Since the AD6676-EBZ by default includes a pair of 19-nH inductors soldered to the evaluation board, the IF range allowed is less than the full range supported by the AD6676.

TIP: Please see paragraph Lext Selection in the datasheet: Maximum External Inductor Value as a Function of IF Frequency

The min/max values the device driver accepts can be set via following devicetree attributes:

	adi,intermediate-frequency-min-hz = <150000000>;
	adi,intermediate-frequency-max-hz = <450000000>;


Since the tuning accuracy is finite - reading back this value allows the user to determine the offset.

This specifies any shell prompt running on the target

root@analog:/sys/bus/iio/devices/iio:device1# echo 200000000 > in_voltage_intermediate_frequency
root@analog:/sys/bus/iio/devices/iio:device1# cat in_voltage_intermediate_frequency
200000000

root@analog:/sys/bus/iio/devices/iio:device1# echo 199000000 > in_voltage_intermediate_frequency
root@analog:/sys/bus/iio/devices/iio:device1# cat in_voltage_intermediate_frequency
199218750

Bandwidth (in_voltage_bandwidth)

The bandwidth of the ADC. Since the AD6676 uses delta-sigma technology, the available bandwidth is a relatively small fraction of the ADC clock rate and the AD6676 achieves the lowest noise and distortion when the bandwidth is small.

The allowed range is between [0.005,0.05]*FADC in Hz

This specifies any shell prompt running on the target

root@analog:/sys/bus/iio/devices/iio:device1# echo 100000000 > in_voltage_bandwidth
root@analog:/sys/bus/iio/devices/iio:device1# cat in_voltage_bandwidth
100000000

Bandwidth Margins (in_voltage_bw_margin_[low|high])

Lower (in_voltage_bw_margin_low) and upper (in_voltage_bw_margin_high) bandwidth margins for the noise-shaping profile of the ADC.

Typical values are 5 MHz, but the user may want to increase these margins in wideband operation in order to optimize the noise profile of the ADC.

Typical range [0,30] MHz in MHz

This specifies any shell prompt running on the target

root@analog:/sys/bus/iio/devices/iio:device1# echo 5 > in_voltage_bw_margin_low
root@analog:/sys/bus/iio/devices/iio:device1# cat in_voltage_bw_margin_low
5

Bandwidth Margin IF (in_voltage_bw_margin_if)

Displacement of the resonance frequency (F1Shift) of the first resonator within the ADC from band-center. Typically 0 is appropriate, but in the widest bandwidth modes positive shifts can be used to reduce the noise density near the upper edge of the passband.

Typical range [-30,30] MHz in MHz

This specifies any shell prompt running on the target

root@analog:/sys/bus/iio/devices/iio:device1# echo -1 > in_voltage_bw_margin_if 
root@analog:/sys/bus/iio/devices/iio:device1# cat in_voltage_bw_margin_if
-1

Full-Scale (in_voltage_scale)

One of the convenient features of the AD6676 is that the full-scale of its ADC is relatively small and adjustable over a 12-dB range [1.00 .. 0.25] The dynamic range of the ADC is highest at the maximum full-scale setting but the noise figure of the system is lowest at the minimum full-scale setting.

Writing a value of 0.5 to this device attribute lowers the PIN_0dBFS by 6 dB. Likewise writing a value of 0.25 to this device attribute lowers the PIN_0dBFS by 12 dB.

This specifies any shell prompt running on the target

root@analog:/sys/bus/iio/devices/iio:device1# cat in_voltage_scale
1.000000
root@analog:/sys/bus/iio/devices/iio:device1# echo 0.25 > in_voltage_scale
root@analog:/sys/bus/iio/devices/iio:device1# cat in_voltage_scale
0.250000

Attenuation Control (in_voltage_hardwaregain)

The AD6676 contains a 50-ohm input attenuator programmable in 1-dB steps. Use this device attribute to set the attenuator's attenuation. The dynamic range of the system increases somewhat with moderate attenuation settings of 6-12 dB, at the expense of an increased noise figure.

The range is from 0 to -27.00 dB in 1dB steps. The nomenclature used here is gain instead of attenuation, so all values are expressed negative.

This specifies any shell prompt running on the target

root@analog:/sys/bus/iio/devices/iio:device1# echo -10.00 > in_voltage_hardwaregain

root@analog:/sys/bus/iio/devices/iio:device1# cat in_voltage_hardwaregain
-10.000000 dB

Shuffle Control (in_voltage_shuffler_control)

The AD6676 includes dynamic reordering of the comparators within the ADC in order to break up the spurious tones and distortion products associated with a fixed ordering. The Shuffle Control device attribute allows the user to experiment with different shuffling rates. The fadc option (Shuffle every 1) reorders the comparators on every clock cycle with 50% probability. This shuffle scheme is able to randomize deterministic spurs but tends to increase the noise density and creates FADC/32 “shuffle humps” in the output spectrum. Similarly, the fadc/2 fadc/3 fadc/4 (Shuffle every 2,3,4) options reorder the comparators every n clock cycles with 50% probability. Using a high value of n decreases the noise degradation at the expense of less effective randomization and FADC/(32*n) shuffle humps that are closer to the main carrier. Fast shuffling can be disabled by selecting the disable option.

This specifies any shell prompt running on the target

root@analog:/sys/bus/iio/devices/iio:device1# cat in_voltage_shuffler_control_available
disable fadc fadc/2 fadc/3 fadc/4
root@analog:/sys/bus/iio/devices/iio:device1# cat in_voltage_shuffler_control
fadc
root@analog:/sys/bus/iio/devices/iio:device1# echo disable > in_voltage_shuffler_control
root@analog:/sys/bus/iio/devices/iio:device1# cat in_voltage_shuffler_control
disable

Shuffle Threshold (in_voltage_shuffler_thresh)

In order to obtain the spur-reduction benefits of shuffling at large signal levels while retaining the low noise of not shuffling when the signal is small, the AD6676 supports dynamic shuffle control via the Shuffle Threshold attribute. Shuffling is disabled if the raw ADC output is below the specified threshold for ~5000 clock cycles. A threshold of zero implies that shuffling is always enabled.

The supported range is from 0..8

This specifies any shell prompt running on the target

root@analog:/sys/bus/iio/devices/iio:device1# cat in_voltage_shuffler_thresh_available
0 1 2 3 4 5 6 7 8
root@analog:/sys/bus/iio/devices/iio:device1# cat in_voltage_shuffler_thresh
5
root@analog:/sys/bus/iio/devices/iio:device1# echo 4 > in_voltage_shuffler_thresh
root@analog:/sys/bus/iio/devices/iio:device1# cat in_voltage_shuffler_thresh
4

Test Modes (in_voltage_test_mode)

Interface test modes supported by the AD6676.

This specifies any shell prompt running on the target

root@analog:/sys/bus/iio/devices/iio:device1# cat in_voltage_test_mode_available
off checkerboard one_zero_toggle pn23 pn9 rep_user_pat sing_user_pat ramp mod_rpat jspat jtspat

root@analog:/sys/bus/iio/devices/iio:device1# echo ramp > in_voltage_test_mode
root@analog:/sys/bus/iio/devices/iio:device1# cat in_voltage_test_mode
ramp

JESD204B Interface Testing

Below Eyes were captured on a Xilinx ZC706 after > 4 hours of operation:

JESD204B Eye Scan

 LANE0  LANE1

More Information

resources/tools-software/linux-drivers/iio-adc/ad6676.1516352400.txt.gz · Last modified: 19 Jan 2018 10:00 by Alexandru Ardelean