Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
resources:tools-software:linux-drivers:iio-adc:ad400x [07 Nov 2018 08:55]
mirceac [Status]
resources:tools-software:linux-drivers:iio-adc:ad400x [14 Nov 2018 11:26] (current)
mirceac [Status]
Line 1: Line 1:
-====== AD4003/​AD4007/​AD4011/​AD4020 Linux Driver ======+====== AD4003/​AD4007/​AD4011/​AD4020/​ADAQ40XX ​Linux Driver ======
  
 ===== Supported Devices ===== ===== Supported Devices =====
Line 21: Line 21:
  
 ^ Source ^ Mainlined? ^ ^ Source ^ Mainlined? ^
-| [[linux.github>​master/​drivers/​iio/​adc/​ad400x.c|git]] | [In progress...] |+| [[linux.github>​master/​drivers/​iio/​adc/​ad400x.c|git]] | [No] |
  
 ===== Files ===== ===== Files =====
  
 ^ Function ^ File ^ ^ Function ^ File ^
-| driver ​ | [[linux.github>​master/​drivers/​iio/​adc/​ad7124.c]] | +| driver ​ | [[linux.github>​master/​drivers/​iio/​adc/​ad400x.c]] | 
-| devicetree bindings | [[linux.github>​master?​Documentation/​devicetree/​bindings/​iio/​adc/​adi,​ad7124.txt | Documentation/​devicetree/​bindings/​iio/​adc/​adi,ad7124.txt]] |+| devicetree bindings | [[linux.github>​master?​Documentation/​devicetree/​bindings/​iio/​adc/​adi,​ad7124.txt | Documentation/​devicetree/​bindings/​iio/​adc/​ad400x.txt]] |
  
 ====== Driver setup ====== ====== Driver setup ======
resources/tools-software/linux-drivers/iio-adc/ad400x.1541577311.txt.gz · Last modified: 07 Nov 2018 08:55 by mirceac