This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:tools-software:linux-drivers:iio-adc:ad400x [02 Nov 2018 11:45] – Mircea Caprioru | resources:tools-software:linux-drivers:iio-adc:ad400x [14 Nov 2018 11:26] – [Status] Mircea Caprioru | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== AD4003/ | + | ====== AD4003/ |
===== Supported Devices ===== | ===== Supported Devices ===== | ||
Line 8: | Line 8: | ||
* [[adi> | * [[adi> | ||
* [[adi> | * [[adi> | ||
+ | * [[adi> | ||
===== Evaluation Boards ===== | ===== Evaluation Boards ===== | ||
Line 20: | Line 21: | ||
^ Source ^ Mainlined? ^ | ^ Source ^ Mainlined? ^ | ||
- | | [[linux.github> | + | | [[linux.github> |
===== Files ===== | ===== Files ===== | ||
^ Function ^ File ^ | ^ Function ^ File ^ | ||
- | | driver | + | | driver |
- | | devicetree bindings | [[linux.github> | + | | devicetree bindings | [[linux.github> |
====== Driver setup ====== | ====== Driver setup ====== |