Wiki

This version is outdated by a newer approved version.DiffThis version (15 Nov 2012 19:50) was approved by Lars-Peter Clausen.The Previously approved version (05 Sep 2012 11:34) is available.Diff

This is an old revision of the document!


ADIS16240 IIO Programmable Impact Sensor and Recorder Linux Driver

Supported Devices

Evaluation Boards

Description

This is a Linux industrial I/O (IIO) subsystem driver, targeting serial interface Accelerometer. The industrial I/O subsystem provides a unified framework for drivers for many different types of converters and sensors using a number of different physical interfaces (i2c, spi, etc). See IIO for more information.

Source Code

Status

Source Mainlined?
git Yes

Files

Declaring SPI slave devices

Unlike PCI or USB devices, SPI devices are not enumerated at the hardware level. Instead, the software must know which devices are connected on each SPI bus segment, and what slave selects these devices are using. For this reason, the kernel code must instantiate SPI devices explicitly. The most common method is to declare the SPI devices by bus number.

This method is appropriate when the SPI bus is a system bus, as in many embedded systems, wherein each SPI bus has a number which is known in advance. It is thus possible to pre-declare the SPI devices that inhabit this bus. This is done with an array of struct spi_board_info, which is registered by calling spi_register_board_info().

For more information see: Documentation/spi/spi-summary.rst

21 Oct 2010 16:10

Depending on the converter IC used, you may need to set the modalias accordingly, matching your part name. It may also required to adjust max_speed_hz. Please consult the datasheet, for maximum spi clock supported by the device in question.

static struct spi_board_info board_spi_board_info[] __initdata = {
#if defined(CONFIG_ADIS16240) \
	|| defined(CONFIG_ADIS16240_MODULE)
	{
		.modalias = "adis16240",
		.max_speed_hz = 1500000,     /* max spi clock (SCK) speed in HZ */
		.bus_num = 0,
		.chip_select = 5, /* CS, change it for your board */
		.platform_data = NULL, /* No spi_driver specific config */
		.mode = SPI_MODE_3,
		.irq = IRQ_PF4,
	},
#endif
};
static int __init board_init(void)
{
	[--snip--]
 
	spi_register_board_info(board_spi_board_info, ARRAY_SIZE(board_spi_board_info));
 
	[--snip--]
 
	return 0;
}
arch_initcall(board_init);

Adding Linux driver support

Configure kernel with “make menuconfig” (alternatively use “make xconfig” or “make qconfig”)

The ADIS16240 Driver depends on CONFIG_SPI
Linux Kernel Configuration
	Device Drivers  --->
		[*] Staging drivers  --->
			<*>     Industrial I/O support --->
			    --- Industrial I/O support
			    -*-   Enable ring buffer support within IIO
			    -*-     Industrial I/O lock free software ring
			    -*-   Enable triggered sampling support

			          *** Accelerometers ***
			    [--snip--]

			    <*>   Analog Devices ADIS16240 Programmable Impact Sensor and Recorder

			    [--snip--]

Hardware configuration

Driver testing

Each and every IIO device, typically a hardware chip, has a device folder under /sys/bus/iio/devices/iio:deviceX. Where X is the IIO index of the device. Under every of these directory folders reside a set of files, depending on the characteristics and features of the hardware device in question. These files are consistently generalized and documented in the IIO ABI documentation. In order to determine which IIO deviceX corresponds to which hardware device, the user can read the name file /sys/bus/iio/devices/iio:deviceX/name. In case the sequence in which the iio device drivers are loaded/registered is constant, the numbering is constant and may be known in advance.

02 Mar 2011 15:16

<box 100% green|shell prompt running on the target>

root:/> cd /sys/bus/iio/devices/
root:/sys/bus/iio/devices> ls
iio:device0  trigger0


root:/sys/bus/iio/devices> cd iio:device0
root:/sys/devices/platform/bfin-spi.0/spi0.5/iio:device0> ls -l
-r--r--r--    1 root     root          4096 Jan  4 04:15 accel_xyz_squared_peak_raw
drwxr-xr-x    2 root     root             0 Jan  4 04:15 buffer
-r--r--r--    1 root     root          4096 Jan  4 04:15 dev
-rw-r--r--    1 root     root          4096 Jan  4 04:15 in_accel_x_calibbias
-r--r--r--    1 root     root          4096 Jan  4 04:15 in_accel_x_raw
-rw-r--r--    1 root     root          4096 Jan  4 04:15 in_accel_x_scale
-rw-r--r--    1 root     root          4096 Jan  4 04:15 in_accel_y_calibbias
-r--r--r--    1 root     root          4096 Jan  4 04:15 in_accel_y_raw
-rw-r--r--    1 root     root          4096 Jan  4 04:15 in_accel_y_scale
-rw-r--r--    1 root     root          4096 Jan  4 04:15 in_accel_z_calibbias
-r--r--r--    1 root     root          4096 Jan  4 04:15 in_accel_z_raw
-rw-r--r--    1 root     root          4096 Jan  4 04:15 in_accel_z_scale
-r--r--r--    1 root     root          4096 Jan  4 04:15 in_temp0_raw
-rw-r--r--    1 root     root          4096 Jan  4 04:15 in_temp0_scale
-r--r--r--    1 root     root          4096 Jan  4 04:15 in_voltage0_supply_raw
-rw-r--r--    1 root     root          4096 Jan  4 04:15 in_voltage0_supply_scale
-r--r--r--    1 root     root          4096 Jan  4 04:15 in_voltage1_raw
-r--r--r--    1 root     root          4096 Jan  4 04:15 name
drwxr-xr-x    2 root     root             0 Jan  4 04:15 power
--w-------    1 root     root          4096 Jan  4 04:15 reset
-r--r--r--    1 root     root          4096 Jan  4 04:15 sampling_frequency_available
drwxr-xr-x    2 root     root             0 Jan  4 04:15 scan_elements
lrwxrwxrwx    1 root     root             0 Jan  4 04:15 subsystem -> ../../../../../bus/iio
drwxr-xr-x    2 root     root             0 Jan  4 04:15 trigger
-rw-r--r--    1 root     root          4096 Jan  4 04:15 uevent
</box>

Show device name

<box 100% green|shell prompt running on the target>

root:/sys/devices/platform/bfin-spi.0/spi0.5/iio:device0> cat name
adis16240
</box>

ADIS16240 device attributes

For a detailed description please see: drivers/staging/iio/Documentation/sysfs-bus-iio

Device files
accel_xyz_squared_peak_raw
in_accel_x_calibbias
in_accel_x_raw
in_accel_x_scale
in_accel_y_calibbias
in_accel_y_raw
in_accel_y_scale
in_accel_z_calibbias
in_accel_z_raw
in_accel_z_scale
in_temp0_raw
in_temp0_scale
in_voltage0_supply_raw
in_voltage0_supply_scale
in_voltage1_raw
name
reset
sampling_frequency_available

Trigger management

This driver only supports it's own default trigger source adis16240-dev0

<box 100% green|shell prompt running on the target>

root:/sys/devices/platform/bfin-spi.0/spi0.5/iio:device0> cat trigger/current_trigger
adis16240-dev0
</box>

Buffer management

<box 100% green|shell prompt running on the target>

root:/sys/devices/platform/bfin-spi.0/spi0.5/iio:device0/buffer> ls
bytes_per_datum  enable           length
</box>

The Industrial I/O subsystem provides support for various ring buffer based data acquisition methods. Apart from device specific hardware buffer support, the user can chose between two different software ring buffer implementations. One is the IIO lock free software ring, and the other is based on Linux kfifo. Devices with buffer support feature an additional sub-folder in the /sys/bus/iio/devices/deviceX/ folder hierarchy. Called deviceX:bufferY, where Y defaults to 0, for devices with a single buffer.

Every buffer implementation features a set of files:

length
Get/set the number of sample sets that may be held by the buffer.

enable
Enables/disables the buffer. This file should be written last, after length and selection of scan elements.

watermark
A single positive integer specifying the maximum number of scan elements to wait for. Poll will block until the watermark is reached. Blocking read will wait until the minimum between the requested read amount or the low water mark is available. Non-blocking read will retrieve the available samples from the buffer even if there are less samples then watermark level. This allows the application to block on poll with a timeout and read the available samples after the timeout expires and thus have a maximum delay guarantee.

data_available
A read-only value indicating the bytes of data available in the buffer. In the case of an output buffer, this indicates the amount of empty space available to write data to. In the case of an input buffer, this indicates the amount of data available for reading.

length_align_bytes
Using the high-speed interface. DMA buffers may have an alignment requirement for the buffer length. Newer versions of the kernel will report the alignment requirements associated with a device through the `length_align_bytes` property.

scan_elements
The scan_elements directory contains interfaces for elements that will be captured for a single triggered sample set in the buffer.

02 Mar 2011 15:16

<box 100% green|shell prompt running on the target>

root:/sys/devices/platform/bfin-spi.0/spi0.5/iio:device0/scan_elements>ls
in_accel_x_en             in_accel_z_index          in_timestamp_type
in_accel_x_index          in_accel_z_type           in_voltage0_supply_en
in_accel_x_type           in_temp0_en               in_voltage0_supply_index
in_accel_y_en             in_temp0_index            in_voltage0_supply_type
in_accel_y_index          in_temp0_type             in_voltage1_en
in_accel_y_type           in_timestamp_en           in_voltage1_index
in_accel_z_en             in_timestamp_index        in_voltage1_type
</box>

in_voltageX_en / in_voltageX-voltageY_en / timestamp_en:
Scan element control for triggered data capture. Writing 1 will enable the scan element, writing 0 will disable it

in_voltageX_type / in_voltageX-voltageY_type / timestamp_type:
Description of the scan element data storage within the buffer and therefore in the form in which it is read from user-space. Form is [s|u]bits/storage-bits. s or u specifies if signed (2's complement) or unsigned. bits is the number of bits of data and storage-bits is the space (after padding) that it occupies in the buffer. Note that some devices will have additional information in the unused bits so to get a clean value, the bits value must be used to mask the buffer output value appropriately. The storage-bits value also specifies the data alignment. So u12/16 will be a unsigned 12 bit integer stored in a 16 bit location aligned to a 16 bit boundary. For other storage combinations this attribute will be extended appropriately.

in_voltageX_index / in_voltageX-voltageY_index / timestamp_index:
A single positive integer specifying the position of this scan element in the buffer. Note these are not dependent on what is enabled and may not be contiguous. Thus for user-space to establish the full layout these must be used in conjunction with all _en attributes to establish which channels are present, and the relevant _type attributes to establish the data storage format.

02 Mar 2011 15:16

More Information

resources/tools-software/linux-drivers/iio-accelerometer/adis16240.1353005402.txt.gz · Last modified: 15 Nov 2012 19:50 by Lars-Peter Clausen