Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision Both sides next revision
resources:tools-software:linux-drivers:gpio:adp5588-gpio [09 Nov 2011 11:54]
Michael Hennerich [Supported Devices]
resources:tools-software:linux-drivers:gpio:adp5588-gpio [05 Sep 2012 11:24]
Michael Hennerich ch
Line 8: Line 8:
 ===== Evaluation Boards ===== ===== Evaluation Boards =====
  
-  * [[adi>​ADP5588-EVALZ]] ​  +  * [[adi>​ADP5588-EVALZ]] 
-  * [[adi>​ADP5587CB-EVALZ]] ​  ​ +  * [[adi>​ADP5587CB-EVALZ]] 
-  * [[adi>​ADP5587CP-EVALZ]] ​+  * [[adi>​ADP5587CP-EVALZ]]
  
 ===== Description ===== ===== Description =====
Line 28: Line 28:
  
 ^  Source ​ ^  Mainlined? ​ ^ ^  Source ​ ^  Mainlined? ​ ^
-| [[bfgit>linux-kernel?drivers/​gpio/​adp5588-gpio.c|git]] |  [[git.linux.org>​drivers/​gpio/​adp5588-gpio.c|Yes]] ​ |+| [[git.linux.org>drivers/​gpio/​adp5588-gpio.c|git]] |  [[git.linux.org>​drivers/​gpio/​adp5588-gpio.c|Yes]] ​ |
  
 ===== Files ===== ===== Files =====
Line 66: Line 66:
 <​note>​ <​note>​
 The ADP5588 Driver depends on **CONFIG_I2C**\\ The ADP5588 Driver depends on **CONFIG_I2C**\\
-IRQ-Chip interrupt controller support is not available in case this driver is build as Module ​+IRQ-Chip interrupt controller support is not available in case this driver is build as Module
 </​note>​ </​note>​
  
 <​code>​ <​code>​
-Device Drivers ​ ---> ​  +Device Drivers ​ ---> 
-[*] GPIO Support ​ ---> ​ +[*] GPIO Support ​ --->
  
     --- GPIO Support     --- GPIO Support
Line 109: Line 109:
 <note tip> <note tip>
 On the ADP5588 Demo Mother Board replace R30 (10kOhm PULL-UP resistor on /INTB strobe) with a 1-3kOhm resistor. On the ADP5588 Demo Mother Board replace R30 (10kOhm PULL-UP resistor on /INTB strobe) with a 1-3kOhm resistor.
-The 10kOhm resistor is too weak - Blackfin might see an additional falling edge interrupt on the rising edge of /​INTB. ​+The 10kOhm resistor is too weak - Blackfin might see an additional falling edge interrupt on the rising edge of /INTB.
 </​note>​ </​note>​
  
resources/tools-software/linux-drivers/gpio/adp5588-gpio.txt · Last modified: 03 Jan 2013 20:42 (external edit)