This is an old revision of the document!
Common elements for all kernel builds:
make
installed on your system, but we generally recommend installing the build-essentials tools for your Linux distributionu-boot-tools
installed, to have the mkimage
utilities available, so it's good to have them available/installedTarget specific details:
The rapid increase in use of free and open-source software (FOSS), in particular Linux, represents the most significant, all-encompassing, and long-term trend that the embedded industry has seen since the early 1980s.1) Like many, Analog Devices creates and maintains Linux Drivers for various Analog Devices products.
Select a driver from the list below.
* AD8801 : Octal 8-Bit TrimDAC with Power Shutdown & Mid-Scale Preset AD8801 * AD8803 : Octal 8-Bit TrimDAC with Power Shutdown & Mid-Scale Preset AD8803