Wiki

This version is outdated by a newer approved version.DiffThis version (15 Nov 2018 13:27) was approved by mirceac.The Previously approved version (17 Oct 2018 15:50) is available.Diff

This is an old revision of the document!


Linux Drivers

Building the ADI Linux kernel

Common elements for all kernel builds:

  • make sure you have make installed on your system, but we generally recommend installing the build-essentials tools for your Linux distribution
  • some builds will require you to have u-boot-tools installed, to have the mkimage utilities available, so it's good to have them available/installed

Target specific details:

The rapid increase in use of free and open-source software (FOSS), in particular Linux, represents the most significant, all-encompassing, and long-term trend that the embedded industry has seen since the early 1980s.1) Like many, Analog Devices creates and maintains Linux Drivers for various Analog Devices products.

Select a driver from the list below.

Driver List

Backlight

Battery Charger

GPIO

Secondary function

IIO - Accelerometers

IIO - Amplifiers

IIO - Analog to Digital Converters

IIO - Capacitance to Digital Converters

IIO - Digital to Analog Converters

IIO - Direct Digital Synthesis

IIO - Frequency Synthesizers / Phase-Locked Loop

IIO - Gyroscopes

IIO - Impedance Converters and Network Analyzers

IIO - Inertial Measurement Units

IIO - Resolvers

IIO - Receivers

IIO - Transceivers

Input - Keyboard

Input - Misc

Input - Touchscreens

LED

Miscellaneous

Multifunction Device

Multiplexers

Networking - MAC802154

Regulators

Sound

Video

1)
IDC study/survey from over 5000 developers in 116 countries. Open Source in Global Software: Market Impact, Disruption, and Business Models. 2006.
resources/tools-software/linux-drivers-all.1542191454.txt.gz · Last modified: 14 Nov 2018 11:30 by mirceac