Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
Next revisionBoth sides next revision
resources:tools-software:linux-build:generic:zynq [14 Feb 2018 12:13] – [Building the Zynq boot image] Michael Hennerichresources:tools-software:linux-build:generic:zynq [24 Aug 2018 10:18] – [Setup cross compile environment variables] Michael Hennerich
Line 47: Line 47:
 | 2016_R2 | | 2016_R2 |
 | 2017_R1 | | 2017_R1 |
 +| 2018_R1 |
 +
  
 <code> <code>
Line 68: Line 70:
 | 2016_R2 | Vivado 2016.2 |  | 2016_R2 | Vivado 2016.2 | 
 | 2017_R1 | Vivado 2016.4 |  | 2017_R1 | Vivado 2016.4 | 
 +| 2018_R1 | Vivado 2017.4 | 
  
 Vivado 2015.2 SDK may be installed into a different directory Vivado 2015.2 SDK may be installed into a different directory
Line 134: Line 137:
  
 === Build the one that fits your FPGA carrier and FMC card === === Build the one that fits your FPGA carrier and FMC card ===
- +| zynq-adrv9361-z7035-bob | [[adi>ADRV1CRR-BOB]] | [[adi>ADRV9361]] | 
-| zynq-zc702-adv7511-ad9361-fmcomms2-3.dts | [[xilinx>ZC702]]the on-board [[adi>ADV7511]] and the [[/resources/eval/user-guides/ad-fmcomms2-ebz|AD-FMCOMMS2-EBZ]] or [[/resources/eval/user-guides/ad-fmcomms3-ebz|AD-FMCOMMS3-EBZ]] board | +| zynq-adrv9361-z7035-bob-cmos | [[adi>ADRV1CRR-BOB]] | [[adi>ADRV9361]] | 
-| zynq-zc702-adv7511-ad9361-fmcomms5.dts | [[xilinx>ZC702]]the on-board [[adi>ADV7511]] and the [[/resources/eval/user-guides/ad-fmcomms5-ebz|AD-FMCOMMS5-EBZ]] | +| zynq-adrv9361-z7035-box | [[adi>ADRV1CRR-BOX]] | [[adi>ADRV9361]] | 
-| zynq-zc702-adv7511-ad9364-fmcomms4.dts | [[xilinx>ZC702]]the on-board [[adi>ADV7511]] and the [[/resources/eval/user-guides/ad-fmcomms4-ebz|AD-FMCOMMS4-EBZ]] board | +| zynq-adrv9361-z7035-fmc | [[adi>ADRV1CRR-FMC]] | the on-board [[adi>ADV7511]] and the [[adi>ADRV9361]] | 
-| zynq-zc706-adv7511-ad9361-fmcomms2-3.dts | [[xilinx>ZC706]]the on-board [[adi>ADV7511]] and the [[/resources/eval/user-guides/ad-fmcomms2-ebz|AD-FMCOMMS2-EBZ]] or [[/resources/eval/user-guides/ad-fmcomms3-ebz|AD-FMCOMMS3-EBZ]] board | +| zynq-adrv9361-z7035-fmc-rfcard-tdd | [[adi>ADRV1CRR-FMC]] | the on-board [[adi>ADV7511]], [[adi>ADRV9361]] and the [[adi>AD-PZSDR2400TDD-EB]] |  
-| zynq-zc706-adv7511-ad9361-fmcomms2-3-pr.dts | [[xilinx>ZC706]]the on-board [[adi>ADV7511]] and the [[/resources/eval/user-guides/ad-fmcomms2-ebz|AD-FMCOMMS2-EBZ]] or [[/resources/eval/user-guides/ad-fmcomms3-ebz|AD-FMCOMMS3-EBZ]] board | +| zynq-adrv9364-z7020-bob | [[adi>ADRV1CRR-BOB]] | [[adi>ADRV9364]] | 
-| zynq-zc706-adv7511-ad9361-fmcomms5.dts | [[xilinx>ZC706]]the on-board [[adi>ADV7511]] and the [[/resources/eval/user-guides/ad-fmcomms5-ebz|AD-FMCOMMS5-EBZ]] board | +| zynq-adrv9364-z7020-bob-cmos | [[adi>ADRV1CRR-BOB]] | [[adi>ADRV9364]] | 
-| zynq-zc706-adv7511-ad9364-fmcomms4.dts | [[xilinx>ZC706]]the on-board [[adi>ADV7511]] and the [[/resources/eval/user-guides/ad-fmcomms4-ebz|AD-FMCOMMS4-EBZ]] board | +| zynq-adrv9364-z7020-box | [[adi>ADRV1CRR-BOX]] | [[adi>ADRV9364]] | 
-| zynq-zc706-adv7511-ad9434-fmc-500ebz.dts | [[xilinx>ZC706]]the on-board [[adi>ADV7511]] and the [[/resources/fpga/xilinx/fmc/ad9434?s[]=ad9434&s[]=fmc&s[]=500ebz|AD9434-FMC-500EBZ]] board | +| zynq-mini-itx-adv7511 | [[http://zedboard.org/product/mini-itx|Mini-ITX]] | the on-board [[adi>ADV7511]] | 
-| zynq-zed-adv7511-ad9361-fmcomms2-3.dts | [[http://zedboard.org/product/zedboard|Zed Board]]the on-board [[adi>ADV7511]] and the [[/resources/eval/user-guides/ad-fmcomms2-ebz|AD-FMCOMMS2-EBZ]] or [[/resources/eval/user-guides/ad-fmcomms3-ebz|AD-FMCOMMS3-EBZ]] board | +| zynq-mini-itx-adv7511-ad9361-fmcomms2-3 | [[http://zedboard.org/product/mini-itx|Mini-ITX]] | on-board [[adi>ADV7511]] and the [[/resources/eval/user-guides/ad-fmcomms2-ebz|AD-FMCOMMS2-EBZ]] or [[/resources/eval/user-guides/ad-fmcomms3-ebz|AD-FMCOMMS3-EBZ]] board | 
-| zynq-zed-adv7511-ad9364-fmcomms4.dts | [[http://zedboard.org/product/zedboard|Zed Board]]the on-board [[adi>ADV7511]] and the [[/resources/eval/user-guides/ad-fmcomms4-ebz|AD-FMCOMMS4-EBZ]] board | +| zynq-mini-itx-adv7511-ad9364-fmcomms4 | [[http://zedboard.org/product/mini-itx|Mini-ITX]] | the on-board [[adi>ADV7511]] and the [[/resources/eval/user-guides/ad-fmcomms4-ebz|AD-FMCOMMS4-EBZ]] board | 
-| zynq-zed-adv7511-ad9467-fmc-250ebz.dts | [[http://zedboard.org/product/zedboard|Zed Board]]the on-board [[adi>ADV7511]] and the [[/resources/eval/ad9467-fmc-250ebz|AD9467-FMC-250EBZ]] board +| zynq-zc702-adv7511 | [[xilinx>ZC702]] | the on-board [[adi>ADV7511]] | 
-| zynq-mini-itx-adv7511-ad9361-fmcomms2-3.dts | [[http://zedboard.org/product/mini-itx|Mini-ITX]]the on-board [[adi>ADV7511]] and the [[/resources/eval/user-guides/ad-fmcomms2-ebz|AD-FMCOMMS2-EBZ]] or [[/resources/eval/user-guides/ad-fmcomms3-ebz|AD-FMCOMMS3-EBZ]] board | +| zynq-zc702-adv7511-ad9361-fmcomms2-3 | [[xilinx>ZC702]] | the on-board [[adi>ADV7511]] and the [[/resources/eval/user-guides/ad-fmcomms2-ebz|AD-FMCOMMS2-EBZ]] or [[/resources/eval/user-guides/ad-fmcomms3-ebz|AD-FMCOMMS3-EBZ]] board | 
-| zynq-mini-itx-adv7511-ad9361-fmcomms2-3-pr.dts | [[http://zedboard.org/product/mini-itx|Mini-ITX]]the on-board [[adi>ADV7511]] and the [[/resources/eval/user-guides/ad-fmcomms2-ebz|AD-FMCOMMS2-EBZ]] or [[/resources/eval/user-guides/ad-fmcomms3-ebz|AD-FMCOMMS3-EBZ]] board | +| zynq-zc702-adv7511-ad9361-fmcomms5 | [[xilinx>ZC702]] the on-board [[adi>ADV7511]] and the [[/resources/eval/user-guides/ad-fmcomms5-ebz|AD-FMCOMMS5-EBZ]] | 
-| zynq-mini-itx-adv7511-ad9364-fmcomms4.dts | [[http://zedboard.org/product/mini-itx|Mini-ITX]]the on-board [[adi>ADV7511]] and the [[/resources/eval/user-guides/ad-fmcomms4-ebz|AD-FMCOMMS4-EBZ]] board | +| zynq-zc702-adv7511-ad9364-fmcomms4 | [[xilinx>ZC702]] the on-board [[adi>ADV7511]] and the [[/resources/eval/user-guides/ad-fmcomms4-ebz|AD-FMCOMMS4-EBZ]] board | 
 +| zynq-zc706-adv7511 | [[xilinx>ZC706]] | the on-board [[adi>ADV7511]] 
 +| zynq-zc706-adv7511-ad6676-fmc | [[xilinx>ZC706]] the on-board [[adi>ADV7511]] and the [[/resources/eval/ad6676-wideband_rx_subsystem_ad6676ebz|AD6676-FMC-EBZ]] board | 
 +| zynq-zc706-adv7511-ad9265-fmc-125ebz | [[xilinx>ZC706]] | the on-board [[adi>ADV7511]] and the [[/resources/fpga/xilinx/fmc/ad9265|AD9265-FMC-125EBZ]] board | 
 +| zynq-zc706-adv7511-ad9361-fmcomms2-3 | [[xilinx>ZC706]] the on-board [[adi>ADV7511]] and the [[/resources/eval/user-guides/ad-fmcomms2-ebz|AD-FMCOMMS2-EBZ]] or [[/resources/eval/user-guides/ad-fmcomms3-ebz|AD-FMCOMMS3-EBZ]] board | 
 +| zynq-zc706-adv7511-ad9361-fmcomms5 | [[xilinx>ZC706]] | the on-board [[adi>ADV7511]] and the [[/resources/eval/user-guides/ad-fmcomms5-ebz|AD-FMCOMMS5-EBZ]] board | 
 +| zynq-zc706-adv7511-ad9361-fmcomms5-ext-lo-adf5355 | [[xilinx>ZC706]] | the on-board [[adi>ADV7511]] and the [[/resources/eval/user-guides/ad-fmcomms5-ebz|AD-FMCOMMS5-EBZ]] board | 
 +| zynq-zc706-adv7511-ad9364-fmcomms4 | [[xilinx>ZC706]] the on-board [[adi>ADV7511]] and the [[/resources/eval/user-guides/ad-fmcomms4-ebz|AD-FMCOMMS4-EBZ]] board | 
 +| zynq-zc706-adv7511-ad9434-fmc-500ebz | [[xilinx>ZC706]] the on-board [[adi>ADV7511]] and the [[/resources/fpga/xilinx/fmc/ad9434|AD9434-FMC-500EBZ]] board | 
 +| zynq-zc706-adv7511-ad9625-fmcadc2 | [[xilinx>ZC706]] | the on-board [[adi>ADV7511]] and the [[/resources/eval/user-guides/ad-fmcdaq2-ebz|AD-FMCADC2-EBZ]] board | 
 +| zynq-zc706-adv7511-ad9739a-fmc | [[xilinx>ZC706]] | the on-board [[adi>ADV7511]] and the [[adi>EVAL-AD9739A]] 
 +| zynq-zc706-adv7511-adrv9371 | [[xilinx>ZC706]] | the on-board [[adi>ADV7511]] and the [[/resources/eval/user-guides/mykonos|ADRV9371]] board | 
 +| zynq-zc706-adv7511-adrv9375 | [[xilinx>ZC706]] | the on-board [[adi>ADV7511]] and the [[/resources/eval/user-guides/mykonos|ADRV9375]] board | 
 +| zynq-zc706-adv7511-fmcadc4 | [[xilinx>ZC706]] | the on-board [[adi>ADV7511]] and the [[/resources/eval/user-guides/ad-fmcadc4-ebz|AD-FMCADC4-EBZ]] board | 
 +| zynq-zc706-adv7511-fmcdaq2 | [[xilinx>ZC706]] | the on-board [[adi>ADV7511]] and the [[/resources/eval/user-guides/ad-fmcdaq2-ebz|AD-FMCDAQ2-EBZ]] board | 
 +| zynq-zc706-adv7511-fmcdaq3 | [[xilinx>ZC706]] | the on-board [[adi>ADV7511]] and the [[/resources/eval/user-guides/ad-fmcdaq3-ebz|AD-FMCDAQ3-EBZ]] board | 
 +| zynq-zc706-adv7511-fmcjesdadc1 | [[xilinx>ZC706]] | the on-board [[adi>ADV7511]] and the [[/resources/eval/user-guides/ad-fmcjesdadc1-ebz|AD-FMCJESDADC1-EBZ]] board | 
 +| zynq-zc706-imageon | [[xilinx>ZC706]] | FMC-IMAGEON | 
 +| zynq-zed-adv7511 | [[http://zedboard.org/product/zedboard|Zed Board]] the on-board [[adi>ADV7511]] | 
 +| zynq-zed-adv7511-ad9361-fmcomms2-3 | [[http://zedboard.org/product/zedboard|Zed Board]] the on-board [[adi>ADV7511]] and the [[/resources/eval/user-guides/ad-fmcomms2-ebz|AD-FMCOMMS2-EBZ]] or [[/resources/eval/user-guides/ad-fmcomms3-ebz|AD-FMCOMMS3-EBZ]] board | 
 +| zynq-zed-adv7511-ad9364-fmcomms4 | [[http://zedboard.org/product/zedboard|Zed Board]] the on-board [[adi>ADV7511]] and the [[/resources/eval/user-guides/ad-fmcomms4-ebz|AD-FMCOMMS4-EBZ]] board | 
 +| zynq-zed-adv7511-ad9467-fmc-250ebz | [[http://zedboard.org/product/zedboard|Zed Board]] | the on-board [[adi>ADV7511]] and the [[/resources/eval/ad9467-fmc-250ebz|AD9467-FMC-250EBZ]] board | 
 +| zynq-zed-adv7511-cn0363 | [[http://zedboard.org/product/zedboard|Zed Board]] the on-board [[adi>ADV7511]] and the [[/resources/eval/user-guides/eval-cn0363-pmdz|EVAL-CN0363-PMDZ]] board  
 +| zynq-zed-imageon | [[http://zedboard.org/product/zedboard|Zed Board]] | FMC-IMAGEON |
  
  
resources/tools-software/linux-build/generic/zynq.txt · Last modified: 02 Feb 2024 16:08 by Marcelo Schmitt