Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:tools-software:linux-build:generic:raspberrypi [08 Dec 2021 15:13]
Antoniu Miclaus add doc for Pi Zero
resources:tools-software:linux-build:generic:raspberrypi [10 Mar 2022 10:13]
Michael Hennerich [Building for Raspberry PI]
Line 10: Line 10:
 The Raspberry PI branches are: The Raspberry PI branches are:
    * [[https://​github.com/​analogdevicesinc/​linux/​tree/​rpi-4.9.y|rpi-4.9.y]] - this is an older branch, when Raspberry PI's default kernel version was at 4.9 ; it's kept around for some older boards/​setups    * [[https://​github.com/​analogdevicesinc/​linux/​tree/​rpi-4.9.y|rpi-4.9.y]] - this is an older branch, when Raspberry PI's default kernel version was at 4.9 ; it's kept around for some older boards/​setups
-   * [[https://​github.com/​analogdevicesinc/​linux/​tree/​rpi-4.14.y|rpi-4.14.y]] - the current default Raspberry PI branch, also the official version of Raspbian at this point in time+   * [[https://​github.com/​analogdevicesinc/​linux/​tree/​rpi-5.10.y|rpi-5.10.y]] - the current default Raspberry PI branch, also the official version of Raspbian at this point in time
    * There maybe be a few other branches that start with **rpi-xxx** ; these should not be used, they will be removed in the future, and were used to test things sometime in the past.    * There maybe be a few other branches that start with **rpi-xxx** ; these should not be used, they will be removed in the future, and were used to test things sometime in the past.
  
resources/tools-software/linux-build/generic/raspberrypi.txt · Last modified: 10 Mar 2022 10:13 by Michael Hennerich