This shows you the differences between two versions of the page.
Last revisionBoth sides next revision | |||
resources:tools-software:freertos:legacy-versions [15 Nov 2022 23:39] – created Murray Anderson | resources:tools-software:freertos:legacy-versions [15 Nov 2022 23:46] – Add details of overlay Murray Anderson | ||
---|---|---|---|
Line 1: | Line 1: | ||
Whilst we always recommend using the latest version of FreeRTOS possible, we understand that older versions are often required for compatibility or compliance reasons. | Whilst we always recommend using the latest version of FreeRTOS possible, we understand that older versions are often required for compatibility or compliance reasons. | ||
- | The version 1.5.1 zip file containing FreeRTOS sources and Demos can be downloaded from [[adi> | + | === Zip file === |
+ | |||
+ | For releases up to ADI FreeRTOS version 1.5.x, source code for both upstream official FreeRTOS release, and the Analog Devices FreeRTOS add on product release are required. | ||
+ | |||
+ | The version 1.5.1 overlay | ||
+ | |||
+ | This zip file needs to be overlayed on top of a standard FreeRTOS version 10 directory which can be downloaded from | ||
+ | https:// | ||
+ | |||
+ | === Github === | ||
Previous versions of ADI FreeRTOS are available via Github. | Previous versions of ADI FreeRTOS are available via Github. | ||
+ | |||
There is a branch containing the latest ADI version for each FreeRTOS version : [[repo> | There is a branch containing the latest ADI version for each FreeRTOS version : [[repo> | ||
+ | |||
There is a tag for each ADI released version : [[repo> | There is a tag for each ADI released version : [[repo> |