Welcome to the Beta for the FreeRTOS Add-In for CrossCore Embedded Studio.
For any questions, feedback or support contact Murray Anderson (murray.anderson@analog.com).
Requires CrossCore Embedded Studio version 2.10.1 or 2.11.0 (http://analog.com/cces/)
FreeRTOS sources are self-contained so there’s no dependency on external sources.
This release supports the following hardware:
The Add-In currently only supports a Kernel based on FreeRTOS version 10.4.3 LTS Patch 2. You may be able to use the generated configuration files with other versions of FreeRTOS but this is not officially supported.
The Add-In can be installed via the Install New Software functionality from within CrossCore Embedded Studio. This is available under Help > Install New Software.
In the Work With field, select CrossCore Embedded Studio Software and Documentation - http://www.analog.com/static/ccesupdatesite. Expand the CrossCore Embedded Studio Add-Ins section, select FreeRTOS Add-in (Beta) and click on Next, Read and agree to the license text, and then click Finish
Double click on the system.svc in the top level of your project.
Click on the Add button to the right of the list of already installed Add-Ins.
Expand Middleware then select FreeRTOS for <core type> and click Finish.
The Add-In will want to modify the main() source with some code to create a task and start the scheduler. To prevent these changes being made, deselect your project from the list of Changes to be performed. Click Finish to Add the Add-In to your project. Sources files will be downloaded and created in your project so this may take a few moments.
Create a new project as normal, and when you get to the Projects and Settings page, click on configure for each project which you want to install FreeRTOS in.
Click on the Add button to the right of the list of already installed Add-Ins.
Expand Middleware then select FreeRTOS for <core type> and click Finish.
The Add-In will want to modify the main() source with some code to create a task and start the scheduler. To prevent these changes being made, deselect your project from the list of Changes to be performed. Click Finish to Add the Add-In to your project.
Double click on the system.svc in the top level of your project.
Click on the FreeRTOS tab along the bottom of the Configuration page:
The tabs along the left contain options within different categories. Making a change and saving the configuration (CTRL + S) will regenerate the appropriate files within your project.
The FreeRTOS Add-In makes 3 modifications to your project: Main, user modifiable sources and system sources.
The FreeRTOS Add-In will add code to your applications main function, which will create a task userStartupTask and then start the scheduler. You can either modify userStartupTask or create your own task(s).
A directory, CustomizableFreeRTOSSources will be added to your project, which contain generated code which can be modified by the user. FreeRTOSUserApplication.c contains the code for userStartUpTask, the default task created by main.
Another directory, FreeRTOS will be added to your project under system. This directory contains both the FreeRTOS Kernel and a generated configuration which is not user modifiable. You should not need to modify anything within the system directory, though it can be stepped through with the debugger or viewed for reference.
A Status view is available from within CrossCore Embedded Studio when connected to a debug session with a FreeRTOS project. It can be accessed via *Window > Show View > Other > Debug > RTOS Status* Currently it'll present information about all of the created tasks. Note: This is only currently available when debugging using the CCES Debugger and not OpenOCD