This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:tools-software:crosscore:cces:getting-started:boot-app-sc5xx [27 Aug 2019 16:13] – Steven MacDiarmid | resources:tools-software:crosscore:cces:getting-started:boot-app-sc5xx [27 Aug 2019 16:14] (current) – Steven MacDiarmid | ||
---|---|---|---|
Line 66: | Line 66: | ||
//Figure 7: The loader file has been created// | //Figure 7: The loader file has been created// | ||
| | ||
- | 11. Return to the [[resources: | + | 11. Return to the [[resources: |
//Aside:// When an application is loaded to a target using the debugger, the IDE can configure external memory as long as the processor is homogeneous (i.e. it has only SHARC cores). However, for heterogeneous processors, such as the ASDP-SC5xx series, which have an ARM core plus one or two SHARC cores, | //Aside:// When an application is loaded to a target using the debugger, the IDE can configure external memory as long as the processor is homogeneous (i.e. it has only SHARC cores). However, for heterogeneous processors, such as the ASDP-SC5xx series, which have an ARM core plus one or two SHARC cores, |