Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:tools-software:bfin:adas1000 [05 May 2016 18:18]
CatherineR there was somehting funny re the zip file
resources:tools-software:bfin:adas1000 [05 May 2016 18:26]
CatherineR
Line 19: Line 19:
 This project demonstrates a framework developed for Visual DSP [[adi>​vdsp-bf-sh-ts|Visual DSP]] to interface the [[adi>​ADAS1000]] to the [[adi>​adsp-bf527|ADSP-BF527]] on the SDP-B controller board. This project demonstrates a framework developed for Visual DSP [[adi>​vdsp-bf-sh-ts|Visual DSP]] to interface the [[adi>​ADAS1000]] to the [[adi>​adsp-bf527|ADSP-BF527]] on the SDP-B controller board.
  
-{{ :​resources:​tools-software:​bfin:​eval-adas1000sdz.jpg?​600 ​|}}+{{ :​resources:​tools-software:​bfin:​eval-adas1000sdz.jpg?​600 }}
  
  
Line 28: Line 28:
   * Display/​Plot the processed data   * Display/​Plot the processed data
  
-==== Requirements:​ ==== +==== Requirements:​ ====   
-  * VisualDSP++ 5.0 Update 10 +  * VisualDSP++ 5.0 Update 10
   * [[adi>​ADAS1000]] Eval Board setup, EVAL-ADAS1000SDZ   * [[adi>​ADAS1000]] Eval Board setup, EVAL-ADAS1000SDZ
-  * SDP-B Rev 1.3 (with Emulator to connect to VisualDSP++), ​[[adi>​SDP|EVAL-SDP-CB1Z]] +  * SDP-B Rev 1.3 (with Emulator to connect to VisualDSP++),​  
-  * Breakout board for SDP-B (If Hardware DRDY is used) [[adi>​SDP|ADZS-BRKOUT-EX3]]+  * Breakout board for SDP-B (If Hardware DRDY is used) 
   * ECG cables and simulator (if required) ​   * ECG cables and simulator (if required) ​
  
Line 38: Line 38:
 The attached zip file contains the relevant files for this project The attached zip file contains the relevant files for this project
  
-{{:​resources:​tools-software:​bfin:​adas1000_sdp_v1.zip|ADAS1000+SDP Framework}} 
  
 Zip File Contents & description: ​ Zip File Contents & description: ​
Line 89: Line 88:
     -       Right click on the plot > Configure > Modify '​Count'​ for number of samples     -       Right click on the plot > Configure > Modify '​Count'​ for number of samples
     -       Halt the code, to see the latest '​Count'​ number of samples plotted     -       Halt the code, to see the latest '​Count'​ number of samples plotted
 +===== Zip file===== 
 +{{:​resources:​tools-software:​bfin:​adas1000_sdp_v1.zip|}}
resources/tools-software/bfin/adas1000.txt · Last modified: 05 May 2016 18:26 by CatherineR