This is an old revision of the document!
ADI’s “Analysis, Control, Evaluation” (ACE) is a desktop software application which allows the evaluation and control of multiple evaluation systems, from across ADI’s product portfolio. The application consists of a common framework and individual component specific plug-ins.
ACE is designed to educate the user in the functional operation of the component and allow the user to access the system at a level of abstraction with which they are comfortable.
The ACE Software Suite requires the following minimum PC requirements:
The following items are required before the ACE Software Suite can be installed. If not present on your system, the ACE installer will install them by default.
ACE 1.5.2524.1004 - Updated March 8, 2017
Offline version - This installer contains the .NET 4.0 Client installer for target machines that don't have .NET 4.0 installed and don't have an internet connection available during installation.
The ACE User Guide provides details on
For ACE support please email ace.support@analog.com. All feedback is also welcome through this address and is much appreciated.