Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
Next revisionBoth sides next revision
resources:tools-software:ace [14 Mar 2018 23:03] – [ACE Does Not Discover High-Speed DAC Eval Boards] John Birnieresources:tools-software:ace [20 Aug 2019 15:18] – Added link to ACE user guide PDF Eoin Hanrahan
Line 3: Line 3:
 <note important>The ACE software installers and available plug-ins are now at [[http://www.analog.com/ace]] on the Analog Devices website.</note> <note important>The ACE software installers and available plug-ins are now at [[http://www.analog.com/ace]] on the Analog Devices website.</note>
  
-===== Known Issues =====+This Wiki will serve as a landing page for known issues and other ACE information.
  
-==== Board & Chip Diagrams Distorted (Regional Formatting Bug) ====+===== Contents ===== 
 +[[resources:tools-software:ace:fluentui|ACE UI Updates (2019)]]
  
-There is a known issue with some regional formats that causes bad loading and rendering of board and chip views.  When the problem occurs, you may see some shapes appear with missing content and exaggerated size.  The problem is particular to formats that use a comma (',') or any character besides '.' as the decimal separator.+[[resources:tools-software:ace:knownissues|Known Issues]]
  
-We will be working on a solution, but in the meantime there is a workaround.+[[resources:tools-software:ace:installscrub|Install Scrub/Refresh Instructions]]
  
-To use the workaround, you need to temporarily change the format settings in Windows to a format that uses '.' as the decimal separator such as English (United States). For example, in Windows 7, you can access the setting through Control Panel -> Change display language, click the Formats tab, and select "English (United States)" in the "Format" drop-down.+[[resources:tools-software:ace:remotecontrol|ACE Remote Control]]
  
-This issue is addressed in ACE versions 1.7++[[resources:tools-software:ace:fftanalysis|FFT Analysis Features]]
  
-{{ :resources:tools-software:formats.png?300 Region and Language : Formats }}+[[resources:tools-software:ace:highspeedadctriggercapture|High Speed ADC Trigger Capture]]
  
 +[[resources:tools-software:ace:exporting|Exporting Interaction With Hardware]]
  
-==== ACE or SDP Driver Install Fails or Warns me the driver/exe is unsigned ==== 
  
-Warnings may be safely ignored and dismissed, but they do highlight likely issues with your PC. The SDPDrivers and ACE package uses the latest signing technology and your PC may be out of date and unable to recognise the signing key. +====== External Links ====== 
- +[[http://swdownloads.analog.com/ACE/ACE_User_Manual_rev3.pdf|ACE User Guide v3]]
-  - Make sure the PC is connected to the Internet and can get root certificate updates, normally this happens automatically. +
-  - Check group policies to automatically update these run gpedit.msc +
-    - Make sure the setting below is either Not Configured or Disabled +
-    - {{ :resources:tools-software:updateroot.png?1000 |UpdateRoot.png}} +
-  - Check for and install all the latest Windows updates +
-  - Check your group policy settings, these may be controlled by IT or a System Administrator +
-  - Ideally select Warn as the safer option in case you later encounter malicious software +
-  - Run gpedit.msc and navigate to the setting below +
-    - {{ :resources:tools-software:codesigning.png?1000 |CodeSigning.png}} +
- +
- +
-==== ACEZIP File Installation Unsuccessful Due to Security Block ==== +
- +
-In some cases downloading an ACEZIP file from an e-mail or from a remote/networked location has caused the file to become blocked by a security feature in Windows. This is not made clear during the download process but when the user attempts to install the ACE plug-in it will not work correctly.  +
- +
-If this happens, follow these steps to verify the ACEZIP has not been blocked and resolve the issue if it has: +
-    - Right click the file. +
-    - Select properties in the context menu. +
-    - Under the General tab, if a file has been blocked a new Security tag and Unblock button will have appeared. {{ :resources:tools-software:acezipfileaccessissue.png |}} +
-    - Click Unblock.     +
-    - Retry the plug-in installation by double clicking the ACEZIP. +
- +
- +
-==== ACE Does Not Discover High-Speed DAC Eval Boards ==== +
- +
-The High-Speed DAC boards have a second on-board USB controller, make sure this is connected as well as the main FPGA controller boardTo avoid potential confusion, ACE only reports boards on the second controller (where it is required). +
- +
-There is also a known driver conflict issue between the NI VISA driver and Keysight's VISA driver (used for automation of equipment). To work around this, you will need to uninstall the Keysight Driver. +
- +
-If you need to automate equipment and use ACE at the same time you might have to use two separate PCs. The ACE remote control/scripting interface can be used by networking the PCs and setting Firewall rules appropriately. +
- +
- +
-Another possible issue causing ACE to not detect Hsdac boards is an outdated version of the "Evaluation Board Service" library. This library is installed as part of DPGDownloader and always contains the latest version. However, the "BitFlipper" application installer overwrites the currently installed version of the library with an incompatible one. Reinstalling the latest version of DPGDownloader will restore the correct version of the library. +
- +
-This is the ACE error log indicating an incompatible version of the "Evaluation Board Service" library: +
- +
-  Could not initialise DPG Client System.Exception: Could not query DPG3 for connected evaluation boards ---> System.Exception: DeviceNotResponding +
-   at AnalogDevices.DPG.USB.CSA_USB.ControlIn(Int16 requestType, Int16 request, UInt16 wValue, UInt16 wIndex, Int16 length) +
-   at AnalogDevices.DPG.EvaluationBoards.Communication.DPG3_CSA.Finder.AttachedBoards(String[DevicePaths)+
resources/tools-software/ace.txt · Last modified: 22 Aug 2023 21:05 by Eoin Hanrahan