This is an old revision of the document!
This WIKI site will introduce ACE and ACE Plug-ins with a brief description and also take you through the installation steps to get the ACE application installed on your machine.
You can return to the ACE WIKI Homepage here: ACE Homepage
ACE stands for Analysis | Control | Evaluation and is a proprietary software developed at ADI to facilitate the evaluation and control of multiple evaluation systems, from across ADI’s portfolio.
ACE is a desktop software that runs on the Windows Operating system.
Supported OS:
Legacy OS:
Older versions of ACE were supported on previous versions of the Windows OS and may still retain some functionality but they are no longer supported and are not actively tested for compatibility with the software. Use of the ACE software cannot be guarenteed on these platforms.
The latest version of ACE is available from www.analog.com/ace. Simply download the latest installer and run it to launch the ACE Setup Wizard. This step by step installation will guide you when installing ACE and it's accompanying software support modules as necessary.
Newer versions of ACE ship with a mixed x64 and x86 installation allowing you to run either from your local machine. The default locations for the application to install are as follows:
Uninstalling ACE is done using the uninstall.exe located in the x86 installation directory. This will uninstall both the x86 and x64 version of the application.
Uninstalling ACE with the default settings will only remove the currently installed application and leave all current user settings, ACE plug-ins, session files etc. installed on your machine. It can be preferable to remove all of this content from your machine under certain circumstances, for example if you find your installation has entered an unknown state and you would like to restore ACE to factory settings.
To remove all ACE content for your installation you can perform a “Scrub Uninstall”, either manually or using the option to Scrub during the uninstall.exe wizard.
You can find more information about this process here: Uninstall Scrub
ACE consists of a common software framework and individual component specific “plug-ins”. An ACE plug-in is a piece of software written using the ACE framework to evaluate a particular product or product group. ACE is driven by the plug-ins available to the application. The plug-ins are added to ACE as software extensions when they are installed through the application plug-in management tool. The plug-ins themselves provide ACE with the information used to evaluate the products (boards and chips) supported by a particular plug-in.
Use the Quickstart Guides below to understand how to launch the ACE application for the first time and start downloading new plug-ins to start your product evaluation: