Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:tools-software:ace:userguide:quickstart [21 Feb 2020 10:24]
Eoin Hanrahan
resources:tools-software:ace:userguide:quickstart [27 Jan 2021 22:34]
Robin Getz use adi> interwiki links
Line 60: Line 60:
 **ACEZIP Installation** **ACEZIP Installation**
  
-ACE also allows plug-in installation from a special file type called an ACEZIP. Plug-ins are often packaged as ACEZIP files and made available through the analog.com website. You can find them in a list on the main [[http://​analog.com/​ace|ACE Software Homepage]] or on the product evaluation page of the specific product being evaluated.+ACE also allows plug-in installation from a special file type called an ACEZIP. Plug-ins are often packaged as ACEZIP files and made available through the analog.com website. You can find them in a list on the main [[adi>ace|ACE Software Homepage]] or on the product evaluation page of the specific product being evaluated.
 <note important>​Not all ACE plug-ins have shipped with an ACEZIP, if you can't find an ACEZIP file on a product page there is a chance you could still find it in the plug-in manager. If not, then maybe there is no ACE plug-in available for the product yet.</​note>​ <note important>​Not all ACE plug-ins have shipped with an ACEZIP, if you can't find an ACEZIP file on a product page there is a chance you could still find it in the plug-in manager. If not, then maybe there is no ACE plug-in available for the product yet.</​note>​
 To install from an ACEZIP file, simply download the file and double click on it. The only prerequisite for the installation is that you have ACE installed. ACEZIP files have a special association with the ACE application. Once you execute the ACEZIP file, it will install the plug-in packaged within it and also launch a new instance of the ACE application so you can quickly get up and running with your new software. To install from an ACEZIP file, simply download the file and double click on it. The only prerequisite for the installation is that you have ACE installed. ACEZIP files have a special association with the ACE application. Once you execute the ACEZIP file, it will install the plug-in packaged within it and also launch a new instance of the ACE application so you can quickly get up and running with your new software.
resources/tools-software/ace/userguide/quickstart.txt · Last modified: 27 Jan 2021 22:34 by Robin Getz