This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:tools-software:ace:remotecontrol [14 Nov 2018 10:28] – [Examples] Ciaran Watterson | resources:tools-software:ace:remotecontrol [13 Dec 2018 20:04] – Added LabVIEW 2015 example. Michael Sink | ||
---|---|---|---|
Line 6: | Line 6: | ||
===== Examples ===== | ===== Examples ===== | ||
+ | |||
+ | ==== Python ==== | ||
=== Large Data Capture With AD9208 === | === Large Data Capture With AD9208 === | ||
+ | |||
Currently 1GB of data can be captured with the ADS8V1 and 2GB of data can be captured with the ADS7V2 using the AsyncRawCaptureToFile transaction. The following example shows how this transaction can be used from a Python script with the AD9208 evaluation platform. | Currently 1GB of data can be captured with the ADS8V1 and 2GB of data can be captured with the ADS7V2 using the AsyncRawCaptureToFile transaction. The following example shows how this transaction can be used from a Python script with the AD9208 evaluation platform. | ||
Line 50: | Line 53: | ||
Download Python and Jupyter Notebook versions of this example: | Download Python and Jupyter Notebook versions of this example: | ||
{{ : | {{ : | ||
+ | |||
+ | ==== LabVIEW ==== | ||
+ | |||
+ | More information on the following example will be added. | ||
+ | |||
+ | {{ : | ||