resources:tools-software:ace:knownissues [27 Apr 2020 15:40]
Frank Meaney Added graphing updates
resources:tools-software:ace:knownissues [30 Jun 2021 13:54] (current)
Ciaran Watterson
Line 18: Line 18:
  
 On some machines it has been found that the ACE application is not graphing as expected. On some machines it has been found that the ACE application is not graphing as expected.
-If this occurs then open the settings tab in ACE and follow these steps  +If this occurs then open the settings tab in ACE and toggle ​the “Use Hardware Acceleration” checkbox.
-Toggle ​the “Use Hardware Acceleration” checkbox.+
 Also please check that the PC in question has the most UpToDate graphics driver. ​ Also please check that the PC in question has the most UpToDate graphics driver. ​
  
Line 26: Line 25:
  
 Note: ACE will need to be restarted to reflect any changes made on this settings page.  Note: ACE will need to be restarted to reflect any changes made on this settings page. 
-this  
   ​   ​
 ===== High-Speed DAC Eval Boards are not discovered ===== ===== High-Speed DAC Eval Boards are not discovered =====
Line 41: Line 39:
 The recommended action if you are actively using these High-Speed DAC Eval Boards with dedicated SPI applications is to not select the options discussed above. ​ The recommended action if you are actively using these High-Speed DAC Eval Boards with dedicated SPI applications is to not select the options discussed above. ​
  
-^ Not yet supported through ACE ^ Supported through ACE with DPGDownloaderLite ​+^Not yet supported through ACE ••• ​^Supported through ACE with DPG Lite 
-| AD9963/61 | AD9129/19 | +|AD9963/61 |AD9129/19 | 
-| AD9148 | AD9122/​21/​25 | +|AD9148 |AD9122/​21/​25 | 
-| AD9789 | AD9135 | +|AD9789 |AD9135 | 
-| AD9993 | AD9136 | +|AD9993 |AD9136 | 
-| | AD9142A | +| |AD9142A | 
-| | AD9144 | +| |AD9144 | 
-| | AD9162/​1/​3/​4 | +| |AD9162/​1/​3/​4 | 
-| | AD9172/​1/​3/​4/​5/​6 | +| |AD9172/​1/​3/​4/​5/​6 | 
-| | AD9739A/7A | +| |AD9739A/7A | 
-| | AD9747/​6/​5/​3/​1 | +| |AD9747/​6/​5/​3/​1 | 
-| | AD9783/​81/​80 | +| |AD9783/​81/​80 | 
-| | AD9717/​16/​15/​14 | +| |AD9717/​16/​15/​14 | 
-| | AD9117/​16/​15/​14 | +| |AD9117/​16/​15/​14 | 
-| | AD9707/​06/​05/​04 | +| |AD9707/​06/​05/​04 | 
-| | AD9736/​35/​34 | +| |AD9736/​35/​34 | 
-| | AD9779A/​78A/​76A | +| |AD9779A/​78A/​76A | 
-| | AD9146 | +| |AD9146 | 
-| | AD9739/37 | +| |AD9739/37 | 
-| | AD9788/​87/​85 | +| |AD9788/​87/​85 | 
-| | AD9748/​44/​42/​40 (on DPGDownloaderLite ​only) | +| |AD9748/​44/​42/​40 (on DPG Lite only) | 
-| | AD9767/​65/​63/​09 (on DPGDownloaderLite ​only) |+| |AD9767/​65/​63/​09 (on DPG Lite only) |
  
 \\ \\
Line 140: Line 138:
 </​WRAP>​ </​WRAP>​
  
-Some of the earlier versions of ACE Release 1.13 had an issue where the ACE updater was not detecting and downloading the latest version of ACE. If this happens, simply download the latest version of ACE from the [[https://​www.analog.com/​en/​design-center/​evaluation-hardware-and-software/​ace-software.html|Analog Website]] and install manually. ​+Some of the earlier versions of ACE Release 1.13 had an issue where the ACE updater was not detecting and downloading the latest version of ACE. If this happens, simply download the latest version of ACE from the [[adi>en/​design-center/​evaluation-hardware-and-software/​ace-software.html|Analog Website]] and install manually. ​
  
 This was resolved in ACE version 1.14.2763.1212. This was resolved in ACE version 1.14.2763.1212.
resources/tools-software/ace/knownissues.1587994811.txt.gz · Last modified: 27 Apr 2020 15:40 by Frank Meaney