resources:tools-software:ace:knownissues [10 Jan 2020 15:29]
Frank Meaney [Contact ACE Support]
resources:tools-software:ace:knownissues [30 Jun 2021 13:54] (current)
Ciaran Watterson
Line 1: Line 1:
-====== Known Issues ======+======= Known Issues ​(ACE Software) ​====== 
 + 
 +You can return to the ACE WIKI Homepage here: 
 +**[[resources:​tools-software:​ace|ACE Homepage]]**
  
 ===== ACEZIP File Installation Unsuccessful Due to Security Block ===== ===== ACEZIP File Installation Unsuccessful Due to Security Block =====
Line 12: Line 15:
     - Retry the plug-in installation by double clicking the ACEZIP.     - Retry the plug-in installation by double clicking the ACEZIP.
  
 +===== Graphing Issues =====
  
 +On some machines it has been found that the ACE application is not graphing as expected.
 +If this occurs then open the settings tab in ACE and toggle the “Use Hardware Acceleration” checkbox.
 +Also please check that the PC in question has the most UpToDate graphics driver. ​
 +
 +{{:​resources:​tools-software:​ace:​graphing_issue_2.png?​600|}}
 +
 +
 +Note: ACE will need to be restarted to reflect any changes made on this settings page. 
 +  ​
 ===== High-Speed DAC Eval Boards are not discovered ===== ===== High-Speed DAC Eval Boards are not discovered =====
  
Line 18: Line 31:
  
 \\ \\
-As of version 1.14, ACE replaces the driver ​of the on-board controller to avoid any of the conflicts with VISA drivers listed below and installs ​the DPGDownloaderLite ​application to replace the High-Speed DAC Software Suite.+As of version 1.15, ACE includes an option to use ADI SDP driver ​for the on-board ​USB controller to avoid any of the conflicts with VISA drivers listed below and another option to install ​the DPG Lite application to replace the High-Speed DAC Software Suite. 
 +Both options can be activated by selecting the "High Speed DAC Components"​ option upon installation:​ 
 +{{ :​resources:​tools-software:​ace:​hsdac_install.png?​nolink&​400 |}}
  
 +\\
 However, at this time, the High-Speed DAC Eval Boards listed below are not yet supported through ACE but through a dedicated SPI application that requires the NI VISA driver. However, at this time, the High-Speed DAC Eval Boards listed below are not yet supported through ACE but through a dedicated SPI application that requires the NI VISA driver.
-The recommended action if you are actively using these High-Speed DAC Eval Boards with dedicated SPI applications is to not update to ACE version 1.14 or install version 1.13 available [[http://​swdownloads.analog.com/​ACE/​ACEInstall_1.13.2728.1194.exe|here]]+The recommended action if you are actively using these High-Speed DAC Eval Boards with dedicated SPI applications is to not select the options discussed above
  
-^ Not yet supported through ACE ^ Supported through ACE with DPGDownloaderLite ​+^Not yet supported through ACE ••• ​^Supported through ACE with DPG Lite 
-AD9783/81/80 | AD9129/19 | +|AD9963/61 |AD9129/19 | 
-AD9717/​16/​15/​14 ​| AD9122/​21/​25 | +|AD9148 ​|AD9122/​21/​25 | 
-AD9117/​16/​15/​14 ​| AD9135 | +|AD9789 ​|AD9135 | 
-AD9707/​06/​05/​04 ​| AD9136 | +|AD9993 ​|AD9136 | 
-AD9736/​35/​34 ​| AD9142A | +| |AD9142A | 
-AD9779A/​78A/​76A ​| AD9144 | +| |AD9144 | 
-AD9748/​44/​42/​40 ​| AD9162/​1/​3/​4 | +| |AD9162/​1/​3/​4 | 
-AD9148 ​| AD9172/​1/​3/​4/​5/​6 | +| |AD9172/​1/​3/​4/​5/​6 | 
-AD9146 ​| AD9739A/7A | +| |AD9739A/7A | 
-AD9739/​37 ​| AD9747/​6/​5/​3/​1 | +| |AD9747/​6/​5/​3/​1 | 
-AD9788/87/85 | | +|AD9783/81/80 | 
-AD9789 ​| | +| |AD9717/​16/​15/​14 ​
-AD9993 ​| | +| |AD9117/​16/​15/​14 ​
-AD9963/61 | | +| |AD9707/​06/​05/​04 ​
-| AD9767/​65/​63/​09 ​|+|AD9736/35/34 | 
 +| |AD9779A/​78A/​76A ​
 +| |AD9146 | 
 +| |AD9739/37 | 
 +| |AD9788/​87/​85 | 
 +| |AD9748/​44/​42/​40 (on DPG Lite only) | 
 +|AD9767/​65/​63/​09 ​(on DPG Lite only) |
  
 \\ \\
-For ACE version 1.13 and earlier, there is a known driver conflict issue between the NI VISA driver and Keysight'​s VISA driver (used for automation of equipment). To work around this, try setting the Keysight VISA driver as the secondary VISA driver. This can be done with the Keysight installer. If this doesn'​t work, you may need to uninstall the Keysight Driver.\\+If the HSDAC components are not installed, there is a known driver conflict issue between the NI VISA driver and Keysight'​s VISA driver (used for automation of equipment). To work around this, try setting the Keysight VISA driver as the secondary VISA driver. This can be done with the Keysight installer. If this doesn'​t work, you may need to uninstall the Keysight Driver.\\
 \\ \\
 The same workaround may be necessary for Rhode-Schwarz VISA. The same workaround may be necessary for Rhode-Schwarz VISA.
Line 116: Line 138:
 </​WRAP>​ </​WRAP>​
  
-Some of the earlier versions of ACE Release 1.13 had an issue where the ACE updater was not detecting and downloading the latest version of ACE. If this happens, simply download the latest version of ACE from the [[https://​www.analog.com/​en/​design-center/​evaluation-hardware-and-software/​ace-software.html|Analog Website]] and install manually. ​+Some of the earlier versions of ACE Release 1.13 had an issue where the ACE updater was not detecting and downloading the latest version of ACE. If this happens, simply download the latest version of ACE from the [[adi>en/​design-center/​evaluation-hardware-and-software/​ace-software.html|Analog Website]] and install manually. ​
  
 This was resolved in ACE version 1.14.2763.1212. This was resolved in ACE version 1.14.2763.1212.
Line 156: Line 178:
 This issues has been fixed with the latest release of ACE, v1.15.2818.1254 This issues has been fixed with the latest release of ACE, v1.15.2818.1254
 </​note>​ </​note>​
 +
 +
 +===== ACEZIP file crashing when launched =====
 +
 +In some cases when you try to open an ACEZIP file it may result in the ACE application crashing. ​
 +
 +If this happens, follow these steps to add the plug-in within the ACE application.
 +  - Open ACE 
 +  - Click on Plug-In MarketPlace (Plug-in manager)
 +  - Click on Installed Packages ​
 +  - Enter the name of the plug-in to the search box eg. AD1234
 +  - If the plug-in is found then Select it and click "​Uninstall Selected"​
 +  - Click on Settings ​
 +  - Click on Plug-ins ​
 +  - Click on the + sign to the right of the "​Zipped Plug-in Sources" ​
 +  - Under name , enter a new value eg "​NewSource"​
 +  - In the Source Column click on the box with three dots  "​..."​.
 +  - When the pop-up opens find and select the ACEZIP file  ​
 +  - Click open (This will now have created a new Zipped Plug-in source )
 +  - Click Ok to return to the "​Plug-in Manager" ​
 +  - Click on "​Available Packages "
 +  - Click on the name you used in step 9 "​NewSource"​
 +  - Click on available plug-in eg. Board.AD1234
 +  - Click "​Install Selected" ​
 +  - Click Close (The plug-in should now be available for use)
  
 ===== Contact ACE Support ===== ===== Contact ACE Support =====
 <note important>​ <note important>​
  
-If the above issues ​do not resolve your issue then  +If the above solutions ​do not resolve your issuethen please ​use the "​Report Issue" function from the ACE menu. 
-use the "​Report Issue" function from the ACE menu.+This will generate an email to the ACE support team (and attach any relevant diagnostic files) 
 + 
 +{{:​resources:​tools-software:​ace:​ace_report_issue.png?​200|}}
  
 Alternatively please contact ACE support at  Alternatively please contact ACE support at 
resources/tools-software/ace/knownissues.1578666590.txt.gz · Last modified: 10 Jan 2020 15:29 by Frank Meaney