This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:tools-software:ace:knownissues [27 Apr 2020 15:40] – [Graphing Issues] Frank Meaney | resources:tools-software:ace:knownissues [30 Jun 2021 13:54] – Ciaran Watterson | ||
---|---|---|---|
Line 18: | Line 18: | ||
On some machines it has been found that the ACE application is not graphing as expected. | On some machines it has been found that the ACE application is not graphing as expected. | ||
- | If this occurs then open the settings tab in ACE and follow these steps | + | If this occurs then open the settings tab in ACE and toggle |
- | Toggle | + | |
Also please check that the PC in question has the most UpToDate graphics driver. | Also please check that the PC in question has the most UpToDate graphics driver. | ||
Line 40: | Line 39: | ||
The recommended action if you are actively using these High-Speed DAC Eval Boards with dedicated SPI applications is to not select the options discussed above. | The recommended action if you are actively using these High-Speed DAC Eval Boards with dedicated SPI applications is to not select the options discussed above. | ||
- | ^ Not yet supported through ACE ^ Supported through ACE with DPGDownloaderLite | + | ^Not yet supported through ACE ••• |
- | | AD9963/61 | AD9129/19 | | + | |AD9963/61 |AD9129/19 | |
- | | AD9148 | AD9122/ | + | |AD9148 |AD9122/ |
- | | AD9789 | AD9135 | | + | |AD9789 |AD9135 | |
- | | AD9993 | AD9136 | | + | |AD9993 |AD9136 | |
- | | | AD9142A | | + | | |AD9142A | |
- | | | AD9144 | | + | | |AD9144 | |
- | | | AD9162/ | + | | |AD9162/ |
- | | | AD9172/ | + | | |AD9172/ |
- | | | AD9739A/7A | | + | | |AD9739A/7A | |
- | | | AD9747/ | + | | |AD9747/ |
- | | | AD9783/ | + | | |AD9783/ |
- | | | AD9717/ | + | | |AD9717/ |
- | | | AD9117/ | + | | |AD9117/ |
- | | | AD9707/ | + | | |AD9707/ |
- | | | AD9736/ | + | | |AD9736/ |
- | | | AD9779A/ | + | | |AD9779A/ |
- | | | AD9146 | | + | | |AD9146 | |
- | | | AD9739/37 | | + | | |AD9739/37 | |
- | | | AD9788/ | + | | |AD9788/ |
- | | | AD9748/ | + | | |AD9748/ |
- | | | AD9767/ | + | | |AD9767/ |
\\ | \\ | ||
Line 139: | Line 138: | ||
</ | </ | ||
- | Some of the earlier versions of ACE Release 1.13 had an issue where the ACE updater was not detecting and downloading the latest version of ACE. If this happens, simply download the latest version of ACE from the [[https:// | + | Some of the earlier versions of ACE Release 1.13 had an issue where the ACE updater was not detecting and downloading the latest version of ACE. If this happens, simply download the latest version of ACE from the [[adi>en/ |
This was resolved in ACE version 1.14.2763.1212. | This was resolved in ACE version 1.14.2763.1212. |