This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:tools-software:ace:knownissues [23 Aug 2019 17:55] – [High-Speed DAC Eval Boards are not discovered] Max Lehuraux | resources:tools-software:ace:knownissues [23 Aug 2019 19:45] – [High-Speed DAC Eval Boards are not discovered] Max Lehuraux | ||
---|---|---|---|
Line 20: | Line 20: | ||
As of version 1.14, ACE replaces the driver of the on-board controller to avoid any of the conflicts with VISA drivers listed below and installs the DPGDownloaderLite application to replace the High-Speed DAC Software Suite. | As of version 1.14, ACE replaces the driver of the on-board controller to avoid any of the conflicts with VISA drivers listed below and installs the DPGDownloaderLite application to replace the High-Speed DAC Software Suite. | ||
- | However, at this time, some High-Speed DAC Eval Boards are not yet supported through ACE but through a dedicated SPI application that requires the NI VISA driver. | + | However, at this time, the High-Speed DAC Eval Boards |
The recommended action if you are actively using these High-Speed DAC Eval Boards with dedicated SPI applications is to not update to ACE version 1.14 or install version 1.13 available [[http:// | The recommended action if you are actively using these High-Speed DAC Eval Boards with dedicated SPI applications is to not update to ACE version 1.14 or install version 1.13 available [[http:// | ||
+ | |||
+ | ^ Not yet supported through ACE ^ Supported through ACE with DPGDownloaderLite ^ | ||
+ | | AD9783/ | ||
+ | | AD9717/ | ||
+ | | AD9117/ | ||
+ | | AD9707/ | ||
+ | | AD9736/ | ||
+ | | AD9779A/ | ||
+ | | AD9748/ | ||
+ | | AD9148 | AD9172/ | ||
+ | | AD9146 | AD9739A/7A | | ||
+ | | AD9739/37 | AD9747/ | ||
+ | | AD9788/ | ||
+ | | AD9789 | | | ||
+ | | AD9993 | | | ||
+ | | AD9963/61 | | | ||
+ | | AD9767/ | ||
\\ | \\ |