This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:tools-software:ace:knownissues [27 Feb 2020 12:44] – update to ACEZIP file fail Frank Meaney | resources:tools-software:ace:knownissues [30 Jun 2021 13:54] – Ciaran Watterson | ||
---|---|---|---|
Line 15: | Line 15: | ||
- Retry the plug-in installation by double clicking the ACEZIP. | - Retry the plug-in installation by double clicking the ACEZIP. | ||
+ | ===== Graphing Issues ===== | ||
+ | On some machines it has been found that the ACE application is not graphing as expected. | ||
+ | If this occurs then open the settings tab in ACE and toggle the “Use Hardware Acceleration” checkbox. | ||
+ | Also please check that the PC in question has the most UpToDate graphics driver. | ||
+ | |||
+ | {{: | ||
+ | |||
+ | |||
+ | Note: ACE will need to be restarted to reflect any changes made on this settings page. | ||
+ | | ||
===== High-Speed DAC Eval Boards are not discovered ===== | ===== High-Speed DAC Eval Boards are not discovered ===== | ||
Line 29: | Line 39: | ||
The recommended action if you are actively using these High-Speed DAC Eval Boards with dedicated SPI applications is to not select the options discussed above. | The recommended action if you are actively using these High-Speed DAC Eval Boards with dedicated SPI applications is to not select the options discussed above. | ||
- | ^ Not yet supported through ACE ^ Supported through ACE with DPGDownloaderLite | + | ^Not yet supported through ACE ••• |
- | | AD9963/61 | AD9129/19 | | + | |AD9963/61 |AD9129/19 | |
- | | AD9148 | AD9122/ | + | |AD9148 |AD9122/ |
- | | AD9789 | AD9135 | | + | |AD9789 |AD9135 | |
- | | AD9993 | AD9136 | | + | |AD9993 |AD9136 | |
- | | | AD9142A | | + | | |AD9142A | |
- | | | AD9144 | | + | | |AD9144 | |
- | | | AD9162/ | + | | |AD9162/ |
- | | | AD9172/ | + | | |AD9172/ |
- | | | AD9739A/7A | | + | | |AD9739A/7A | |
- | | | AD9747/ | + | | |AD9747/ |
- | | | AD9783/ | + | | |AD9783/ |
- | | | AD9717/ | + | | |AD9717/ |
- | | | AD9117/ | + | | |AD9117/ |
- | | | AD9707/ | + | | |AD9707/ |
- | | | AD9736/ | + | | |AD9736/ |
- | | | AD9779A/ | + | | |AD9779A/ |
- | | | AD9146 | | + | | |AD9146 | |
- | | | AD9739/37 | | + | | |AD9739/37 | |
- | | | AD9788/ | + | | |AD9788/ |
- | | | AD9748/ | + | | |AD9748/ |
- | | | AD9767/ | + | | |AD9767/ |
\\ | \\ | ||
Line 128: | Line 138: | ||
</ | </ | ||
- | Some of the earlier versions of ACE Release 1.13 had an issue where the ACE updater was not detecting and downloading the latest version of ACE. If this happens, simply download the latest version of ACE from the [[https:// | + | Some of the earlier versions of ACE Release 1.13 had an issue where the ACE updater was not detecting and downloading the latest version of ACE. If this happens, simply download the latest version of ACE from the [[adi>en/ |
This was resolved in ACE version 1.14.2763.1212. | This was resolved in ACE version 1.14.2763.1212. |