This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:tools-software:ace:knownissues [22 Jan 2024 13:56] – [IIO Controllers not being detected] Sid Balasubramanian | resources:tools-software:ace:knownissues [22 Jan 2024 14:07] (current) – [IIO Controllers not being detected] Sid Balasubramanian | ||
---|---|---|---|
Line 228: | Line 228: | ||
IIO currently does not work with ACE x86. It requires the 64-bit version of ACE. | IIO currently does not work with ACE x86. It requires the 64-bit version of ACE. | ||
+ | |||
+ | === IIO WCF Wrapper === | ||
+ | |||
+ | If you're having issues with IIO controllers and are seeing a console application opening up along with ACE called IIOWCFServerHelper or LibIIO WCF Server, you might be running older versions of the IIO packages and can possibly encounter issues when loading plugins. | ||
+ | |||
+ | {{: | ||
+ | |||
+ | To resolve this, you'll need to update your packages using the ACE plugin manager. | ||
+ | |||
+ | - Open ACE and navigate to the **Plug-in Manager** using the sidebar on the left. | ||
+ | - Click on the **Available Updates** tab. | ||
+ | - Click Update All and wait for the process to complete. Restart ACE if you're prompted to do so. | ||
+ | - Repeat the process one more time to make sure all packages are updated. | ||
=== Visual Studio redistributables === | === Visual Studio redistributables === |