This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:ace:highspeedadctriggercapture [22 Aug 2018 22:32] – Added screenshots and updated instructions. Michael Sink | resources:tools-software:ace:highspeedadctriggercapture [07 Nov 2018 15:30] (current) – Michael Sink | ||
---|---|---|---|
Line 15: | Line 15: | ||
Option A: If the plug-in has a button to allow navigation to the FPGA memory map, then click it and modify register 0x0106 bit 1 in the GUI, as shown in the following two screenshots. | Option A: If the plug-in has a button to allow navigation to the FPGA memory map, then click it and modify register 0x0106 bit 1 in the GUI, as shown in the following two screenshots. | ||
- | {{ : | + | {{ : |
- | {{ : | + | {{ : |
- | Option B: If the plug-in does not have this button, you'll need to execute a macro. | + | Option B: If the plug-in does not have this button, you'll need to execute a macro. |
+ | < | ||
+ | -- Analog Devices, Inc. evaluation macro file | ||
+ | @Subsystem_1.ADS7-V2.AD9208 FPGA: Evaluation.Control.SetRegisterBit(0x106, | ||
+ | @Subsystem_1.ADS7-V2.AD9208 FPGA: @ApplySettings(); | ||
+ | </ | ||
+ | Be sure to click the **Play** button in the **Macro Tools** to execute the macro. | ||
+ | |||
+ | {{ : | ||
4. Go to the Analysis view in ACE and click **Run Once**. | 4. Go to the Analysis view in ACE and click **Run Once**. | ||
- | {{ : | + | {{ : |
5. Wait for falling edge (1.8V) output on SMA J6 (or wait long enough to ensure system is ready). | 5. Wait for falling edge (1.8V) output on SMA J6 (or wait long enough to ensure system is ready). | ||
- | {{ : | + | {{ : |
6. Pulse trigger input or turn off input to 0V. Minimum pulse width of trigger is 640 divided by the serial line rate. | 6. Pulse trigger input or turn off input to 0V. Minimum pulse width of trigger is 640 divided by the serial line rate. | ||
- | Once trigger has been applied, ACE should capture and refresh the data onscreen. | + | Once the trigger has been applied, ACE should capture and refresh the data onscreen. |
- | {{ : | + | {{ : |