This shows you the differences between two versions of the page.
Next revision | Previous revision | ||
resources:tools-software:ace:highspeedadctriggercapture [22 Aug 2018 21:56] – created Michael Sink | resources:tools-software:ace:highspeedadctriggercapture [07 Nov 2018 15:30] (current) – Michael Sink | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== High Speed ADC Trigger Capture ====== | ====== High Speed ADC Trigger Capture ====== | ||
+ | ===== ADS7V2 Instructions ===== | ||
+ | |||
+ | The following instructions were created using the AD9208 evaluation board. | ||
+ | |||
+ | <note important> | ||
+ | |||
+ | 1. Configure the plug-in/ | ||
+ | |||
+ | 2. Apply a 1.8V input to SMA J5 on the ADS7V2 board. | ||
+ | |||
+ | 3. Enable external trigger mode by writing a 1 to bit[1] of FPGA register 0x0106. | ||
+ | |||
+ | Option A: If the plug-in has a button to allow navigation to the FPGA memory map, then click it and modify register 0x0106 bit 1 in the GUI, as shown in the following two screenshots. | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | Option B: If the plug-in does not have this button, you'll need to execute a macro. | ||
+ | |||
+ | < | ||
+ | -- Analog Devices, Inc. evaluation macro file | ||
+ | @Subsystem_1.ADS7-V2.AD9208 FPGA: Evaluation.Control.SetRegisterBit(0x106, | ||
+ | @Subsystem_1.ADS7-V2.AD9208 FPGA: @ApplySettings(); | ||
+ | </ | ||
+ | |||
+ | Be sure to click the **Play** button in the **Macro Tools** to execute the macro. | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | 4. Go to the Analysis view in ACE and click **Run Once**. | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | 5. Wait for falling edge (1.8V) output on SMA J6 (or wait long enough to ensure system is ready). | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | 6. Pulse trigger input or turn off input to 0V. Minimum pulse width of trigger is 640 divided by the serial line rate. | ||
+ | |||
+ | Once the trigger has been applied, ACE should capture and refresh the data onscreen. | ||
+ | |||
+ | {{ : |