You can return to the ACE Application User Guide Homepage here: Application User Guide
When a subsystem is added to the system ACE automatically tries to acquire the associated hardware. After this point hardware can be acquired or released through the acquire/release menu in the System View which can be access by clicking on the USB connectivity button, see System View for more information.
Where available initialization wizards provide a setup process which collects and applies the initial startup conditions for a board and all its components. Once the software inputs are complete pressing the apply button will perform all necessary writes and reads in order to put the hardware into the defined state, see Board View for more Information
The view toolbars in each of the Board, Chip and Memory Map views provide controls for communicating with hardware. The View Toolbar is Located at the top of the View as seen below.
Each view toolbar contains a selection of the following communication options:
device.
For more view specific information see:
The Register Debugger is a Tool View which allows the performance of raw register reads and writes, see Here for more information.