Click here to return to the Hardware Setup page
AD2433 with SOM carrier ez-kit
Evaluation boards
The AD243x standard power evaluation boards used in the demos are explained in the following subsections.
ADZS2433-MINI
Figure 39 shows a ADZS2433-MINI board which can be used as a standard power A2B master. The board has following peripherals
Figure 39: ADZS-2433MINI
Hardware modifications
The following hardware modifications are required:-
For all ADZS2433-MINI boards, remove R21, R18, R58, R59.
For all ADZS2433-MINI boards, add R17.
For the board with
I2C address 0x68, remove R33 and add R34.
For the board with
I2C address 0x6A, remove R34 and add R33.
Jumper settings
The jumpers on the board must be in the following positions
EVAL-AD2433WB1BZ
Figure 40 shows EVAL-AD2433WB1BZ board which can be used as a standard power bus powered A2B sub node. The board has following peripherals
Figure 40: EVAL-AD2433WB1BZ board
Jumper settings
The following jumper settings are required:-
EV-21569-SOM Rev B
EV-SC594-SOM Rev B
EV-SOMCRR-EZKIT Rev A
Connections
To run the sample demo, the following setup connections are to be made.
Figure 41: Multi-main connections using PC(Host) and ADSP-21596 SOM carrier kit and ADZS2433MINI’s
The step described in this section are recommended to run the following configurations
AD2433 multi-main sample demo using
ADSP-21596 platform and PC as host.
The Evaluation boards shall be connected in the following order.
Connect the EV-21569-SOM to the EV-SOMCRR-EZKIT.
Connect one of the two ADZS2433-MINI boards to J10 A2B interface of the EV-SOMCRR-EZKIT. Let this be “main node 0” with
I2C address configured to be 0x68.
Connect other ADZS2433-MINI to J11 A2B interface of the EV-SOMCRR-EZKIT. Let this be “main node 1” with
I2C address configured to be 0x6A.
For A2B chain 0:- ADZS2433-MINI (Main node 0) → EVAL-AD2433WB1BZ (Sub node 0) → EVAL-AD2433WB1BZ (Sub node 1), the connections are as follows
Connect twisted-pair wire between the “B” connector on the main node 0 board and the “A” connector on the sub node 0 board.
Connect twisted-pair wire between the “B” connector on the sub node 0 board and the “A” connector on the sub node 1 board.
For A2B chain 1:- ADZS2433-MINI (Main node 1) → EVAL-AD2433WB1BZ (Sub node 2) → EVAL-AD2433WB1BZ (Sub node 3), the connections are as follows
Connect twisted-pair wire between the “B” connector on the main node 1 board and the “A” connector on the sub node 2 board.
Connect twisted-pair wire between the “B” connector on the sub node 2 board and the “A” connector on the sub node 3 board.
Connect 12V power supply to the power connector of EV-SOMCRR-EZKIT.
Audio In/out for ADSP-21569 and PC as a host – multi-main
Connect an audio source (
e.g., output from an iPod) to ‘Audio Line- in’ port, shown in
Figure 41 (Audio Input).
Connect separate audio sink such as headphones to line out as shown in the
Figure 41 .