Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:tools-software:a2bv2:quickstartguide:hardware-setup:ad2430 [09 Dec 2022 07:24] – [Sample Demo Setup] Gireesha Nirvanaiahresources:tools-software:a2bv2:quickstartguide:hardware-setup:ad2430 [05 Oct 2023 15:22] (current) Sanjeeva Reddy
Line 1: Line 1:
 +**[[:resources:tools-software:a2bv2:quickstartguide:hardware-setup | Click here to return to the Hardware Setup page]]**
 +
 ====== AD2430 ====== ====== AD2430 ======
  
Line 5: Line 7:
  
 ==== EVAL-AD2430WD1BZ ==== ==== EVAL-AD2430WD1BZ ====
-Figure 14 shows an EVAL-AD2430WD1BZ board which can be used as either an A2B main or sub node. The board has following components+[[:resources:tools-software:a2bv2:quickstartguide:hardware-setup:ad2430#eval-ad2430wd1bz|Figure 14]] shows an [[:resources:tools-software:a2bv2:quickstartguide:hardware-setup:ad2430#eval-ad2430wd1bz|EVAL-AD2430WD1BZ]] board which can be used as either an A2B main or sub node. The board has following components
   * AD2430 A2B transceiver   * AD2430 A2B transceiver
   * ADAU1452 SigmaDSP Audio Processor   * ADAU1452 SigmaDSP Audio Processor
Line 17: Line 19:
  
 ==== EVAL-AD2430WC1BZ ==== ==== EVAL-AD2430WC1BZ ====
-The Figure 15 shows an EVAL-AD2430WC1BZ board which can be used as an A2B sub node. The board has following peripherals+The [[:resources:tools-software:a2bv2:quickstartguide:hardware-setup:ad2430#eval-ad2430wc1bz|Figure 15]] shows an [[:resources:tools-software:a2bv2:quickstartguide:hardware-setup:ad2430#eval-ad2430wc1bz|EVAL-AD2430WC1BZ]] board which can be used as an A2B sub node. The board has following peripherals
   * AD2430 A2B transceiver   * AD2430 A2B transceiver
   * 4 PDM Microphones   * 4 PDM Microphones
Line 26: Line 28:
  
 ==== EVAL-AD2428WB1BZ ==== ==== EVAL-AD2428WB1BZ ====
-Refer Section 3.5.1.1.1+Refer [[:resources:tools-software:a2bv2:quickstartguide:hardware-setup:ad242x-standard-power#eval-ad2428wd1bz|Section 3.5.1.1.1(Jumper Settings)]]
  
  
Line 34: Line 36:
 ==== Evaluation boards ==== ==== Evaluation boards ====
 A2B Evaluation boards shall be connected in the following order A2B Evaluation boards shall be connected in the following order
-  - EVAL-AD2430WD1BZ (Main) <–>EVAL-AD2428WB1BZ (Sub 0) <–> EVAL-AD2430WC1BZ (Sub 1) as shown in Figure 16+  - [[:resources:tools-software:a2bv2:quickstartguide:hardware-setup:ad2430#eval-ad2430wd1bz|EVAL-AD2430WD1BZ]] (Main) <–>[[:resources:tools-software:a2bv2:quickstartguide:hardware-setup:ad242x-standard-power#eval-ad2428wb1bz|EVAL-AD2428WB1BZ]] (Sub 0) <–> [[:resources:tools-software:a2bv2:quickstartguide:hardware-setup:ad2430#eval-ad2430wc1bz|EVAL-AD2430WC1BZ]] (Sub 1) as shown in [[:resources:tools-software:a2bv2:quickstartguide:hardware-setup:ad2430#evaluation_boards1|Figure 16]]
   - Connect twisted-pair wire between the A2B connector on the Main board and the “A” connector on the Sub 0 board.   - Connect twisted-pair wire between the A2B connector on the Main board and the “A” connector on the Sub 0 board.
   - Connect twisted-pair wire between the “B” connector on the Sub 0 board and the A2B connector on the Sub 1 board.   - Connect twisted-pair wire between the “B” connector on the Sub 0 board and the A2B connector on the Sub 1 board.
   - Connect 12V power supply to the power connector (P7) on AD2430WD1BZ board.   - Connect 12V power supply to the power connector (P7) on AD2430WD1BZ board.
-<note>This connection is recommended for running the sample demo using PC as host. Refer Section 5 for more details on using ADSP-21569 as host processor.</note>+<note>This connection is recommended for running the sample demo using PC as host. Refer Section 5 for more details on using ADSP-21569 as host processor</note>
  
 {{:resources:tools-software:a2bv2:quickstartguide:a2b_eval_board_connections.png?500|}} {{:resources:tools-software:a2bv2:quickstartguide:a2b_eval_board_connections.png?500|}}
Line 49: Line 51:
  
 ==== Audio In/out ==== ==== Audio In/out ====
-  * Connect separate audio sources (e.g., output from an iPod) to ‘Audio Line- in’ on AD2428WB1BZ as shown in Figure 16 +  * Connect separate audio sources (e.g., output from an iPod) to ‘Audio Line- in’ on AD2428WB1BZ as shown in [[:resources:tools-software:a2bv2:quickstartguide:hardware-setup:ad2430#evaluation_boards1|Figure 16]]. 
-  * Connect separate audio sinks (e.g., active speakers) to ‘Audio Line-out’ ports, shown in Figure 16, on AD2430WD1BZ and AD2428WB1BZ.+  * Connect separate audio sinks (e.g., active speakers) to ‘Audio Line-out’ ports, shown in [[:resources:tools-software:a2bv2:quickstartguide:hardware-setup:ad2430#evaluation_boards1|Figure 16]], on AD2430WD1BZ and AD2428WB1BZ.
  
  
Line 62: Line 64:
 **Figure 17:** Sample A2B demo configuration **Figure 17:** Sample A2B demo configuration
  
-For PC Software setup, refer section 2.1.1 and for Hardware Setup refer section 4.1.2.4 . To run the sample demo, refer section 4.1.3 .+For PC Software setup, refer [[:resources:tools-software:a2bv2:quickstartguide:systemrequirements#software_requirements|Software Requirements]] and for Hardware Setup refer [[:resources:tools-software:a2bv2:quickstartguide:running-sample-demo#hardware_setup|Standard Power – AD2430 / AD2438 jumper setting]] . To run the sample demo, refer [[:resources:tools-software:a2bv2:quickstartguide:running-sample-demo#running_sample_demo|Running the Sample Demo)]] .
  
  
 ===== SC59x EZ-Kit Mode ===== ===== SC59x EZ-Kit Mode =====
 This section describes the steps to run the demo using EV-SC594-SOM with AD2430. This section describes the steps to run the demo using EV-SC594-SOM with AD2430.
-*Note:* Running this demo requires CrossCore Embedded Studio to be installed on the machine. For details, refer section 2.1.1+*Note:* Running this demo requires CrossCore Embedded Studio to be installed on the machine. For details, refer  [[:resources:tools-software:a2bv2:quickstartguide:systemrequirements#software_requirements|Software Requirements]]
  
 ==== Setup ==== ==== Setup ====
 The hardware connections to be done are described below. The hardware connections to be done are described below.
 A2B Evaluation boards shall be connected in the following order A2B Evaluation boards shall be connected in the following order
-  - EV-SC594-SOM (Rev B) <-> EV-SOMCRR-EZKIT (Rev A) <–>Eval-AD2430WD1BZ(Main) <-> EVAL-AD2428WB1BZ (Sub 0) <–> EVAL-AD2430WC1BZ (Sub 1) as shown in Figure 18+  - EV-SC594-SOM (Rev B) <-> EV-SOMCRR-EZKIT (Rev A) <–>Eval-AD2430WD1BZ(Main) <-> EVAL-AD2428WB1BZ (Sub 0) <–> EVAL-AD2430WC1BZ (Sub 1) as shown in [[:resources:tools-software:a2bv2:quickstartguide:hardware-setup:ad2430#setup|Figure 18]]
   - Connect twisted-pair wire between the “B” connector on the Main board and the “A” connector on the Sub 0 board. Repeat the same connection between Sub 0 and Sub 1   - Connect twisted-pair wire between the “B” connector on the Main board and the “A” connector on the Sub 0 board. Repeat the same connection between Sub 0 and Sub 1
   - Connect 12V power supply to the power connector (P8) on EV-SOMCRR-EZKIT board.   - Connect 12V power supply to the power connector (P8) on EV-SOMCRR-EZKIT board.
   - Connect 12V power supply to the power connector (P7) on Eval-AD2430WDZ board.   - Connect 12V power supply to the power connector (P7) on Eval-AD2430WDZ board.
   - Attach JTAG to P1 on EV-SC594-SOM board and other end of JTAG to USB port of PC.   - Attach JTAG to P1 on EV-SC594-SOM board and other end of JTAG to USB port of PC.
-  - Connect audio source (e.g., output from an iPod) to ‘Audio Line- in’ ports, shown in Figure 18, AD2428WB1BZ boards. +  - Connect audio source (e.g., output from an iPod) to ‘Audio Line- in’ ports, shown in [[:resources:tools-software:a2bv2:quickstartguide:hardware-setup:ad2430#setup|Figure 18]], AD2428WB1BZ boards. 
-  - Connect separate audio sinks (e.g., active speakers) to ‘Audio Line-out’ ports, shown Figure 18, on EV-SOMCRR-EZKIT and AD2428WB1BZ boards.+  - Connect separate audio sinks (e.g., active speakers) to ‘Audio Line-out’ ports, shown [[:resources:tools-software:a2bv2:quickstartguide:hardware-setup:ad2430#setup|Figure 18]], on EV-SOMCRR-EZKIT and AD2428WB1BZ boards.
  
 {{:resources:tools-software:a2bv2:quickstartguide:sc594-ad2430_setup.png?400|}} {{:resources:tools-software:a2bv2:quickstartguide:sc594-ad2430_setup.png?400|}}
Line 89: Line 91:
 === Running target framework on EV-SOMCRR EZ-KIT === === Running target framework on EV-SOMCRR EZ-KIT ===
   - Ensure that the “Boot Mode” switch is set to 0 on the EV-SC594-SOM EZ-KIT board.   - Ensure that the “Boot Mode” switch is set to 0 on the EV-SC594-SOM EZ-KIT board.
-  - Connect the JTAG (ICE 1000 or ICE 2000) and power on the board with the setup as shown in 3.4.4.1 .+  - Connect the JTAG (ICE 1000 or ICE 2000) and power on the board with the setup as shown in[[:resources:tools-software:a2bv2:quickstartguide:hardware-setup:ad2430#setup| Setup]] .
   - Create Debug Session in CCES by clicking Run -> Debug Configurations -> Application with CrossCore Debugger -> Sharc -> SC594 -> Emulator -> ICE 1000 / 2000 -> Finish   - Create Debug Session in CCES by clicking Run -> Debug Configurations -> Application with CrossCore Debugger -> Sharc -> SC594 -> Emulator -> ICE 1000 / 2000 -> Finish
   - Select the SC59x dxe to be loaded and click Debug to start the session as shown below.   - Select the SC59x dxe to be loaded and click Debug to start the session as shown below.
resources/tools-software/a2bv2/quickstartguide/hardware-setup/ad2430.txt · Last modified: 05 Oct 2023 15:22 by Sanjeeva Reddy